Posted by
14rhb Feb 3, 2019
This is a quick blog post about using my NooElec SDR for the first time. Back last year I was luckily chosen to roadtest three Molex Antennas Molex 2.4GHz / 5GHz Antenna Kit - Review and that re-kindled my interest in RF work at home. Wanted to have a 'play around' I bought myself a low-cost SDR for fun and it arrived today. It cost me just over £20 (UK) and plugs into the USB port of my computer plus it has a SMA connector for the antenna. I actually made a misjudgment and bo ...
Posted by
14rhb Jan 13, 2019
Wearable Tech Enter Your Electronics & Design Project for a chance to win a $100 Shopping Cart! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll
Introduction
My Submission to Wearable Tech
Basic Design Calcs
Time for a PCB
Construction
The Program and Programming
Finishing Off
Summary
Introduction When it was commented that there was only one applicant for the Wearable Tech Project14 I joked that I was going to wire ...
Posted by
14rhb Jan 11, 2019
Merry Boxes & LEDs Enter Your Project for a chance to win a Maker Tool Kit, an Oscilloscope Grand Prize for the project that brings the Most Joy to the Heart, and Gift to Gives! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll
1. Videos
1.1 First Video
1.2 Second Video
2. The Effects
2.1 PIC Microcontroller Firework ...
Posted by
14rhb Dec 31, 2018
Merry Boxes & LEDs Enter Your Project for a chance to win a Maker Tool Kit, an Oscilloscope Grand Prize for the project that brings the Most Joy to the Heart, and Gift to Gives! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll I added a few other effects to follow on from LED Fireworks - Festive Lights 2018 including an Arduino Uno powered effect with the initial streak as the rocket goes up. Happy new year to everyone on Element14 (members ...
Posted by
14rhb Dec 2, 2018
Merry Boxes & LEDs Enter Your Project for a chance to win a Maker Tool Kit, an Oscilloscope Grand Prize for the project that brings the Most Joy to the Heart, and Gift to Gives! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll I posted a Status Update yesterday stating I had put up some festive lights and genebren asked if I had any photos: so I've just been outside and video'd them...as you can see I'm not very good with a camera and focusing in t ...
Posted by
14rhb Sep 30, 2018
1. STM32CubeMX - Creating a Music Player
2. SW4STM32 - An Initial Build
3. Adding Some 'Screenage'
4. My Next Steps
Previous Blog: STM32L4R9I-Discovery Board: Part 3 (the development cycle) This is my final blog that will form the basis of my roadtest review on STMicroelectronics STM32l4R9I-discovery board. I have managed so far to get the development cycle to work wit ...
Posted by
14rhb Sep 23, 2018
Forward
1. 'Bricking' My Board
2. STM32 Demo Application
3. The Board Support Package (BSP) Example
4. Making My Own Copy of a Project
5. Modified BSP Demo - My First Program ?
6. Useful Links
7. Next Steps
8. Millennium Falcon Makes the Jump to Light Speed...only on the STM32L4R9I-disco ...
Posted by
14rhb Sep 15, 2018
Differences Pynq-Z1 and Digilent Arty-Z1
Jupyter Notebook
Online Notebook - "Hello Element14" Example
Online Notebook - 'Bottles of Beer' Example
Online Notebook - Cells With Different Content
Jupyter Notebook on My PYNQ-Z1
Pynq-Z1 Board - Buttons and LEDs Example
Pynq-Z1 Board -The Microblaze Softcore
Summary So Far
To Follow
I really enjoyed my recent Roadtest of the Digilent Arty S7 board Digilent ARTY S7 Dev Board (Xilinx Spartan 7) - Review b ...
Posted by
14rhb Aug 25, 2018
I'm not sure how I've managed this; I've read plenty of articles on controlling stepper motors, stripped stepper motors from old printers to keep them and even bought a nice set of 5x NEMA steppers for making a 3D printer....but I've never actually got around to powering and controlling one. Seeing all the cool things E14 members are making and especially in the Movers and Shakers Project14 I decided I really must get one working. I had a A4988 mini driver board that was for my 3D printe ...
Posted by
14rhb Jul 21, 2018
During a discussion over a friend's flat car battery they brought out their 'car battery booster' but it soon became apparent to me that that also wasn't working....and so, like most tinkerers, engineers and makers, it ended up on my bench at home. The unit contained a 12v 13Ah Sealed Lead Acid (SLA) battery, large diameter cables and croc clips for connecting to the discharged car battery, a voltmeter, a light and an external cigarette lighter socket. Charging the booster unit was via ...
Posted by
14rhb Jun 17, 2018
This is my test of a Wera bitset. as shown below. 1. Initial Thoughts Without being biased, by knowing Wera is a quality brand, the first thing I noticed when getting the set out of the packaging was its weight. It had a decent amount of weight for the size which equated subliminally to me as 'there's a decent amount of real metal parts in here = it will be strong'. Inspecting the tool I could see it composed of the Zyklop Mini ratchet along the top, one visible ...
Posted by
14rhb Jun 9, 2018
Background
First Investigation
Roll On Another 2 Months
New Diode Selection
Reassembly and Testing
Diode Voltages (After Desoldering)
Safety
[Having mentioned this TV repair on my Status page and getting supportive comments from dixonselvan and genebren, I felt perhaps a blog post would help] Background I was given a nice 22" TV a few years ago as a present. About a year later it stopped working - not even the power light came on. I checked the fuse tha ...
Posted by
14rhb Jun 3, 2018
Preface I live in the UK and have never seen a native Firefly or glow worm - I'm not even sure if we get them here. Some years back I visited North Carolina to visit friends and was amazed to see fireflies flashing away in the garden shrubs ...if only I could bring that magic to my garden in summer by making some RGB LED 'fireflies'. My Initial Design Some years back I used the Microchip techsheet AN1606 and the Configurable Logic Cells (CLC) of the PIC16F1509 microcontroller t ...
Posted by
14rhb Oct 21, 2017
I bought an ESP-12 (ESP8266) module last year and, after mounting it in a DIL format (via a piece of Veroboard), I never got around to actually using it. A few weeks ago I dug the ESP-12 module out of the drawer, mounted it on my breadboard, added a 3.3v regulator, voltage divider and CD4011 (2x logic gates wired as a non-inverting buffer) and then fiddled away for a few evenings until I got it to boot properly. Satisfied with progress I ordered some more modules...the aim was to control ...
Posted by
14rhb Sep 5, 2017
Arduino Home An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. Arduino Tutorials Arduino Projects Arduino Starter Kit Competition INDEX: Element14's Arduino Starter Kit Competition Element14's Arduino Starter Kit Competition - Part 1 Element14's Arduino Starter Kit Competition - Part 2 Element14's Arduino Starter Kit Competition - Part 3 Element14's Arduino Starter Kit Competition - Part 4 Element14's Arduino ...