I admit it ain't too creative but I really wanted to know if the purple flames from my accidental destruction of a Tantalum cap was a fluke. I saw in Wikipedia that the flame test for tantalum is in deed blue so fancied a go at it and also it was an excuse to do some slow mo on my GoPro Hero 4( only 4x slow down though!).
Enjoy...it is Christmas after all ...
Had an email from XMOS yesterday advertising their latest competition. Rules are simple.. Create a Christmas orientated project using the XMOS device get it video'd and up on Youtube/Vimeo and do it before the 19th of December. Short notice I know but if you have already got a project that can be co-opted for the festive period then you may be up for a winner. Good luck
Here's the instructions on how to enter ...
Just had a read of this guys post who has some good advice and basic information on hacking those Linux in a can IP cameras which all seem to have the same design I think? Any way he gets to the serial port on the PCB and uses a USB-Serial adaptor to gain access through what is more of a side door than a back door(let's call it a tradesman's entrance) Well done blog post deserves to come over to E14...Any way over to him! http://felipe.astroza.cl/hacking-hi3518-based-ip ...
Well unfortunately he didn't get down and dirty on the details of his optical table Jason Sapan gives a good feel on how and what a Hologram is and what you can do with them.
You can go to the site http://www.holographer.com/ and see more they do visits and even internships which sounds great for those who have the bug to do such a thing. Either way a nice 13 min "nerd out" hope you'll enjoy .... John ...
Just thought I would catch up with you all with the OSCAR Display port Board and Panel. Still not perfect but a lot better. everything lines up at the front: Rear now gives access to the board to allow you to get to the Controls The stand is now separate making it easier to get the cables in also this makes the whole thing more flexible in as far as you can now mount it anywhere and now you can assemble one with out the other getting in the way ! No doubt I ...
Jim goes into his Electric Bike collection and how he's pimped them up with some interesting mods and exotic chemistry battery packs!
I can't believe it's been nearly 5 years since we were going on about these devices , nice to see they are still going well ...
OK.. I can't take any kudos for the design as my friend John2 ( ) did this himself with minimum interaction from me. Any way figured you would like to have a look at work so far! A few faults that need to be worked on but other wise excellent first effort! ...
A few months ago on Kickstarter I spotted OSCAR a device which allowed you to put an iPad screen on to a conventional PC with a Displayport adapter. Rather than some proprietary signalling the iPad panel supports Displayport directly and you could just wire it up to a cable if everything wasn't just so small also there is a small problem of power and control as well. This is where the OSCAR board comes in it has connectors for the Displayport 12V input and the iPad flat flex connector as well ...
The little WIFI device that can is certainly causing a stir amongst those folk including the IOT intelligentsia. A new SDK has been released as well as a Lubuntu based VM so you don't have to go through the bother of compiling the environment your self Or risking your desk top. Now that such devices are available to everybody at a ridiculous £3-$5 I can't wait to see what people produce next with it ! ...
The ESP8266 is an exciting new WIFI device. It's suddenly become so popular because of an influx of cheap (£3) modules been made available on EBAY. So obviously you have been able to get USB WIFI devices for this price for a while but now they even have all the processing and even some GPIO on board so all you require to access them is a serial port and a few AT commands. This makes WIFI practical for any Arduino/PIC/uC application that has at least one serial port which is a very lo ...
OK I'm ripping off my mate Jim again, sure he won't mind as he really can't be bothered to do the Blog posts This week he's taken the nichrome wire out of a toaster and making a couple of nice new toys namely an Acrylic Bender and Hot wire Polystyrene cutter. Murder a toaster and have fun today !!! Subscribe to his channel if you like the vid ...Cheers ...
Ok Just another quick one. My mate Jim has been hacking away building switch gear for his Hydroponic set up. Anyway cheap ebay timers and a nice box to mount them in and some basic mechanical building to make them safe. Take a look and enjoy ...
Shropshire Linux User Group(Yeah SLUG!!) had a stand at the local Radio Rally(TDARS) on the 1st. We had a 3D printer,QSSTV decoding images from our visitor operated "SSTV Selfie Cam" running on a Raspberry Pi and FLDIGI busily decoding data from the attached radio. Around 1000 visitors came through the doors so we had our work cut out demonstrating and showing all things Linux to the Radio crowd! ...
Well a few weeks ago now I actually got down to Wuthering Bytes Open Hardware Meetup @ Hebden Bridge, UK once again. The meet up was excellent as usual and now extends over 3 days including the Sunday Workshop. Having a single track over two days made it easier to see all the talks with out compromise. Talks varied from designing space capable rockets to flood warning systems and the future of microprocessors .£10 per day with some food represented excellent value! Thanks aga ...
Still with Jim and his Vids around 4 years ago we purchased an old carriage for use as a robot base. Jim had over a period of a few weeks reverse engineered the control protocol for the attendant pendant which allows for a carer to completely control the chair. That way he was able to robotically control the chair without destroying it in the process the result is PIP.
Watch PIP chase his beloved Apples ......Subscribe if you want to see more ...