Skip navigation
2014
I'm currently waiting for my HackRF to arrive via the Kickstarter so I recently received  a nice update report showing what folk are doing with the HackRF Jawbreaker which is the development release of the Hack RF.   Hopefully mine will arrive Feb so more updates then!!! ...
Since I have made lots of friends in the QL community I'm very happy to say that  the QL is now 30 Based on the 8bit version of the 68K the 68008 and 128K of RAM it opened a whole range of 3rd party hardware/software and still after all this time has a wide following and Vendor support   Enjoy the little trip to the 80;s      ...
I saw this on the BBC??? it shows  that there's nothing new in re-using even the most banal of tech like a kid's toy into a technical weapon...Here's more on Gizmodo   ...
  The Idea of gun totting penguins comes to mind but this is the real thing a $17K rifle from a company from Austin Tx called Trackingpoint   View Through the Sight     The aiming system actually makes the pressure required to pull the trigger change depending on the lock so it's still possible to fire with out the computer but it's much harder so the human is still in charge of firing but still it raises ethical questions! The whole article is here at Arstech ...
Is here again 1st and 2nd of Feb in Brussels As they say 400+Lectures and 5000+ attendees. FOSDEM is huge and has topics from Open source Mapping to Linux to ARM64 to Big Data to social issues. I'm going  but who else is from the Element 14 community? Fancy meeting up ...shout out here and reply below. See you there!! ...