Posted by
dhal Jan 12, 2018
1/ Raspberry's configuration I have downloaded the "Raspbian Stretch with Desktop" version from the Rasperry site and copy the image with Win32DiskImager on a 16Go micro SDHC card (class 10, up to 100 MB/s, "A1"). I have let the raspberry boot on it (expand the filesystem), then I have adapted the local configs (keyboard, TimeZone, no splash ..) and allowed SSH login . After that, I have added some extra info in the /boot/cmdline.txt file : - logo.nologo ...
Posted by
dhal Jan 12, 2018
Let's report on the Tractor simulator (cabin tractor interface with Farming Simulator 17): Part 1 to see the global sketch. All the PC, except Master, start at boot. The following launch.bat are linked in C:\Users\{USER}\AppData\Roaming\Microsoft\Windows\Start Menu\Programs\Startup directory (accessible with Startup:shell in execute menu). launch.bat____________________________________________________________________________ @echo off color 71 set PROC=ExeToLaunchWithoutExeExt ...
Posted by
dhal Jan 12, 2018
All elements (hardware & software) to realize a tractor simulator interface for Farming Simulator 17 See the videos in demo mode (with a speaker, see video1 ) and in play mode (guests can play with FS17, see video2, video3,). Global presentation Tractor simulator (cabin tractor interface with Farming Simulator 17): Part 1 - global presentation The hardware Tractor simulator (cabin tractor interface with Farming Simulator 17): Part 2 - the hardware Arduino ...
Posted by
dhal Dec 15, 2017
Here is one of my recent works; creating an interface between a cabin tractor and Farming Simulator 17 (FS17) software for an exhibition. The goal was to show the benefits tire technology and linked services could bring to a farmer. So 2 modes were prepared: a demo mode (with a speaker, see video1 ) and a play mode (guests can play with FS17, see video2, video3,). The global sketch ¤ 3 raspberry pi: to display the dashboard, to simulate the "zen@terra" application (tha ...
Posted by
dhal Dec 15, 2017
1/ the outputs (tractor lights - beacon, blinkers, lights) I choose to use a Raspberry Pi for this task (Raspberry "Outputs" on the global sketch); I needed something independent of the PCs to lighten their processes and a board that can receive orders from TCP/IP. Fortunately, I didn't need more than 24 outputs. So I have designed an extended board, with a voltage shifter (Txs0108e) (from 3.3V to 5V) to switch relays on a 8 relays module: I have preferred to let the l ...
Posted by
dhal Dec 17, 2017
1/ Arduino DUE 1.1/ Keyboard : (attached to "FS Hat" PC) Arduino DUE has to behave as a keyboard, so I will use the <keyboard.h> lib. But all the keys are not included in this lib, so an extension is needed to add extra keys: keyboard_ext.h ______________________________________________________________ /* Keyboard_ext.h keyboard extension adapted from https://github.com/rampadc/arduino-thinkpadkb-usb/blob/master/MicroThinkPadAda ...