Skip navigation

Blogue de Damien Hallez

December 2017 Previous month
Here is one of my recent works; creating an interface between a cabin tractor and Farming Simulator 17 (FS17) software for an exhibition. The goal was to show the benefits tire technology and linked services could bring to a farmer. So 2 modes were prepared: a demo mode (with a speaker, see video1 ) and a play mode (guests can play with FS17, see video2, video3,).   The global sketch   ¤ 3 raspberry pi: to display the dashboard, to simulate the "zen@terra" application (tha ...
1/ the outputs (tractor lights - beacon, blinkers, lights)   I choose to use a Raspberry Pi for this task (Raspberry "Outputs" on the global sketch); I needed something independent of the PCs  to lighten their processes and a board that can receive orders from TCP/IP. Fortunately, I didn't need more than 24 outputs. So I have designed an extended board, with a voltage shifter (Txs0108e) (from 3.3V to 5V) to switch relays on a 8 relays module:   I have preferred to let the l ...
1/ Arduino DUE   1.1/ Keyboard : (attached to "FS Hat" PC)   Arduino DUE has to behave as a keyboard, so I will use the <keyboard.h> lib. But all the keys are not included in this lib, so an extension is needed to add extra keys:   keyboard_ext.h  ______________________________________________________________ /*   Keyboard_ext.h     keyboard extension adapted from   https://github.com/rampadc/arduino-thinkpadkb-usb/blob/master/MicroThinkPadAda ...