I decided I was too cheap to buy them one but I will spend the time to design and make it go figure eh?

With a little help from the CNC Machine and V-Carve Pro I most of the battle is done.  I see tons of these on the internet not sure why I don't see

anything special about them but hey the kids wanted some so why not was a fun project to play with tomorrow I finish up the stain and clear coat just have

to design some bearing caps which I will make on the CNC machine as well. I thin I could have done it a bit different and made the bearing hole .3 mm smaller.

Just to add a bit more pressure but I hope the stain an clear coat will help swell the bearings into place a bit better ill add a bit of glue tho.  Will probably

change the size on my next ones tho.

 

20170418_161206.jpg