So I was trying to figure out a decent way to speed up the time it took to reset I ended up taking another instance of the low being +2
and then adding the first high-low-low as being 2.25 degrees I have added a few video's so you can see the results I am by far no means
any good when it comes to messing with the arduino besides using other people code but since I got that kit let me tell you its be a great
adventure in the arduino land.


//LOVE METER WITH FASTER RESET.
const int sensorPin = A0;const float baselineTemp = 22.0;
void setup(){   Serial.begin(9600);
  for(int pinNumber = 2; pinNumber<5; pinNumber++){    
pinMode(pinNumber,OUTPUT);   
digitalWrite(pinNumber, LOW); 
}
}
void
loop(){ 
int sensorVal = analogRead(sensorPin);  
Serial.print("Sensor Value: ");  
Serial
.print(sensorVal);  
float voltage = (sensorVal/1024.0) * 5.0;  
Serial
.print(", Volts: ");  
Serial
.print(voltage); 
Serial.print(", degrees C: "); 
float temperature = (voltage - .5) * 100;  
Serial
.println(temperature);    
if
(temperature < baselineTemp){    
digitalWrite
(2, LOW);    
digitalWrite
(3, LOW);    
digitalWrite
(4, LOW); 
}  
else
if(temperature >= baselineTemp+2.25 && temperature < baselineTemp+4){    
digitalWrite(2, HIGH);    
digitalWrite
(3, LOW);    
digitalWrite(4, LOW);   }  
else if(temperature >= baselineTemp+4 && temperature < baselineTemp+6){    
digitalWrite
(2, HIGH);    
digitalWrite
(3, HIGH);    
digitalWrite(4, LOW);   }  
else
if(temperature >= baselineTemp+6){    
digitalWrite(2, HIGH);    
digitalWrite
(3, HIGH);     digitalWrite(4, HIGH);  
}  
else if(temperature >= baselineTemp+2){    
digitalWrite(2, LOW);    
digitalWrite
(3, LOW);    
digitalWrite
(4, LOW);  
}  
delay(.25);




This code seemed to output the following for me which I didn't think to be ideal the above code tho
Produced the below video here which I felt was better.  (was a bit cooler in the room when I did this bottom one
so test didn't light up all 3 but will give you a example of the drop at the end)


PLEASE POST BELOW IF THERE IS A BETTER CODE TO TRY.
Will play with this more but more info is always appreciated.