Skip navigation
For the past few years, hey its been more like a decade. I have been working on an experimental aircraft the Phoenix2000 which was to have flown in, yup you guessed it, thirteen years ago. Well we can all dream a little. In my currently reduced circumstances I can not build the airframe, hey there is only so much crap you can get into a two bedroom apartment. So a few years ago I decided to write a simulation of the aircraft. As it turns out building the plane is much easier than getting all th ...
If you can remember last time I said that I would describe the Control program running on the Linux box. Well its rather simple once you understand the signal(2) command. This is the mechanism which receives the interrupt and then sends it the right handler or function.   This diagram is a simplified block diagram of RadioControl running on the LinuxPc. So lets assume that the pilot changed the frequency on the Radio #2 on that Gables head. DATA TO RadioControl from the Slave The Sla ...
This is a copy of Scotts article that I found the picture of so called good soldering technique published in Import Tuner:   The most fundamental skill needed to assemble any electronic project is that of soldering. Basic soldering is a skill that's easy to learn and not too hard to master but misconceptions on the proper procedures also include many individuals having no clue on where to start.  Soldering is accomplished by quickly heating a metal or metallic alloy to join metallic s ...

Filter Blog