Skip navigation
Monthly Projects: Aug 2018 - Dec 2019 Aug 14, 2018 Clustered MCUs: Anything Goes with Two or More MCUs! Feb 11, 2019 Electromagnetism: The Force of Electromagnetism: Anything from Solenoids, Motors, to Wireless Transfer! Aug 25, 2018 RSS using RS-485 w/ NASA's Edian Lite Bus Protocol. Feb 20, 2019 Smarthab: Door Locks .. Overview Sep 10, 2018 Test Instrumentation: Apr 24, 2019 Smarthab: Door Strikes Sept 19, 2018 Automated Cable Test System .. part 1 June 4, 2019 Remote Monitoring and Control: ...
Well, this was a mess, and I blame it on myself. In my rush to work on the box, I disconnected all the plugs, I just wanted them out of my way. No, I did not cut them nor did I record what was hooked to what and where.  So I had to do this one on my own. On the back of the unit, there are five 50-pin male receptacles, which are 10 x 10 easy. The Jacks are labeled J1 through J5 and have cables attached to them. The other end of the cables has a 34-pin male header. One is pin 1 to pin 34, whi ...
have talked about the CP-1252/ASN-128 before Hacking The Navigation Computer Display. I have changed my mind about using a ps2 decoder to interface with the keyboard. I will write my own. It's about 30 lines of code, not including Scanner.h  (prototypes) and Matrix.h which describes the 2 dimension array for the keyboard. The Switches where made by Clare Pendar (Now Visualux) Pn: S180 11D5F4 and are very pricey. Thankfully I have about 3 of these units in various stages of disrepair so part ...