Skip navigation
Monthly Projects II: 2020 - 2021 1/25/20/20 Acoustics Competition Sep 21, 2020 Sensors Competition: Design, Control System 1/25/2020 Nexgen: FAA Nav Aid Station Morse Code Id Sep 25, 2020 Smarthab smart thermostat 2/03/2020 Slant Range Math - Revisited Sep 28, 2020 Better name Life Support: Monitor and Control. 2/09/2020 Design Overview Oct 12, 2020 Recycle & Retrofit Software Design Sept 22, 2020 NexGen: Fuel Load Indicator: Pinouts Redux 4/5/2020 Morse Code Software Oct 14, 2020 NexGen ...
On the bench Terminal Session Well, I'm not done yet. I might be down. I need some more stuff for this project so off to Micro Center. And about 130 miles later. I started over from scratch here is what I did: * Please note: this information has come from two sources https://elinux.org/Beagleboard:BeagleBoneBlack_Debian#Flashing_eMMC BeagleBone AI Survival Guide V3.11: PWM I downloaded a new image from Debian to my computer. copied to my 64 Gb Flash with a DD command. In /boot/uEnv.txt:  ...
Road Tests: Smarthab: Jul 21, 2013 Review of Anaren AIR CC2530 BoosterPack Kit Feb 5, 2019 Essentials: Automation I Sep 27, 2015 Review of  TI Multi-Node IoT Bundle Dec 24, 2019 Welcome to Smart Wiring Dec 12, 2019 Smart wiring II Feb 11, 2019 Door Strikes Sept 14, 2019 Facial Recognition Jun 4, 2019 Remote Sensing and Control   Back to the Main Index ...
To give you all a refresher about NASA's EADIN Lite Communications Protocol, I was happy to embrace it. The problem is the downsides for me: Only an 8-bit payload. Before the Data Field, I need a Data Lenth Field of 1 byte Each board must be programmed for its unique address in the chain. As I am very lazy, I can resolve this by installing a 4-bit switch that can be set be for installing into the network. This address is read at startup. And I don't need the CRC check Also, the node_ID and ...
Well, the power and the cables are getting under my skin. So being in Dallas, I stopped at Tanners Electronics, and I solved my cooling issues and power which now includes a 12vdc fan. So this is what I picked up today. A Pace AC Adapter 115AC to 12vdc @ 3amps. A female DC jack to plug the power supply into.  A DC fan model: FFB0812EHE 12vdc @ 1.35 amps A DC to DC converter. (Adjustable) A USB A Breakout board This is all going is a small plastic box, as I am tired of the balancing ...
As much as l like Debian 9.x, I hate this jury-rigged Cloud 9 Interface. Just getting the BB AI on my network (static IP address) was a chore and way too many steps! This took many hours of trial, blind alleys, and miss-steps, As there is NO network icon on the desktop or trays. So for those of you that want to follow in my footsteps, here we go: Click on the Red Menu button in the lower-left Click on Preferences Click on Connman UI Click on Config  button at the bottom right (you mi ...
It's Alive!! ...
Well, this update has been more than a few days in coming, as I have been in network hell. I have made good progress, and I am working on programming currently. This was the first time I used a Polyprinter at my local library.  The Tinkercad and the Polyprinters work-beds were not the same sizes. The first panel with the pictures I lost and the second attempt was better. Second Attempt Maybe on the third try, I'll get it right.  I wish that there was a program that was better then Tin ...

Filter Blog