Skip navigation
They claim and I quote "Loose Batteries can touch and lose power" are they nuts? This claim is about 1 minute in. Did the world of physics or electronics change??  In the words of PT Barnum "There's a sucker born every minute"         ...
Ok, First Remove the Three (3) Knobs. Next, Remove the Filter lens which has six (6) Allen screws (in Red). Now remove the five (5) screws (in Green) from the light plate itself. Next Insert s plastic kitchen knife and very gently pry the plate off as there is a power connector built-in. Now using a 9/16" nut driver remove the two rotary switches nuts, push them through and replace the hardware so you don't lose them. Also use a 9/8" nut driver to loosen the dimmer nut. Next, there are 4 ...
phoenixcomm

MCU-128 Backpanel

Posted by phoenixcomm Top Member Jul 23, 2021
PROBLEM: I have been struggling to find a solution to a mess that has stopped me from doing much with this project. The interconnection is weird 0.025" square, on a 0.1" center. Nothing fits this dam thing to make matters worse there are no manufacture part numbers After being on the phone with AMP customer support and then he wants pictures, oh no. In my desperation, I called Samtec. SOLUTION: Guss what this damn thing is a standard connector. They are sending me a bunch of the little sobs. S ...

Filter Blog