I needed to create a 3D printed case for my Maixduino kit to make it easier to handle.  I came up with a quick prototype that I'll need to tweak but it lets me get started with testing.

Maixduino case LCD side

 

The small cutout at the bottom of the case is for the external speaker connector.  I haven't provided the opening yet for the MEMS microphone which is located about halfway between the camera and the speaker connector.  It will be interesting to see how well the microphone will work embedded within a case.  And I'll need to print a cover for the exposed section.  I left it open for now to allow easy access to the Reset and Boot push buttons.  I'll also probably want to add some function buttons in the blank area to the right of the LCD.

Maixduino case Camera side