Skip navigation
ralphjy

JQ6500 MP3 Player

Posted by ralphjy Top Member Sep 26, 2021
I recently saw a discussion by Sean Conway about an MP3 Player that he was attempting to control: Looking for member insight into the JR6001 Serial MP3 Custom Programmable Sound Recorder Module .   That inspired me to try out a similar module - the JQ6500 https://www.amazon.com/gp/product/B01N47M1V2/ref=ppx_yo_dt_b_asin_title_o00_s00?ie=UTF8&psc=1 .  I'll have to admit that I chose this one because it was available on Amazon Prime and I could get it in a couple of days.  Thes ...
I'm currently participating in the Low Power IoT Challenge.  I am trying to find a low power camera that I can use with the PSoC 62S2.  I've tried the OV7670: Arduino Nano 33 BLE Sense with OV7670 Camera .  I've ruled that one out because it requires more pins than I have available for its 8 bit parallel data interface.   The HM01B0 is a monochrome 324x324 camera that has a flexible data interface that can be 1-bit, 4-bit, or 8-bits wide.  The module that I'm using from ...
This is a continuation of my post: Arduino Nano 33 BLE Sense with OV7670 Camera .   I wanted to do a quick evaluation of the performance on a deployed object classification model.  I decided to develop a simple model to identify 3 fairly distinct hardware objects - a bolt, nut and washer.  This was not intended to be a rigorous test of the model quality.   I captured a small dataset from the camera using the Data Acquisition panel.  I used a white background and only a ...
I've been looking for a camera board that I could use with the PSoC 62S2 dev board for the Low Power IoT challenge.  This dev board does not have a dedicated camera interface and I haven't seen any examples using a camera.  vlasov01 suggested that I look at the Edge Impulse example that uses the Arduino Nano 33 BLE Sense with the OV7675 camera: adding sight to your sensors .  This is the same hardware used in the arduino-tiny-machine-learning-kit minus the shield that provides the ...