Skip navigation
Light Fidelity Background: Light Fidelity (Li-Fi) is a wireless communication method which uses light to transmit data between devices. "In technical terms, Li-Fi is a visible light communications system that is capable of transmitting data at high speeds over the visible light, ultraviolet, and infrared spectrums," (Wikipedia). The actual term "Li-Fi" was termed by Professor Harald Haas in his TED Talk, a co-founder of PureLiFi. This technology is fairly new and many different organizations are ...
THE PROJECT The plan for this project was to build a car which could be navigated via a WiFi connection and follow a black line. This blog post will go over the final product. We will be looking at both the hardware and software which was used in this project.   BILL OF MATERIALS MSP430FR5994 RF TXRX MODULE WIFI CHIP ANT CUSTOM CONTROL BOARD 120:1 MINI PLASTIC GEARMOTOR OFFSET 2mm SPLINE OUTPUT (2) LCD MODULE 4X10 WH BKGRND RFLT 2.6mm   THE CODE FIND THE ENTIRE CODE HERE   INIT_AD ...
In today's world it seems far too often computer security takes a backseat to all the drama and stories and feeds that engulf social media. So I decided in light of this and as a late Computer Security Day post I wish to enlighten those who may come across this post on the myths of password security and some good password hints and tips that are good for all platforms.   MYTHS: Complex Passwords are #1 Password strength is directly related to password entropy. Password entropy is increas ...