Skip navigation

Is Industrial Automation Ready for 5G?

5G is starting to being rolled out on telecom networks so consumers can take advantage of faster speeds and low latency is they can see and do amazing stuff on their treasured smartphones. But what about 5G in the industrial space? Augmented and virtual reality tech will surely use 5G to their advantage in manufacturing. Smart engineers will use 5G in machine vision and motion control systems at some point. But are they ready for it?

 

Poll question: Is Industrial Automation Ready for 5G?

Poll Results
  • They are ready to go! (0%)
    0/35
  • Some but not all are ready for 5G (26%)
    9/35
  • It's a work in progress (37%)
    13/35
  • Not even close (37%)
    13/35
  • Other; please explain in comments (0%)
    0/35

Comments

Archive Poll

Confirm archive of Is Industrial Automation Ready for 5G?

Archiving expires a poll and removes it from the active polls list.

To restore an archived poll, edit the poll, change the dates as desired, and save the poll.

Delete Poll

Confirm delete of Is Industrial Automation Ready for 5G?

Warning: This will delete the poll and all of its comments.