Skip navigation

Poll: Why Haven't You Applied for this Roadtest: STM32H7B3I-DK -  DISCOVERY KIT

Summertime is one of those busy times of year where people spend quality time with family, friends, and significant others. But this year you may be spending your summer time closer to home. And what better way to spend your quality time than with an element14 roadtest!

 

Inn particular, this roadtest: STM32H7B3I-DK -  DISCOVERY KIT

 

There are so many good things I could say about this dev board (with display). But the thing that stands out for me is what you can do with this board given all the peripherals you can experiment with:  the board help to evaluate the following peripherals: USB HS OTG, microSD™ card, 8-bit camera interface, audio DAC stereo with audio jack input and output, 128-Mbit SDRAM memory, 512-Mbit Octo-SPI Flash memory, Wi‑Fi® module (802.11 b/g/n compliant), I2C extension connector, FD-CAN, 20-pin microphone MEMS connector with DFSDM interface, 4.3-inch TFT-LCD (480*272) using an RGB interface with a capacitive touch panel.

 

You can even take advantage of three graphical stacks running on the same board with many featured applications:

– Menu launcher

– Audio player TGFX application (MP3 support)

– Clock and Weather with Alarm feature

– Video player TGFX application (enabled)

– TGFX Graphic demonstration

– STemWin Graphic demonstration

– EWZ Graphic demonstration

 

Poll Question: What's holding you back from applying to this roadtest?

Poll Results
  • Very Busy with other things (29%)
    11/38
  • My schedule is packed. (21%)
    8/38
  • Vacation time with the family (0%)
    0/38
  • I have other interests (3%)
    1/38
  • Just Not Interested (11%)
    4/38
  • Sorry, I'm golfing! (3%)
    1/38
  • Other; please explain in comments (34%)
    13/38

Comments

Archive Poll

Confirm archive of Poll: Why Haven't You Applied for this Roadtest: STM32H7B3I-DK - DISCOVERY KIT

Archiving expires a poll and removes it from the active polls list.

To restore an archived poll, edit the poll, change the dates as desired, and save the poll.

Delete Poll

Confirm delete of Poll: Why Haven't You Applied for this Roadtest: STM32H7B3I-DK - DISCOVERY KIT

Warning: This will delete the poll and all of its comments.