Skip navigation

Should the smaller screen be used in the SN35 Mini?

For more information, see the relevant post here: SN35 Mini Update #02 – How Big Is It Ben? – Hack Like Heck

Poll Results
  • Sure. It's supposed to be mini and portable, right? (47%)
    9/19
  • Of course, I wouldn't want a grip bigger than the original SNES controllers (0%)
    0/19
  • There has to be a way to include a bigger screen! (26%)
    5/19
  • Not sure.. it looks oddly long as it is. (11%)
    2/19
  • Meh. I'm not really a fan of the SNES controllers anyway (5%)
    1/19
  • None of these - see my comment below! (11%)
    2/19

Comments

Archive Poll

Confirm archive of Should the smaller screen be used in the SN35 Mini?

Archiving expires a poll and removes it from the active polls list.

To restore an archived poll, edit the poll, change the dates as desired, and save the poll.

Delete Poll

Confirm delete of Should the smaller screen be used in the SN35 Mini?

Warning: This will delete the poll and all of its comments.