Skip navigation

Poll: Do You Know The Scientists Who Developed Classical Electromagnetic Theory?

Classical electromagnetic theory explains how electromagnetic forces interact with charges and currents based on a Newtonian model.

 

Here's the poll question:

 

In 1820 _________ discovered that when an electric current flows in a conductor a magnetic field is produced. Less than a decade later,  ________ established the relationship between current and the magnetic field. In 1831, ________ discovered that a changing magnetic field causes current to flow in a closed electric circuit linked by a magnetic field. _________demonstrated that there is a relationship between a changing magnetic field and the induced current. ________ proved that magnetic poles cannot exist in isolation. In 1865, _______ unified electromagnetism theory in four equations that completely describe the behavior of electric and magnetic fields.

 

(If you like this quiz question, stay tuned to the element14 Quiz Series. In September, we will publish our Quiz on Inductors. This quiz question is a taste of what you will be quizzed on. As usual, if you get 100%, you will earn a secret prize.

 

Randall Scasny

element14 Quiz Maker

Poll Results
  • Ampere, Faraday, Lenz, Gauss, Oersted, Maxwell (6%)
    2/32
  • Lenz, Gauss, Oersted, Maxwell, Ampere, Faraday (3%)
    1/32
  • Oersted, Ampere, Faraday, Lenz, Gauss, Maxwell (81%)
    26/32
  • Gauss, Maxwell, Oersted, Ampere, Faraday, Lenz (0%)
    0/32
  • Faraday, Lenz, Gauss, Maxwell, Oersted, Ampere (9%)
    3/32

Comments

Archive Poll

Confirm archive of Poll: Do You Know The Scientists Who Developed Classical Electromagnetic Theory?

Archiving expires a poll and removes it from the active polls list.

To restore an archived poll, edit the poll, change the dates as desired, and save the poll.

Delete Poll

Confirm delete of Poll: Do You Know The Scientists Who Developed Classical Electromagnetic Theory?

Warning: This will delete the poll and all of its comments.