Skip navigation

Webinar Poll:  What Programming Language Do You Like to Use?

Catch the On-Demand Version of our recent LiveStream and Show & Tell with MATRIX Labs and Special Guest Raising Awesome:

 

 

Poll Results
  • C++  - You prefer this type of programming because it is a mature programming language that allows interaction with low level hardware, allowing real time performance! (10%)
    6/58
  • C -  You enjoy the purity of C without the Object-Oriented Programming, Exception Handling and the rich C++ Library. (21%)
    12/58
  • MATLAB - you enjoy using this to analyze data, produce advanced graphs or implement control systems, (2%)
    1/58
  • Python - Its good enough for Pi and like Java its an interpretive language so you don't need to see everything that is going on under the hood! (19%)
    11/58
  • Arduino - You love the ease and simplicity of Arduino and its way of making electronics accessible to all! (14%)
    8/58
  • Hardware Description Languages (HDL) -  You love FPGA and enjoy having the ability to develop electronics without having to produce a silicon chip! (3%)
    2/58
  • Assembly -  you enjoy programming at the lowest level,  1s and 0s! (2%)
    1/58
  • C#/.NET - You prefer to do most of your programming using Microsoft's proprietary language which everyone will use once Microsoft takes over everything in 10 years! (3%)
    2/58
  • Java - You prefer Java because it just works and is a lot easier to program than using C! (10%)
    6/58
  • Swift - you love something that is general-purpose, open-source, and a compiled programming language developed by Apple Inc. (0%)
    0/58
  • SQL - You love to execute queries, retrieve data, insert records, update records, delete records, create new databases, create new tables, create stored procedures, create views, and set permissions. (0%)
    0/58
  • Fortran - If its good enough for astrophysical modeling of stars and galaxies then its good enough for me. (0%)
    0/58
  • Rust - You enjoy C++ but love that this was developed to be more memory safe than C++ during runtime! (0%)
    0/58
  • Ruby - You love an open source and dynamic language that is focused on simplicity and productivity with fewer lines of code! (0%)
    0/58
  • PHP - You enjoy generating dynamic pages, collecting data from forms, sending and receiving website and/or browsing cookies, encrypting data, etc! (2%)
    1/58
  • Javascript - You love something flexible, powerful, and used everywhere from web, mobile, server, and even IoT! (9%)
    5/58
  • R - You love data mining and appreciate a wide a wide variety of statistical and graphical techniques! (0%)
    0/58
  • Erlang -  You love having the ability to use immutable data structures as well as functional programming with pattern matching support! (0%)
    0/58
  • RPG - You love IBM and getting down to business with a high level programming language. (0%)
    0/58
  • Other - Let Us Know in the Comments Below! (5%)
    3/58

Comments

Archive Poll

Confirm archive of Webinar Poll: What Programming Language Do You Like to Use?

Archiving expires a poll and removes it from the active polls list.

To restore an archived poll, edit the poll, change the dates as desired, and save the poll.

Delete Poll

Confirm delete of Webinar Poll: What Programming Language Do You Like to Use?

Warning: This will delete the poll and all of its comments.