Skip navigation

Poll: How Are You Going to Use a Pressure Sensor in Your Next Electronics Project?

In this tech spotlight (Tech Spotlight: Piezoresistive and Foil-Based Pressure Sensing Technologies) we discussed some of the basic pressure sensing technologies. We also went over the main types of pressure sensors: Absolute, Gage, Sealed Reference, Vacuum, and Differential. Sensing pressure is one of the most basic physical forces known to humankind. Pressure has been used and sensed since ancient times. The Egyptians used it to operate an automatic door opener. The ancient Romans used pressure transducers to measure flow in their aqueducts. Today, we have the technology to develop micro-sized MEMS pressure sensors and transducers, smaller than the tip of a pen. It's all pretty amazing. So here's your poll question: How Are You Going to Use a Pressure Sensor in Your Next Electronics Project? I've listed some ideas below, but you can offer your own in the comments section.

Poll Results
  • Pressure regulator (8%)
    3/40
  • Weather station (32%)
    13/40
  • Hover board steering system (2%)
    1/40
  • Air filter monitor (8%)
    3/40
  • Water pressure monitor (5%)
    2/40
  • Clog detector of an Espresso Coffee Machine (8%)
    3/40
  • Fall detector (0%)
    0/40
  • Liquid level monitor (12%)
    5/40
  • Automatic cat feeder (0%)
    0/40
  • Air or water purifier (0%)
    0/40
  • Leak detector (2%)
    1/40
  • Educational project (physics class, general science class) (5%)
    2/40
  • Other; please explain in comments (18%)
    7/40

Comments

Archive Poll

Confirm archive of Poll: How Are You Going to Use a Pressure Sensor in Your Next Electronics Project?

Archiving expires a poll and removes it from the active polls list.

To restore an archived poll, edit the poll, change the dates as desired, and save the poll.

Delete Poll

Confirm delete of Poll: How Are You Going to Use a Pressure Sensor in Your Next Electronics Project?

Warning: This will delete the poll and all of its comments.