Skip navigation

What is the maximum data rate to be achieved by an RS-485 transceiver to date?

RS-485 is a simple, inexpensive, reliable communications specification. It is a widely used protocol for POS, industrial, and telecom applications. Its wide common-mode range enables data transmission over longer cable lengths and in noisy environments such as the floor of a factory. Also, the high input impedance of the receivers allows more devices to be attached to the lines.

 

Lots of factors limit the maximum data rate of RS-485, including cable length, cable construction (shielding enhances noise immunity), driver output impedance, receiver input impedance, terminations, driver slew rate, and more.

 

Poll Question: What is the maximum data rate that has been achieved by an RS-485 transceiver to date?

Poll Results
  • 20Mbps over 50 meters of Cat6 cable (10%)
    2/20
  • 40Mbps over 100 meters of Cat5 cable (10%)
    2/20
  • 100Mbps over 10 meters of Cat5e cable (50%)
    10/20
  • 200Mbps over 50 meters of Cat6 cable (15%)
    3/20
  • Other; Please Explain in comments (15%)
    3/20

Comments

Archive Poll

Confirm archive of What is the maximum data rate to be achieved by an RS-485 transceiver to date?

Archiving expires a poll and removes it from the active polls list.

To restore an archived poll, edit the poll, change the dates as desired, and save the poll.

Delete Poll

Confirm delete of What is the maximum data rate to be achieved by an RS-485 transceiver to date?

Warning: This will delete the poll and all of its comments.