Poll: What is the most common type of temperature sensor used in medical applications?

Designing electrical and electronic systems for medical instruments, devices, or other applications have special requirements for ensure the safety, precision, and reliability. As such, they must meet rigid regulations and standards of quality. When selecting a temperature sensor for a medical application, one must examine both the essential requirements and key characteristics of the application to select the appropriate type of sensor.

 

Poll Question: What is the most common type of temperature sensor used in a medical application?

Poll Results
  • Change-of-state temperature sensors (0%)
    0/29
  • Infrared sensor (non-contact) (55%)
    16/29
  • RTD (Resistance temperature detector) (14%)
    4/29
  • Semiconductor (3%)
    1/29
  • Thermocouple (7%)
    2/29
  • Thermistor (3%)
    1/29
  • Thermometer (3%)
    1/29
  • Thermopile (0%)
    0/29
  • Other; please explain in comments (14%)
    4/29

Comments

Archive Poll

Confirm archive of Poll: What is the most common type of temperature sensor used in medical applications?

Archiving expires a poll and removes it from the active polls list.

To restore an archived poll, edit the poll, change the dates as desired, and save the poll.

Delete Poll

Confirm delete of Poll: What is the most common type of temperature sensor used in medical applications?

Warning: This will delete the poll and all of its comments.