Skip navigation

Small form-factor microcontroller board families

Which of the following board types / eco-systems do you think has the largest exposure and has been used in real projects the most?

 

This is about form factors smaller than the standard Arduino Uno format. I am thinking about new shields and want to put a second connector option on there to make it more flexible. It is going to be a display function, so I am not really interested in the higher power computer modules like RaspberryPi and such which already have video output.

 

- Wolfgang.

Poll Results
  • Arduino MKR (15%)
    4/27
  • Adafruit Feather (15%)
    4/27
  • Arduino Nano (33%)
    9/27
  • Teensy (0%)
    0/27
  • NodeMCU (11%)
    3/27
  • Wemos (0%)
    0/27
  • SparkFun Qwiic (0%)
    0/27
  • ESP 32/6288 (Do they have a common pinout/platform?) (19%)
    5/27
  • Other, the comments are all yours. (7%)
    2/27

Comments

Archive Poll

Confirm archive of Small form-factor microcontroller board families

Archiving expires a poll and removes it from the active polls list.

To restore an archived poll, edit the poll, change the dates as desired, and save the poll.

Delete Poll

Confirm delete of Small form-factor microcontroller board families

Warning: This will delete the poll and all of its comments.