Skip navigation

Poll: How Beneficial Is It To Have Sensors with Machine Learning Cores?

Machine Learning (ML) is an application of Artificial Intelligence where a machine learns by itself or under supervision, without explicit programming. The system acquires the ability to learn and progress from experience sans compromising data accuracy spontaneously. Technological advancements enable ML cores to be embedded on a chip with multiple sensors. As discussed in a recent element14 tech spotlight, Learn About Inertial Sensors with a Machine Learning Core , the ML processing capability permits the transference of several algorithms from the host processor to the sensor itself.

 

Poll Question: How Beneficial Is It To Have Sensors with Machine Learning Cores?

Poll Results
  • Extremely Beneficial (20%)
    5/25
  • Very Beneficial (16%)
    4/25
  • Interesting, but it ll depends on the use case (40%)
    10/25
  • Need to understand more about it (8%)
    2/25
  • Not sure how widespread value it will bring (16%)
    4/25
  • Other; Please Explain in comments (0%)
    0/25

Comments

Archive Poll

Confirm archive of Poll: How Beneficial Is It To Have Sensors with Machine Learning Cores?

Archiving expires a poll and removes it from the active polls list.

To restore an archived poll, edit the poll, change the dates as desired, and save the poll.

Delete Poll

Confirm delete of Poll: How Beneficial Is It To Have Sensors with Machine Learning Cores?

Warning: This will delete the poll and all of its comments.