Skip navigation

Are you Interested in Roadtesting the 96Boards ON Semiconductor Dual Camera Mezzanine?

I had a meeting this week and the new 96Boards ON Semiconductor Dual Camera Mezzanine by AVNET was being considered for a roadtest.

 

This 96Boards mezzanine card features two Polight IAScompatible imaging modules based on imaging sensors from ON Semiconductor. These sensors interface to an AP1302 imaging coprocessor. By using the 96Boards standard, this card could be easily prototyped with the Ultra96-V2 platform. This kit simplifies the complex process of developing with imaging sensors.

 

96Boards ON Semiconductor Dual Camera Mezzanine

 

MIPI-CSI2 is widely used in the consumer industry for high-speed communications from host processor to image sensors, but many image sensor modules have varying connector formats which can lead to difficulties with experimenting with different camera modules. The Imager Access System (IAS) image sensor module format from ON Semiconductor helps solve this problem and enables the following:

 

- Ease of Design-In: OEMs do not have to source lens or explore module vendors

- Decreases time to market by enabling low-touch design

- Prior imaging system expertise is not required since IAS is a plug-and-play solution

 

It works with the Ultra96-V2, so that would probably be included in this roadtest.

Ultra96 V2

 

I want to gauge the interest on the element14 community for this roadtest. Please vote below. Providing a comment on what you would do with this gear would also be helpful. Thanks. (More info by going here: 96Boards ON Semiconductor Dual Camera Mezzanine )

 

Randall Scasny

RoadTest Program Manager

Poll Results
  • Yes (65%)
    26/40
  • No (28%)
    11/40
  • Leave a Comment (8%)
    3/40

Comments

Archive Poll

Confirm archive of Are you Interested in Roadtesting the 96Boards ON Semiconductor Dual Camera Mezzanine?

Archiving expires a poll and removes it from the active polls list.

To restore an archived poll, edit the poll, change the dates as desired, and save the poll.

Delete Poll

Confirm delete of Are you Interested in Roadtesting the 96Boards ON Semiconductor Dual Camera Mezzanine?

Warning: This will delete the poll and all of its comments.