Skip navigation
> RoadTest Reviews

Review of Agilent U1272A

Scoring

Product Performed to Expectations: 10
Specifications were sufficient to design with: 10
Demo Software was of good quality: 10
Product was easy to use: 9
Support materials were available: 10
The price to performance ratio was good: 10
TotalScore: 59 / 60
  • RoadTest: Agilent U1272A
  • Evaluation Type: Independent Products
  • Was everything in the box required?: No - you would think for the price of these that they would include a case for them.
  • Comparable Products/Other parts you considered: I would compare it to fluke/case naturally.alligator clips
  • What were the biggest problems encountered?: Not really a problem, but I could not figure out how to get it to read in Fahrenheit only Celsius. But to some I guess it could be..

  • Detailed Review:

    First off thanks to all that allowed me to do this road test. Secondly this is my first ever review so I hope it's good.

    My  first impression was that this is a very nice unit, documentation good,  they give you the test results for the meter.Very informative  instruction booklet.Solid, well made, just looking at it and you can  tell that it is durable.The unit itself is a nice size,  doesn't get  lost on a workbench or fall into an engine compartment easily.

    Large  screen easy to read even from 3 feet away. And backlighting helps alot  when working late nights  running down electrical  problems on someones  vehicle.Continuity tone and other beeps are loud. Large dial and big  buttons are nice especially when wearing gloves.Leads are good and long  and the interchangeable probes are a nice touch and are easy to hold on  to. I   did not use all the functions on these meters.but what I did use  I used a lot on  a  range of things like trouble shooting home  electrical problems, home appliances,auto electrical, some circuit  testing, fuses, batteries. I even used the thermocoupler to check my  kids temp. (underarm of course)because the thermometer was broken, works  great.

    All in all for the things I used this meter for I cant  complain one bit. It is one of the best made meters I've ever used.  Worth every penny, and I would highly recommend these to someone else.


Comments

Also Enrolling

Enrollment Closes: Feb 17 
Enroll
Enrollment Closes: Feb 10 
Enroll
Enrollment Closes: Feb 11 
Enroll
Enrollment Closes: Feb 10 
Enroll