Skip navigation
> RoadTest Reviews

The Internet of Holiday Lights RoadTest Plus - Review

Scoring

Product Performed to Expectations: 10
Specifications were sufficient to design with: 9
Demo Software was of good quality: 9
Product was easy to use: 9
Support materials were available: 10
The price to performance ratio was good: 9
TotalScore: 56 / 60
  • RoadTest: The Internet of Holiday Lights RoadTest Plus
  • Buy Now
  • Evaluation Type: Independent Products
  • Was everything in the box required?: No - Infineon Shield required headers to be bought separately and soldered.
  • Comparable Products/Other parts you considered: DigiX: Arduino compatible, Wifi-enabled board.
  • What were the biggest problems encountered?: Getting started with the Infineon Shield.

  • Detailed Review:

    Review

     

    I've already shared some experiences with the kit provided over the course of the build (blog posts at the bottom), but here's a summary of the pros and cons, as I experienced them.

     

     

    Arduino UNO/YUN

     

    Arduino is great! I've had an UNO for some years now, and it is usually the first thing I grab for quick prototyping.

     

    the pin name stickers on the side of the headers are extremely useful

    wireless programming and debugging is awesome (YUN only)

    big community for a mature product, meaning lots of support and references

    a wide variety of shields is available covering the needs of most projects

    at 61 EUR the YUN is not very cheap

    the YUN's USB and ethernet port stand in the way of shields without extra long headers

    the YUN's Vin pin is not regulated meaning the input has to be 5V (as opposed to the UNO: 7-12V)

     

    I haven't used the Linux side of the YUN during my project, but it is something I will certainly explore further as I keep experimenting with the YUN.

     

     

    Infineon RGB Shield

     

    The Infineon RGB Shield is hard to get started with, but once set up, it functions very well!

     

    very practical push terminals to connect the LED strip and power, no screwdriver required

    wide input voltage range (12-48V)

    lots of software configurable parameters

    price point is acceptable at 24 EUR taking into account current "issues"

    no headers are provided with the kit, requiring the need to buy some separately and have the end user own a soldering iron (not plug-and-play)

    no Arduino library available and code examples on the Infineon website are Windows-only (*.exe files)

     

    I feel the user experience could greatly be improved by tackling some of the above points with following actions:

    • - a pair of stackable headers could be included in the kit, preferably soldered
    • - an official library should be made available, facilitating quick prototyping
    • - provide the example files in an OS independent format such as *.zip

     

     

    Project

     

    Here you will find the blog posts created as part of this RoadTest, in which I get to know and use both the Arduino Yun and the Infineon Shield combined with some LED strips.

     

    DSCN3182.JPGDSCN3180.JPGDSCN3186.JPGDSCN3188.JPG


Comments

Also Enrolling

Enrollment Closes: Aug 18 
Enroll
Enrollment Closes: Jul 13 
Enroll
Enrollment Closes: Aug 7 
Enroll
Enrollment Closes: Jul 14 
Enroll
Enrollment Closes: Jul 28 
Enroll
Enrollment Closes: Jul 20 
Enroll
Enrollment Closes: Jul 17 
Enroll