Skip navigation
> RoadTest Reviews

RoadTest the ADS7042 BoosterPack and MSP430FR4133 - Review

Scoring

Product Performed to Expectations: 9
Specifications were sufficient to design with: 9
Demo Software was of good quality: 10
Product was easy to use: 10
Support materials were available: 10
The price to performance ratio was good: 10
TotalScore: 58 / 60
  • RoadTest: RoadTest the ADS7042 BoosterPack and MSP430FR4133
  • Buy Now
  • Evaluation Type: Independent Products
  • Was everything in the box required?: Yes - No difficulties
  • Comparable Products/Other parts you considered: Considered low power micro-controlles from Microchip
  • What were the biggest problems encountered?: Integrating the ADC of ADS7042 along with the pFatFs library in LPM3.5 mode so that ADC and SD-Card write could function simultaneously in the active period and be inactive during sleep in LPM3.5. and achieving the lowest power consumption.

  • Detailed Review:

    It was a privilege and pleasure to conduct this RoadTest. I decided to build a practical application in order to exhaustively check out the features of the combination of the MSP-EXP430FR4133 LaunchPad development kit and the ADS7042 Ultra-Low Power Data Acquisition BoosterPack.

     

    The full development details are available at: Full Development Details

     

    1.  Project title: Anemometer and Wind-Vane Wind-Speed and Direction Logger

    001_Anemometer.jpg

    2. Project brief: A stand-alone unit operating from three AA batteries which is capable of measuring and logging wind-speed and wind-direction on a SD-card for a period of one year at intervals of 5 minutes or less with simultaneous display of interval-count, speed and direction on the LCD.

     

    Using DIY hardware wind-speed is sensed by a cup-anemometer driving a small dc-motor acting as a dc-generator with output is in the range 0 to 300 mV. Wind-direction is sensed by a wind-vane which drives a one-wire potentiometer with a resistance range 0 to 24 kilo Ohm.

     

    After signal-conditioning wind-speed is A/D converted by the ADS7042 and the wind-direction is A/D converted by one of the ADC channels of the MSP430FR4133. To achieve the lowest standby current the MSP430FR4133 is operated in LPM3.5 mode and the circuitry required for signal-conditioning, A/D conversion and writing to SD-card are switched ON only during the desired measurement interval.

     

    An ‘Anemometer Booster Pack’ incorporating all additional circuitry and SD-card is specially designed and integrated below the MSP430FR4133 LaunchPad development kit while the ADS7042 BoosterPack with minor modifications is fixed above.

    004_Assembly.jpg

    3.  Observations:

     

    3.1. The OutOfBox_MSP430FR4133 example software compiled and ran without difficulty on CCS Cloud in ‘c’.

    3.2. Following the Ti instructions and imported the BOOST-ADS7042_Firmware.ino file into CCS Cloud. It compiled and ran without any difficulty using Energia.

    3.3. Three different methods for programming the MSP430FR4133 worked successfully:

    3.3.1. Using FET-Pro430-Lite-3v41

    3.3.2. Using the command line Flasher MSPFlasher.exe

    3.3.3. Using the Cloud Based Flasher 'UniFlash'

    3.4. After working with CCS-Cloud, CCS-6 and Energia-18 application development was continued in Energia-18 primarily because of ease in incorporating the Petit FatFS SD Card Library

    3.5. Three modifications were carried out on the ADS7042 booster pack:

    3.5.1. First the 3.3V line to the power LED (Green) before R34 was cut in order to reduce the card current drain of the LED.

    3.5.2. Second the 3.3V line from the 3.3V tag to the SMD fuse F1 was cut and an additional wire connected at the input end of F1. This permits switching power to the booster pack as required.

    3.5.3. An additional wire was connected at JP1 pin 2 for feeding the signal to be A/D converted instead of using the SMA connector for input.

     
      005_BP_Mods.jpg

    3.6. Software development was carried out in stages. There was no difficulty in checking the LCD, ADC of MSP430FR4133, ADC of ADS7042 and the SD-card functions individually. Inconstancy was noticed when the ADS7042 and the SD-card functions were used together in LPM 3.5 mode.

    The Energia-18 compiler gave inconsistent results when the SPI function from the example program for ADS7042 and the pfatfs functions were used together. Apparently the SPI function defined in pfatfs affects the SPI code defined for the ADS7042.

    This problem was overcome by calling the ADS7042 ADC function during the period when pfatfs was open. However the combination of the ADC result MSB and LSB had to be modified to get the correct value.

     

    3.7. A switching scheme was devised whereby the supply 3.3V to the booster pack and the ground to the SD-card could be selected by software control. In      LPM 3.5 mode the standby current measured was 0.01mA and the maximum current drawn was ~30mA during SD-card write.

     

    As the Vref on ADS7042 booster pack has been chosen as 3.0V the supply required is 3.3V. This required three AA batteries and an external 3.3V regulator. The very low quiescent LDO Ti LM2936 was chosen for this.

     

    With this LDO supplying 3.3V to the integrated set-up from an input of 4.5V the detailed current profile was measured to be 0.03mA when in sleep during LPM 3.5 and 38 for 0.5 sec during SD-card write, 22mA for .2 sec during SD-card close and another 1.5 mA for 1.7 sec during the active period.  This totals to 25.95 mAsec for the active period of 2.4 sec.

     

    Considering a write interval of 5 min the estimate of power drawn for 1 year would be: (25.95 mAsec (active) + 8.93 mAsec (sleep)) x 12 x 24 x 365 = 3666585.6 mAsec or 1018.496 mAH. Alkaline AA batteries with 1.2AH capacity should theoretically meet the one year requirement.

     

    4.      Results

     

    4.1. A quick evaluation was carried out on the A/D converters of the ADS7042 and MSP430FR4133 the results are show below:

     

     

    Full RangeLow Range

    ADC Channels of MSP430FR4133 and ADS7042

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

          4.2  Current Profile in LPM 3.5 update every 16 seconds

     

    16 Seconds mode for checking current consumptionExpanded SD-Card portion

     

          4.3. Typical log file output 1 minute update

     

    Day 006   01:25   009 km/hr   061  deg

    Day 006   01:26   009 km/hr   062  deg

    Day 006   01:27   009 km/hr   046  deg

    Day 006   01:28   009 km/hr   094  deg

    Day 006   01:29   016 km/hr   093  deg

    Day 006   01:30   016 km/hr   092  deg

    Day 006   01:31   016 km/hr   093  deg

    Day 006   01:32   016 km/hr   093  deg

    Day 006   01:33   016 km/hr   080  deg

    Day 006   01:34   016 km/hr   343  deg

    Day 006   01:35   016 km/hr   343  deg

    Day 006   01:36   016 km/hr   343  deg

    Day 006   01:37   030 km/hr   342  deg

    Day 006   01:38   030 km/hr   341  deg

    Day 006   01:39   030 km/hr   295  deg

     

    5.    Project Details:

          5.1. DIY Anemometer and Vane

    The Anemometer was built from repurposed parts. This includes a novel method of creating a one-wire potentiometer using a commutator-brush assembly from an old universal-motor and a DC motor from an old CD-ROM drive.

     

    The wind-direction sensor is based on the commutator which is removed from the old motor assembly. With a hole drilled through the shaft and then 24 1kOhm resistors soldered between commutator segments and one end connected to the shaft. This creates a 24kOhm variable resistor between the brush and grounded shaft which can be used to determine angular position of the wind-direction.

     

    The cup- anemometer is built using plastic balls which have been cut in half and fixed to a central hub using tapped aluminum rods cut from an old clothes-hanger. A small DC motor is driven by the rotating cup-assembly by a thin shaft which passes through the commutator shaft.

     

    This creates a novel concentric assembly integrating anemometer wind-speed measurement using a dc-motor as a generator and commutator variable-resistance as a wind-direction sensor.

     

    Using a simple method the anemometer was calibrated against wind-speed by fixing the assembly on a motor-cycle and noting the values of DC-voltage generated by the small-motor against speed measured on the motor-cycle speedometer.

     

    The images below illustrate the steps in building the DIY anemometer wind-sensor:

     

    Old Motor Assembly

    Disassembled Commutator

    Hole in commutator shaft

     

     

    Commutator  and DC-motor assembly

    Anemometer parts required

    Wind-speed calibration

    1 kilo Ohm resistors

    Final assembly

     

    5.2. Electronics

    An ‘Anemometer Booster pack’ was designed and fabricated so as to integrate with the the MSP-EXP430FR4133 LaunchPad development kit and the ADS7042 Ultra-Low Power Data Acquisition BoosterPack. The circuit implements the following:

     

              5.2.1. 3.3V LDO based on the TI LM2936        

     

    5.2.2. Switched current source for driving one-wire-resistor (commutator with 24, 1 kilo Ohm resistors)

     

    5.2.3. Amplification of the anemometer sensor output (DC-motor output)

     

    5.2.4.   Switchable power to the  ADS7042 BoosterPack

     

    5.2.5. Switchable ground to the SD-card

     

    5.2.6 Circuit Schematic:

     

     

     

    5.2.7. Circuit PCB artwork

     

     

      PCB TOP

    PCB BOTTOM

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

    5.2.8. Circuit PCB hardware

     

     

     

    6.     Software Code Listing

    /* --COPYRIGHT--,BSD

       Uses example code provided by  Texas Instruments

       Copyright (c) 2014, Texas Instruments Incorporated

       All rights reserved.

     

       Arduino Wrapper Function Library for FatFs

       (c) 2010, David Sirkin sirkin@stanford.edu

     

       FatFS by ChaN:

    http://elm-chan.org/fsw/ff/00index_e.html

      --/COPYRIGHT--*/

     

    //******************************************************************************

    //

    //   Road Test on the MSP-EXP430FR4133 LaunchPad development kit and

    //   the ADS7042 Ultra-Low Power Data Acquisition BoosterPack.

    //

    //   MSP430FR4133 Anemometer Code - LPM3.5, device enter LPM3.5 every 5 minutes

    //   and captures the value of wind-speed and direction which are stored

    //   on an SD-Card

    //

    //   Description: Device enter LPM3.5 after configuring the RTC. The RTC wakes

    //   the device up from LPM3.5 every 5 minutes and increments a counter.

    //   It stores the values of counter, Day, Hour and Min in the Backup RAM Registers.

    //

    //   It integrates the TI ADS7042 BoosterPack and  DIY Anemometer BoosterPack

    //

    //  Wind-speed output ofer signal conditioning is fed to Pin8.0 of MSP430FR4133

    //  Wind-direction output after signal-conditioning is fed to the ADC of ADS7042

    //

    //  Ajoy Raman

    //  Freelance Engineer

    //  www.ajoyraman.in

    //  January 2017

    //  Built with energia-1.6.10E18

    //******************************************************************************

    #include <SPI.h>

    #include <LCD_Launchpad.h>

     

    #include <pfatfs.h>

    #include <pffconf.h>

     

    #include <msp430.h>

     

     

    #define sd_card_cs_pin 9           // SD-Card chip select pin

    //#define booster_pack_cs_pin 12        // ADS7042 Booster pack chip select pin

    #define extAIN      6           // BoosterPack A_IN Pin8.0

    LCD_LAUNCHPAD LCD;

     

    volatile unsigned int *myCount = &BAKMEM0; //memory location myCount

    volatile unsigned int *Days = &BAKMEM1; //memory location day

    volatile unsigned char *Hours = &BAKMEM2_L; //memory location hour

    volatile unsigned char *Minutes = &BAKMEM2_H; //memory location minute

    unsigned short int bw;//bytes written

    int rc;  // relates to the status of the file operation

    DIR dir;                /* Directory object */

    FILINFO fno;            /* File information object */

     

    uint32_t ReadTemp;

    uint32_t ReadTemp1;

    uint8_t StringLength = 0, StringLength1 = 0;

    char buf[60];

    volatile uint32_t counter = 0;

    uint32_t AccStringLength = 0;

     

    uint16_t ADCresult; // ADC result of Booster-pack ADC

    uint32_t ADCresult1;

    uint8_t RXMSB, RXLSB; //Rx MSB, Rx LSB results of Booster-pack ADC

    uint8_t Day, Hour, Min, Speed;

     

    void setup()  //Does setup() and then goes to loop()

    {

     

      WDTCTL = WDTPW | WDTHOLD;   // Stop WDT

      FRCTL0 = FRCTLPW | NWAITS_1;

      // Set FRAM wait states, necessary for MCLK > 8

     

      initGpio();

      setup32kHzOsc();

      setupClock(); //16MHz

      setupSPI();   //required when we add ADS7402

      LCD.init();   // Initialize the LCD

      setupUART();  // initialize the serial terminal

      analogReference(DEFAULT);

      __delay_cycles(1600000);

     

    }

     

    /*-----------------------------------------------------------------------*/

    /* Program Main */

    /*-----------------------------------------------------------------------*/

    void loop()

    {

     

      // First determine whether we are coming out of an LPMx.5 or a regular RESET.

      if (SYSRSTIV == SYSRSTIV_LPM5WU)  {

        // When woken up from LPM3.5, reinitialize

        //update time variables for print

        Day = *Days;

        Hour = *Hours;

        Min = *Minutes;

        counter = * myCount;//restore counter value from memory

     

     

        // At this time both Current-Source and Booster-Pack power is ON

        // Read AIN on MSP430FR4133

        __delay_cycles(1600000);

        ReadTemp = analogRead(extAIN); //first reading may be in error

        __delay_cycles(1600000);

        ReadTemp = analogRead(extAIN);

        __delay_cycles(1600000);

     

        sprintf( buf, "x%05X  ", counter);

        LCD.displayText(buf);

     

     

        //---------------Writing to SD-Card

        // carry out the ADS7042 reads during this time as it works

        //only within pfatfs when pfatfs is used

     

        P8OUT |= BIT3;//SD Card GND ON

     

     

        __delay_cycles(1600000);

        //Serial.println("FatFs.begining");

        FatFs.begin(sd_card_cs_pin);      // initialize FatFS library calls

        //Serial.println("FatFs.opening");

        //"Opening log file to write temperature(LOG.txt)."

        __delay_cycles(1600000);

        rc = FatFs.open("LOG.TXT");

        if (rc) die(rc);

        __delay_cycles(1600000);

        //Serial.println("FatFs.open");

     

        //Read ADS7042 values

        Read_ADS7042_ADC();//first reading may be in error

        __delay_cycles(1600000);

     

        Read_ADS7042_ADC();

        __delay_cycles(1600000);

     

        Read_ADS7042_ADC();

        __delay_cycles(1600000);

        //send_BP_ADC_result();

     

     

        P1OUT |= BIT3; //Switch off afer ADC Conversion OFF

        P5OUT |= BIT0; //Current source ckt OFF

     

        ReadTemp = ReadTemp * 3600 / 687;

        ReadTemp1 = ReadTemp / 10;

     

        ADCresult1 = ADCresult;

        ADCresult1 = (ADCresult1 * 6000) / 1872;//2080; //~ 64/256 >>2

        ADCresult1 = ADCresult1 / 100;

        ADCresult  = ADCresult1;

     

     

        sprintf( buf, "%02d %03d", ADCresult, ReadTemp1);

        LCD.displayText(buf);

     

     

        sprintf( buf, "Day %03d %02d:%02d   %03d  km/hr %03d  deg ",

                 Day , Hour, Min, ADCresult, ReadTemp1 );

        Serial.println(buf);   // write to uart

     

        __delay_cycles(1600000);

     

        bw = 0;

     

        StringLength =  strlen(buf); //required for SD Card file write

     

        //SD Card open write and close file

        AccStringLength =  (counter - 1) * 512;

        //FAT format writes are in blocks of 512

        rc = FatFs.lseek(  AccStringLength );

        //moves to the position where we should write

        if (rc) die(rc);

        rc = FatFs.write(buf, StringLength, &bw);

        //write contents of buf with length StringLength

        if (rc) die(rc);

        rc = FatFs.write(0, 0, &bw);  //Finalize write

        if (rc) die(rc);

        rc = FatFs.close();  //Close file

        if (rc) die(rc);

     

        Serial.println("File Closed");

     

        P8OUT &= ~ BIT3; //SD card off

     

        // -- end of SD-Card write -------------------------------

     

        // Store counter value in backup memory register before enter LPM3.5

        * myCount = counter;

        incrementTime(); //increment day hour minute count

     

        __enable_interrupt();    // The RTC interrupt should trigger now...

      }

      else   {

     

        *Minutes = 0; // Set initial time

        *Hours = 0;

        *Days = 1;

        // Configure RTC

        // Initialize RTC to use XT1 and enable RTC interrupt

        // Interrupt and reset happen every 1024/32768 * 32 = 1 sec.

        RTCMOD =  9600 - 1; //300 sec

        //RTCMOD =   512 - 1; //16 sec

        //RTCMOD = 32-1; //1 sec

        RTCCTL = RTCSS__XT1CLK | RTCSR | RTCPS__1024;

        RTCCTL |= RTCIE;

     

        // Store counter value in backup memory register before enter LPM3.5

        counter = 0;

        * myCount = counter;

     

        //print opening message

        LCD.displayText("AJ RDT ");

        Serial.print("MSPFR4311 Anemometer Logger Starting \n\r");

        __delay_cycles(1600000);

      }

     

      // Enter LPM3.5 mode with interrupts enabled. Note that this operation does

      // not return. The LPM3.5 will exit through a RESET event, resulting in a

      // re-start of the code.

      PMMCTL0_H = PMMPW_H;                    // Open PMM Registers for write

      PMMCTL0_L |= PMMREGOFF_L;               // and set PMMREGOFF

      __bis_SR_register(LPM3_bits | GIE);     // Re-enter LPM3.5

      __no_operation();                       // For debugger

     

    }

     

    //ISR

    void __attribute__ ((interrupt(RTC_VECTOR))) RTC_ISR (void) {

      switch (RTCIV)

      {

        case (0) : break;//No Interrupt

        case (2) :      // RTC Overflow

          counter = * myCount;

          P4OUT |= BIT0; //for debug

          counter++;

          // Store check value in backup memory register

          * myCount = counter;

     

          break;

        default:          break;

      }

    }

     

     

    /* Stop with dying message */

    void die ( int pff_err  )

    {

      Serial.println();

      Serial.print("Failed with rc=");

      Serial.print(pff_err, DEC);

      for (;;) ;  //infinite loop

    }

     

    void initGpio(void)

    {

      P1DIR = 0xFF; P2DIR = 0xFF; P3DIR = 0xFF; P4DIR = 0xFF;

      P5DIR = 0xFF; P6DIR = 0xFF; P7DIR = 0xFF; P8DIR = 0xFF;

      P1REN = 0xFF; P2REN = 0xFF; P3REN = 0xFF; P4REN = 0xFF;

      P5REN = 0xFF; P6REN = 0xFF; P7REN = 0xFF; P8REN = 0xFF;

      P1OUT = 0x00; P2OUT = 0x00; P3OUT = 0x00; P4OUT = 0x00;

      P5OUT = 0x00; P6OUT = 0x00; P7OUT = 0x00; P8OUT = 0x00;

     

      // All are defined as outputs and LOW

     

      //Booster Pack LED1 & LED2 off as invered logic

      P2OUT |= BIT7;      // LED1

      P1OUT |= BIT5;      // LED2

     

      //Used to control the ground line to SD Card

      P8DIR |= BIT3;

      P8OUT &= ~ BIT3; //OFF

     

      //Used to control the Booster pack LDO

      P2DIR |= BIT5;

      P2OUT &= ~ BIT5; //OFF

     

      //Ext ADCIN input

      P8DIR &= ~ BIT0; //Configured as input

     

      //Used to give power to the ADS7042 Booster Pack

      P1DIR |=  BIT3;//Configured as output

      //drives base of NPN transistor power ON when Low

      P1OUT &= ~ BIT3; //ON

      //P1OUT |= BIT3; //OFF

     

      //Used to give power to the Current source circuit

      P5DIR |=  BIT0;//Configured as output

      //drives base of NPN transistor power ON when Low

      P5OUT &= ~ BIT0; //ON

     

      // Disable the GPIO power-on default high-impedance mode

      PM5CTL0 &= ~LOCKLPM5;// to activate previously configured port settings

    }

    void setupClock() {

      // Set MCLK = SMCLK = DCOCLKDIV = 16 MHz

      // Set ACLK = REF0CLK = ~32 kHz

      __bis_SR_register(SCG0);            // disable FLL

      CSCTL3 |= SELREF__REFOCLK;          // Set REFO as FLL reference source

      CSCTL0 = 0; // clear DCO and MOD registers

      CSCTL1 &= ~(DCORSEL_7);             // Clear DCO frequency select bits first

      CSCTL1 |= DCORSEL_5;                // Set DCO = 16MHz

      CSCTL2 = FLLD_0 + 487;              // DCOCLKDIV = 16MHz

      __delay_cycles(3);

      __bic_SR_register(SCG0);                       // enable FLL

      while (CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1));    // FLL locked

     

      CSCTL4 |= SELMS__DCOCLKDIV | SELA__REFOCLK;

      // set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz

      // default DCOCLKDIV as MCLK and SMCLK source

    }

    void setup32kHzOsc() {

      // Initialize XT1 32kHz crystal

      P4SEL0 |= BIT1 | BIT2;                  // set XT1 pin as second function

      do

      {

        CSCTL7 &= ~(XT1OFFG | DCOFFG);      // Clear XT1 and DCO fault flag

        SFRIFG1 &= ~OFIFG;

      } while (SFRIFG1 & OFIFG);              // Test oscillator fault flag

    }

    void setupUART() {

      //--------------------------- Configure UART pins -----------------------------------------------------

      P1SEL0 |= BIT0 | BIT1;    // I/O Function Selection

     

      // Configure UART for backchannel UART data logging

      UCA0CTLW0 |= UCSWRST;

      UCA0CTLW0 |= UCSSEL__SMCLK;

     

      // Baud Rate calculation 9600 Baud ------------------------ 9600 Baud ------------------------------

      // 16000000/(16*9600) = 104.167

      // Fractional portion = 0.167

      // User's Guide Table 14-4: UCBRSx = 0xD6

      // UCBRFx = int ( (104.167-104)*16) = 2

      UCA0BR0 = 104;                                 // 16000000/16/9600

      UCA0BR1 = 0x00;

      UCA0MCTLW = 0xD600 | UCOS16 | UCBRF_2;

     

      UCA0CTLW0 &= ~UCSWRST;             // Initialize eUSCI (Enhanced Universal Serial Communication Interface)

    }

    void setupSPI() {

      // Initialize SPI for 4 MHz SCLK, used to communicate with the ADS7042

      //pinMode( booster_pack_cs_pin, OUTPUT);

      P5SEL0 |= BIT1 | BIT2 | BIT3;                  // select secondary mode for pins

      UCB0CTLW0 |= UCSWRST;                          // **Put state machine in reset**

      UCB0CTLW0 |= UCMST | UCSYNC | UCMSB | UC7BIT;  // 3-pin, 8-bit SPI master

      UCB0CTLW0 |= UCSSEL__SMCLK;                    // MODCLK

      UCB0BR0 = 4;                                   // /2,fBitClock = fBRCLK/(UCBRx+1).

      UCB0BR1 = 0;                                   //

      UCB0CTLW0 &= ~UCSWRST;                         // **Initialize USCI state machine

    }

    // Routine reads values from booster pack ADC

    void Read_ADS7042_ADC()

    {

      P1OUT &= ~BIT4;                       // PIN 12 Drive CS pin low to begin SPI communication

      //P1.4 directly  could have used CS #define CS 12

      __delay_cycles(160000);

      UCB0TXBUF = 0x00; // Send empty byte to ADS7042

      while (!(UCB0IFG & UCRXIFG));         // Wait for RXBUF to receive byte

      RXMSB = UCB0RXBUF;                    // Place byte in RXMSB

     

      UCB0TXBUF = 0x00; // Send empty byte to ADS7042

      while (!(UCB0IFG & UCRXIFG));         // Wait for RXBUF to receive byte

      RXLSB = UCB0RXBUF;                    // Place byte in RXLSB

      P1OUT |= BIT4;         // Return CS pin high, done with ADS7042 SPI for now

      //ADCresult = (RXMSB << 7) | RXLSB; //TI exapmle program

      ADCresult = (RXMSB << 6) | (RXLSB >> 2);//Changed to work with pFatFs SPI

      //ADCresult &= 0x00FF; //kills any 1's in result above 12bit

     

    }

    // Time Function

    void incrementTime(void)

    {

      // Deal with minutes increment every interrupt at 5 minute interval

      //(*Minutes) = (++(*Minutes) % 60); //60

      (*Minutes) = ( ((*Minutes)+5) % 60); //60

      if ((*Minutes) == 0)

      {

        (*Hours) = (++(*Hours) % 24); //24

     

        if ((*Hours) == 0)

          (*Days)++;

      }

    }

     

    // -----------------Used during development for debug-----------------

     

    void send_BP_ADC_result() {

      //------------Send Booster Pack ADC result on back channel----------------------

      ADCresult = (RXMSB << 7) | RXLSB;     // Send ADS7042 result via backchannel UART

      ADCresult &= 0x0FFF; //kills any 1's in result above 12bit

      //sendASCII((ADCresult >> 12));       // Send upper most nibble

      sendASCII((ADCresult >> 8));          // Send upper nibble

      sendASCII((ADCresult >> 4));          // Send middle nibble

      sendASCII(ADCresult);                 // Send lower nibble

      while (!(UCA0IFG & UCTXIFG)); UCA0TXBUF = 10;  // End line

    }

    void send_LP_ADC_result() {

      //------------Send Launch pad ADC result on back channel----------------------

      sendASCII((ReadTemp >> 8)); // Send upper nibble

      sendASCII((ReadTemp >> 4)); // Send middle nibble

      sendASCII(ReadTemp );                             // Send lower nibble

      while (!(UCA0IFG & UCTXIFG)); UCA0TXBUF = 10;     // End of line character

    }

    // Hex to ASCII sendASCII subfunction

    // takes a hex value and turns it into its ASCII representation

    // then sends the number to the host via backchannel UART

    void sendASCII(int hexvalue)

    {

      hexvalue &= 0x000F;

      if (hexvalue <= 9) {

        while (!(UCA0IFG & UCTXIFG));

        UCA0TXBUF = hexvalue + 48;

      }

      else if (hexvalue <= 15) {

        while (!(UCA0IFG & UCTXIFG));

        UCA0TXBUF = hexvalue + 55;

      }

    }

     

    7.  Summary

     

    It was an great learning experience to carry out this RoadTest. I was able to work with all the IDE tools provided by TI including the CCS Cloud and CCS6 downloaded to my PC. The example and demo programs formed an excellent starting point for software development. The low power modes were fully exploited and it was impressive to see only 100uA in LPM3.5 which increased to only 300uA when the low quiescent current LDO was added. The major current contributor in the active period within LPM 3.5 is the SD-Card which needs 30mA for write operations.Integrating the SD-Card pFatFs library was a major challenge and some interaction was noticed with the SPI c-code of the ADS7042.   A work around was found for this. I worked mostly in the Energia-18 work-space as I found it easy to integrate the library functions of Energia with the other c-routines which needed to be added. The hardware provide has been very stable over several programming cycles.

     

    Finally I must acknowledge TI and Element-14 for giving me an opportunity to carry out this RoadTest.


Comments

Also Enrolling
Enrollment Closes: Oct 22 
Enroll
Enrollment Closes: Oct 12 
Enroll
Enrollment Closes: Oct 9 
Enroll
Enrollment Closes: Oct 1 
Enroll
Enrollment Closes: Oct 15 
Enroll
Enrollment Closes: Oct 8 
Enroll
Enrollment Closes: Sep 27 
Enroll