Skip navigation
> RoadTest Reviews

Autodesk EAGLE PCB Design Software, Premium (1yr) - Review

Scoring

Product Performed to Expectations: 7
Specifications were sufficient to design with: 10
Demo Software was of good quality: 8
Product was easy to use: 10
Support materials were available: 10
The price to performance ratio was good: 7
TotalScore: 52 / 60
  • RoadTest: Autodesk EAGLE PCB Design Software, Premium (1yr)
  • Buy Now
  • Evaluation Type: Independent Products
  • Was everything in the box required?: Yes
  • Comparable Products/Other parts you considered: This is part one of the Eagle Road Test - (Auto)Router
  • What were the biggest problems encountered?: software crash, exception error, on starting routing

  • Detailed Review:

    Dear Randall,
    Dear suppliers,

     

     

    Thank you very much for selecting me, that I can participate to the Autodesk Eagle Road Test.

     

    Preface:
    Why do I write here the first review and as far as exclusively about the router?
    Actually, because it caused a crash of the software, and that has happened several times.

    I think in this review absolutely positive and it is NO criticism in the sense of "These are many errors".
    No, yes, I am a service engineer and a developer and understand the hard work of developers and testers of this excellent product.

    But, I think the correct function of the router can be a purchase decision, it is probably also the most complex function module.
    Above all, the software can not crash completely here.

    It is interesting, as far as I have an overview, all similar products have probably the same quality characteristics.
    The Schematic Editor works as good as always up to 100%.
    The PCB editor without the router is similar, but here is the great complexity, up to 95%.
    The router, in what makes, or qualities, it reaches my view so 70 - 80%.
    And most of all, where problems were, the component management is with the library module.

    "If the router works without crash, then I buy the product"; So are many statements of marketing during the shopping negotiations.
    Although the quality of my experience is never 100%.

    In this sense - EAGLE - a "easy-to-use graphic layout editor" is a great tool, which now comes out of the children's shoes.

     

    Best Regards

    Gerald

    --------

     

    Eagle is a very fine tool which you can build your schematic diagrams also the layout for the PCB.
    I like to work with it because this is an easy to use tool.

     

    -> Firstly I tested the Autorouter also manual routing. I think that is the most important function module; yes of coarse the module schematic editor.


    The schematic editor works as expected also basically the router and also the library.
    Eagle comes also with the help file, eagle manual also with a fine tutorial so that you can easy learning the steps from the schematic to the layout and also for the fabrication.

    / -> The help file have many old information, e.g. types of Eagle packages which are obsolete. Please actualize it. Thank you.

     

    In this meaning, in the Road Test, I'll not rolling out the basic functions of the software tools - I would say there are three tools:
    Schematic, PCB, Autorouter; a fourth module can be the Library but it comes with sch or with pcb.

    In this first part of the review I've tested the most important tool (for me) - the (auto)router.
    For this I just created a test board with the most used devices, standard also special devices.
    In the library I created a simple part, a 7 segment display (I've drawn it with help lines).

     

    1.) Schematic diagram:
    Basically the schematic was working as excepted.

    Without the new functions there was no problem (e.g. module, design block).
    In the sch are basic parts also special parts e.g. one with an FPBGA with 256 pins (fine pitch BGA).

    Then I inserted a simple Design block, a module.
    e.g. this simple module have a µC and its board to board connectors, like as a "test socket".

     

    test-sch1.pngtest-sch2.png

     

    test-sch4.png

     

    2.) The PCB:

    The dimension with the two modules.

    At the area around the standard parts I routed manually. This was done with the Eagle V8.0.

    During Road Test I used the Eagle V8.1.1.

    The FPBGA was routed with BGA routing - it worked as expected but before starting it there is needing to check the design rules.

     

    The most important with this I would say is the right routing grid.

    And in that meaning, setting the right grid also routing grid is necessary for error free routing.

     

    -> Here, I would suggest, if it possible to get a flexible grid schematic.
    e.g. often I use a 50mil grid for standard parts but the FPBGA needs a 0.1mil grid.

    So I would like use one dimension area with separating the both routing islands the two routing grids.
    Like in this demo PCB - at the top the standard parts have a 50mil grid and around the FPBGA because it was created with decimal dimension have a decimal grid with e.g. 0.001mm.

     

    Flexible grids would be also fine for creating the devices in the library.
    I created a 7 segment display to showing what i mean. The grid here is 1mic the helplines are horizontal, vertical and in angles e.g. for that display character.

    But the grid for the pins are in 100mil.

     

    test-sch010.png

     

    - routing -

    The track from IC4 to IC3 was made with pair routing.
    It works but it was tricky connecting at the ends to the pads.

    Here I would suggest that pair routing needs more flexibility also flexible editing the parameters. The best of this seems interactive changing the parameters during routing with the mouse buttons.

    Also pair routing starting form both ends going to the middle of the track (as the manual mentioned) can have problems.

    If there some corners, calculating errors or rounding errors can appear, then it may loosing the routing grid so that the tracks would not overlap 100% to each other.

     

    test-pcb1.png

    Around the IC3 to RN1 (resister network) routing was made with auto routing. Also the second module IC101 was made with auto routing.

    This module does not need Via - ok, it seems the setting of the routing rules needs a bit finer.

     

    ! Well, now it comes what i didn't thought about.

     

    ! Crashing the complete Eagle software.

    Really? - yes.

    Here there are some videos, Autorouter, manual routing.

    In the first video i also tried editing the port properties; it not works - there are no buttons or checkboxes nor editable text fields.

    If some missing during creating the modules and its ports in the schematic there is no possible to edit the properties. - Eagle V8.1.1

    2nd, 3rd scene the Autorouter: Routing grid also grid of the dimension!!! -

    !! First, in the grid setting I switched to the finest grid.

    test-sch005.png

    Then you can route the tracks. If not, setting in the routing rules may crash the software.

    It seems there is a bug.

     

     

    The problem exist also in manual routing. - It seems that the function "walkaround obstacle" have a problem.

    Or the problem lies in routing the two modules at the same time or in same routing dimension.

     

    // Oh, during writing this review, Eagle liked to upgrade to the V8.2.0.

    So, the Eagle V8.1.1 will now not more used for this Road Test, Part 2.

    I'll then use V8.2.0 for the next test.

     

    The last but not least I used manual routing the 8 tracks.

    Here, the "walkaround obstacles" was no problem, also the function interactive switching the layers worked.

    Once I asked here in Eagle support forum (i used Eagle V8.1.0): https://www.element14.com/community/message/218479/l/v-810-obstacle-does-it-functioning-right#218479

     

     

    Conclusion:

    If the corresponding settings are made at the beginning, the setting of the grid is important, then the router is a valuable aid in the development of the board.

    I have entered the PCB settings of my PCB manufacturer for the Design Rules and routed the board with this.
    My favorite: www.pcb-pool.com with whom I work for many years.

    Of course, here I bring the other great features of Eagle in the review. But this description above was now to be done quickly.

     

    Installing new versions of Eagle:

    As mentioned today I received the new version of Eagle, V8.2.0.

    The installing was easy.

    But, the folders where there the new software versions are, are being now very much on the hard disc.

    test-sch011.png

    And all of them have the same content in the folders.

    I think it would better that the exe files may installed as overwriting.

    For the lib files I use a separate hard disc, on there the projects are stored.

    In the Eagle Panel, / options / folders - there are registered the project folders, exe folders also the lib folders.

    This can be used during installing the new Eagle versions, so that the lib can be overwriting too.


    A word about Autodesk Support:
    Thanks to Autodesk Support, thanks to Randall for getting the permission for Eagle relatively quickly.
    I see this so that there are two shoes, the support here for the road test and the support for the purchased licenses.
    There were countries or continent-related misunderstandings.

     

    Thank you very much.

    Best Regards,

    Gerald

    ----


Comments

Also Enrolling
Enrollment Closes: Jun 29 
Enroll
Enrollment Closes: Jul 23 
Enroll
Enrollment Closes: Jun 29 
Enroll
Enrollment Closes: Jul 20 
Enroll
Enrollment Closes: Jul 9 
Enroll
Enrollment Closes: Jun 30 
Enroll