Skip navigation
> RoadTest Reviews

Microchip AVR-IoT WG Dev Board - Review

Scoring

Product Performed to Expectations: 7
Specifications were sufficient to design with: 8
Demo Software was of good quality: 7
Product was easy to use: 6
Support materials were available: 7
The price to performance ratio was good: 3
TotalScore: 38 / 60
  • RoadTest: Microchip AVR-IoT WG Dev Board
  • Buy Now
  • Evaluation Type: Development Boards & Tools
  • Was everything in the box required?: Yes
  • Comparable Products/Other parts you considered: basic, cheap ESP modules...
  • What were the biggest problems encountered?: Communication issues caused by misunderstanding of Google Cloud billing policy...

  • Detailed Review:

     

    Introduction

    First of all I'd like to express my thanks to Microchip and Element 14 for selecting me as the roadtester of this amazing board!

     

    The roadtest concern new development board designed to fulfill requirements of easy to introduce projects focusing secured (CryptoAuthentication) IoT data acquisition and computation

    board details:

    AVR-IOT WG Development Board

    Microchip Part Number: ac164160

     

    I need to admit, after relative easy start, I faced some terrible issues conducting experiments with the board.

    At last, my basic tests ended successfully but I couldn't managed to conduct all planned tasks in time.

    I regret, that most advanced part still wait for realization.

     

    I hope my idea of results presentation - less comments more pictures

    will be acceptable!

     

    Overall technical overview

    Going to base Microchip's AVR-IoT Development Board site link:

    https://avr-iot.com/

    you have access to main information about the board.

     

    According to Microchip statement

    The AVR-IoT WG development board combines a powerful 8-bit ATmega4808 MCU,

    an ATECC608A CryptoAuthentication™ secure element IC and the fully certified ATWINC1510 Wi-Fi® network controller

    - which provides the simple and effective way to connect  users embedded application to Google’s Cloud IoT core platform.

    The board also includes an on-board debugger, and requires no external hardware to program and debug the MCU.

     

     

    Documentation and the software

    As usually with their products, Microchip prepared very professional support for its devices.

    Details and links to documentation are available here

    https://www.microchip.com/design-centers/internet-of-things/google-cloud-iot/avr-iot

    https://www.microchip.com/developmenttools/ProductDetails/AC164160

     

     

    Documents and Software are always available under onboard  "KIT-INFO.htm" link


    Selection of most important documentation of the board                               
    AVR-IoT-WG-User-Guide-50002809A.pdf            

                                             
    MCHP-ML3208UK-Fact Sheet Secure IoT Sensor Node)-97865M.pdf

     

    ATWINC1500

    https://www.microchip.com/wwwproducts/en/ATWINC1500

     

    AVR-IOT WG Cloud idea

    AVR-IOT is based on the idea of IoT developed mainly with support of:

     

    Summary of  AVR-IOT  parameters  and  Features

      • ATmega4808 microcontroller
        • Four user LED’s
        • Two mechanical buttons
        • mikroBUS header footprint
        • TEMT6000 Light sensor
        • MCP9808 Temperature sensor
        • ATECC608A CryptoAuthentication™ device
      • WINC1510 WiFi Module
      • On-board nEDBG Debugger
        • Auto-ID for board identification in Atmel Studio and Microchip MPLAB X
        • One green board power and status LED
        • Programming and debugging
        • Virtual COM port (CDC)
        • Two DGI GPIO lines
      • USB and battery powered
      • Integrated Li-Ion/LiPo battery charger

     

    The AVR-IOT WG board implements a wireless (WiFi) IoT sensor node using  AVR microcontroller

    • The ATmega4808 with 48KB of Flash and 6K of RAM with complement of analog and digital peripherals including Core Independent (Event System) functionality.
    • The ATECC608A Secure Elements provides secure key generation/storage and offloads all cryptography tasks enabling security available to modern IoT applications. The secure element is pre-provisioned for immediate (out of the box) authentication with the Google IoT Core Cloud services.
    • The WINC1510 Network Controller provides wireless connectivity and offloads all networking tasks from the main processor providing a secure socket connection and server authentication.
    • The MCP9808 Temperature sensor, a third party lighting sensor, Battery Charger MCP73871, Power Regulator MIC33350, nEDBG Debugger.

     

     

    AVR-IOT WG Board I/O description

     

    Unboxing - quality of delivery, packing

    As the late roadtester I do not want to bore you with the duplication of the process of opening a package.

    All previous roadtesters showed it properly. I confirm it was the fun to open that orange box with brand new, outstanding board.

    Lack of any accompanying stuff as cables, terminals or paper documentation didn't surprise me.

    Omitting the unpacking phase I need to confirm, the shipment was very fast. The box was packed well and delivered safely.

    unboxing AVR-IoT WG

     

    above: all the stuff I only forget to show ESD bag which secure the shipment but also warn the user to be carefully with electrostatic issues!

     

    Start-up the device

    - driver installation

     

     

    The MCU is preloaded with a firmware image that enables to quickly connect and send data to the Google Cloud IoT platform

    using the on-board temperature and light sensors.

     

     

     

     

    "D:\AUTORUN.INF"

    AUTORUN

    [autorun]

    icon=AUTORUN.ICO

     

    "D:\KIT-INFO.TXT"

    Firmware:       01.04.013C (hex)

    Kit:            AVR-IoT WG                                             

    Serial:         ATML320XXXXXX

    Device:         ATmega4808 

     

    nEDBG Debugger and  firmware drag&drop

    At that point I would like to mention the Drag & Drop idea of firmware uploading.

    I was prepared to act as usually with firmware : debug/ compile/build and than still using the dedicated software - upload the binary code into the controller...

     

     

     

     

     

     

    Firmware update procedure

    https://github.com/MicrochipTech/AVR-IoT_WG_Sensor_Node

     

    after upgrade AVR-IoT_WG_Sensor_Node_v1_0_3.hex:

    in KIT-INFO.TXT file

    Firmware:       01.05.0142 (hex)

     

     

     

    Wi-Fi configuration

     

    node starting page (available under

    CLICK-ME.HTM

     

    Cloud based data acquisition

    communication issues:

    At the beginning the board didn't want to communicate with the WLAN.

    After several attempts and switching on- off it started to work.

     

    The board uses its sensors - temperature and light intensity transducers.

    On the pictures below you can see first measurements - temperature and light  readouts in cloud archive

     

    Atter several weeks of experiments I found new firmware version available on Git.

    After providing the board with new firmware - I discovered new functionality on the dashboard.

    It gave extra features and daschboard view:

    But truly speaking - I had no idea how to employ these new functionality using pure, original software

    The Google Cloud/ Leverege functions (later described) do not support it I'm afraid.

    The next easy way to start communication with the board is:

    SERIAL terminal Command Line Interface(CLI)

    The board could be managed using common UART interface.

    Using simple terminal programm after connecting via USB to the computer it works as ordinary RS232 device:

    following few commands are available in the original firmware:

    reset

    device

    key

    reconnect

    version

    cli_version

    wifi <

    debug

     

    next inportant stage ef board exploration will be:

    Cloud Resource Center / Google Cloud registration etc  - Leverege

    All you need to start is available on Git:

    https://github.com/Leverege/microchip-avr-iot

    additioanlyy you can use that link as the support

    Leverege - Getting Started with AVR-IoT: Pushing Data from Device to Cloud

    https://www.leverege.com/blogpost/avr-iot-guide-pushing-data-to-cloud

     

    I found most valuable information about the Leverege solutions concerned AVR-IoT here:

    https://www.leverege.com/blogpost/avr-iot-guide-pushing-data-to-cloud

    https://www.leverege.com/blogpost/iot-connectivity-options-for-asset-tracking

    https://www.leverege.com/blogpost/cellular-iot-security

     

    https://console.cloud.google.com/cloud-resource-manager?pli=1

    https://cloud.google.com/iot-core/

     

    GCP Google Cloud Platform

     

    I realized, that google Chrome is most convieneient when working with GCP - specially that concern the cloud shell interface.

     

     

     

     

     

     

    Run the Quickstart Script

    in the GCP window

     

     

     

    Google Cloud, you'll see IoT Core on the side bar in the BIG DATA section.

     

     

    If you forget to add the key before - in the shell there is possibility to correct the mistake here:

     

    adding functions

     

     

     

    LOGs

     

     

    Console - cloud shell

    Here you can see the script created in the shell console:

     

     

     

     

    Atmel START Rapid Development Tool

     

     

     

    >>> Instruktion page 15

     

    Cloud configuration

     

    The section below was a little confusing for me at the bagining as the instruction wasn't upgraded properly after introduction of the new version of LEVEREGE project

    Under the WLAN Configuration section, we need to enter our WiFi credentials.

    I need to choose:

    WIFI_0

    WLAN CONFIGURATION

     

     

     

     

    now we are ready to:

    just to avoid the risk of loose entered setting.

     

     

     

     

    I could save/ load configuration file -  "Load existing project"

     

    Sometimes I got some errors

    - mostly the version mismatch issues etc...

    Could not load project for identifier=None

    Traceback (most recent call last):

    File "/usr/local/lib/python2.7/site-packages/atmelstart/project/repository/helpers/config_yaml.py", line 118, in populate_project_from_data_dict

    data_output, changes = fix_invalid_v2_project(data)

    File "/usr/local/lib/python2.7/site-packages/atmelstart/project/repository/helpers/serializers.py", line 366, in fix_invalid_v2_project

    format(definition, str(e)))

    UnknownIdentifierError: Unable to load driver config definition Atmel:Commad_Line_Interface:1.0.0::CLI: Unable to load config definition Atmel:Commad_Line_Interface:1.0.0::CLI: No driver container found with identifier: Atmel:Commad_Line_Interface:1.0.0

     

    I got similar errors also with  “foreign” projects or projects from previous version

     

     

     

    At the end of the above operations I got the file:

    AVR IoT WG Sensor Node.atzip

     

     

     

    Installation of software/applications

    The AVR-IoT board is supported by two popular and advanced Integrated Development Environments (IDEs)

    - Atmel Studio

    and Microchip MPLAB® X IDE

    I decided to avoid (boring) description of installation of software used to program the device.

    I have Microchip's MPLAB X with its compilers instaleed and used sucessfully from years.

    Nevertheless the basic version of that suite is free, easy to get on Michrochip site and user friendly during installation.

     

     

    MPLAB X

    now: try to import the new project to the MPLAB X

     

    The chip was "imported" properly:

     

     

     

    According to the NOTICE from the Atmel START user guide

    I had to add

    "ATCA_NO_HEAP;ATCA_NO_POLL;ATCA_HAL_I2C;ATCAPRINTF;TCPIP_BSD"

    to project settings

    ->XC8 Compiler->Preprocessing and messages->Define macros.

    And also

    "-Wno-pragmas"

    to XC8 Global options>additional options

    moreover:

    The project needs to be compiled in "-Os" optimization which needs a licensed version.

     

    errors of build using the XC8 compliler in MPLAB X after import the project from the Atmel START

    #pragma pack(pop, ATCAPacket)

             ^

    In file included from cli/cli.c:37:0:

    cli/../mqtt/mqtt_core/mqtt_core.h:319:34: error: unknown type name 'mqttContext'

    mqttCurrentState MQTT_Disconnect(mqttContext *mqttContextPtr);

                                      ^

    cli/../mqtt/mqtt_core/mqtt_core.h:320:43: error: unknown type name 'mqttContext'

    mqttCurrentState MQTT_TransmissionHandler(mqttContext *mqttContextPtr);

                                               ^

    cli/../mqtt/mqtt_core/mqtt_core.h:321:40: error: unknown type name 'mqttContext'

    mqttCurrentState MQTT_ReceptionHandler(mqttContext *mqttContextPtr);

    ...

    cloud/crypto_client/crypto_client.c:35:2: error: #error : This project uses CryptoAuthLibrary V2. Please add "ATCA_NO_HEAP" to toolchain symbols.

    #error : This project uses CryptoAuthLibrary V2. Please add "ATCA_NO_HEAP" to toolchain symbols.

      ^

    cloud/crypto_client/crypto_client.c:39:2: error: #error : This project uses ATCA_NO_POLL option. Please add "ATCA_NO_POLL" to toolchain symbols.

    #error : This project uses ATCA_NO_POLL option. Please add "ATCA_NO_POLL" to toolchain symbols.

     

    BUILD FAILED (exit value 2, total time: 13s)

     

    Attempt to use the Atmel START (http://start.atmel.com/) failed

    and the exported project couldn't be compiled in mplabX.

     

    after the struggle with AVR-GCC compiler toolchain connection with MPLAB X

    - The simple steps condusted according to the microchip instructions failed... - It's described some lines below.

    I decided to install the whole ATMEL STUDIO.

    After embedding avr-gcc-toolchain

     

    BUILD SUCCESSFUL (total time: 18s)

    Loading code from C:/   ...   /MPLABXProjects/AVR_IoT_WGSN_AtmStrt.X/dist/Default/production/AVR_IoT_WGSN_AtmStrt.X.production.hex...

    Configuration Bits: address 0x821282: FREQSEL = 0 does not match any valid value in the device database.

    Setting to the default value.

    Configuration Bits: address 0x83128A: LB = 0 does not match any valid value in the device database.

    Setting to the default value.

    Loading completed

     

     

    I also succeed to compile the project preparing it from the beginning in mplab X.

    Creating the project "from the beginning" in the MPLAB X

     

     

    we choose ATmega4808:

    our board is visible here:

    XC8 v2 was "onboard" - installed previously

    I decided to add the AVR-gcc - to compare compilers capabilities etc...

    https://www.microchip.com/mplab/avr-support/avr-and-arm-toolchains-c-compilers

    Avr8-gnu-toolchain-3.6.2.1759-win32.any.x86.zip

     

     

     

     

     

     

    According to the picture below, the GCC compiler is available now:

     

     

    NOW -

    LET'S CREATE THE NEW PROJECT using MCC!

     

     

     

     

     

    The latest source code for AVR-IoT WG Development Board (which uses ATmega4808) is available in MPLAB Code Configurator (MCC):

    https://www.microchip.com/mplab/mplab-code-configurator,

    MCC is available as a plugin in MPLAB X.  In MCC, the user needs to navigate to

    Device Resources -> Internet Of Things -> Examples and double click on 'AVR-IoT WG Sensor Node' to add it to 'Project Resources'.

    The complete source code (with hardware peripherals configured for the AVR-IoT WG Development Board) will be generated on clicking the 'Generate' button in MCC.

     

     

     

     

    now change:

    into:

     

     

    changed to my individual project names:

     

     

     

    ramained intouched!

     

     

    GENERATE NOW

    17:44:30.498    INFO: Fetching list of available libraries.

    17:44:30.869    INFO: Download Complete: ..............\.mcc\en586797.xml

    17:44:52.340    INFO: Start MCC

    17:44:52.601    INFO: Core v4.65 loaded.

    17:44:52.609    INFO: Libraries defined in the configuration:

    17:45:52.429    INFO: Saved configuration to file ...........\MPLABXProjects\AVR_4808_moj1.X\MyConfig.mc3

    @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@

    18:02:49.019    INFO: Saved configuration to file ..........\MPLABXProjects\AVR_4808_moj1.X\MyConfig.mc3

    @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@

    19:03:29.342    INFO: Saved configuration to file ..........\MPLABXProjects\AVR_4808_moj1.X\MyConfig.mc3

    @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@

     

    19:03:41.213    INFO: ...nerated_files\winc\spi_flash\source\spi_flash.c Success. New file.

    19:03:44.782    INFO: *****************************************************

    19:03:44.782    INFO:  Generation complete (total time: 15437 milliseconds)

    19:03:44.782    INFO: *****************************************************

    19:03:44.783    INFO: Generation complete.

    19:03:44.910    INFO: Saved configuration to file .............\MPLABXProjects\AVR_4808_moj1.X\MyConfig.mc3

    19:06:01.167    INFO: Saved configuration to file .............MPLABXProjects\AVR_4808_moj1.X\MyConfig.mc3

     

     

    The project compiles without any problem with XC8

    as the result I got binary file here:

    I had serrious issues trying to use gcc compiler

    build/default/production/att13Anewmain.o att13Anewmain.c  -DXPRJ_default=default 

    nbproject/Makefile-default.mk:116: recipe for target 'build/default/production/att13Anewmain.o' failed

    make[2]: Leaving directory '............../MPLABXProjects/attiny13A_test1.X'

    nbproject/Makefile-default.mk:90: recipe for target '.build-conf' failed

    make[1]: Leaving directory '.................MPLABXProjects/attiny13A_test1.X'

    nbproject/Makefile-impl.mk:39: recipe for target '.build-impl' failed

    avr-gcc.exe: error: CreateProcess: No such file or directory

    make[2]: *** [build/default/production/att13Anewmain.o] Error 1

    make[1]: *** [.build-conf] Error 2

    make: *** [.build-impl] Error 2

     

    BUILD FAILED (exit value 2, total time: 323ms)

     

    I tried to solve the problem

    I knew I'm not the first faced similar issue:

    https://www.microchip.com/forums/m1072109.aspx#1085922

    I decided to continue that subjest on the microchip forum and alsu add the new post concerning gcc toolchain

    https://www.microchip.com/forums/m1087155.aspx

    Unfortunatelly I didn't get any advice.

     

     

    ATMEL STUDIO

    Finally I decided to install ATMEL STUDIO

    Now I managed to build the imported project using Atmel studio...

    some fine tuning was necessary:

    building the project

    was sucessfull

    moreover:

    I realized that gcc toolchain form installation above works properly as the gcc compiler in MPLAB X.

    I was able now to build AVR-IOT projects using MPLAB X with both compilers"XC8 and AVR-GCC.

     

    Running my project in Firebase.

    After simple drag and drop of my binary file (my firmware) into the CURIOSITY folder

    I found above view on the dashboard

     

    and after the while- charts known from the original firmware:

     

    Unfortunately the communication was extremely unstable.

    It was strange - and concerned only instability of connection with my “own” program prepared according to Leverege instructions .

    I tested two ways - using ready to use Atmel-Start example and building “from the beginning” using MPLAB-X and MCC.

    After upload, the “firmware” It disconnects often - sometimes restores to work for the while or get lost at all!

     

    To avoid notices about my WiFi connection reliability I must ensure, the WLAN’s are sufficient enough,  the board works fine with original firmware/ software.

    I checked it with two WLAN's - everything went fine with "base"  [AVR-IoT_WG_Sensor_Node_v1.0.3.hex] and also “fresh” [v1.1.0] firmware.

    After clicking "CLICK-ME.HTM" dashboard on  https://avr-iot.com/device/---- is alive and online full time.

     

    Unfortunately after putting my ".hex" (nothing beyond the example from manual) into the board, after move to my dashboard at https://avr-iot-mc1.firebaseapp.com/device/0123...

    it catches the connection for a moment to lose it soon.

     

    I checked - this is not a problem with my WLAN, in many places and with different routers the issue repeats!

    Above - very rare screen in my case at these days

     

    I was told about the UI feature, which expects a constant flow of data,and would show the “connection page” if it doesn't receive data for 15s or longer.

    But I didn’t change data flow parameters I suppose “my” firmware broadcasts data as frequently as “original”,

    I was suggested to  adjust the maxDataAge variable in the UI source code but, honestly, I’m afraid that parameter is unavailable in our standard project.

    That problem consumed a lot of time and frustrated me very much.
    And the solution was simple but strange anyway!
    I don't know how and why
    but at the very beginning of setting my AVR-IOT google cloud project I wasn't asked to set account billing options.
    I was sure, I can use it as the trial one year free, without account activation, card connection etc...
    Moreover I didn't get any warning about lack of billing in Google Cloud Shell.
    Only dealying with next project version, when, after desperate removal of the first "edition" some new errors appeared
    ERROR: (gcloud.services.enable) FAILED_PRECONDITION: Billing must be enabled for activation in projec
    After correction of that negligence my project worked properly.
    The only problem which still remains is something as idle function problem...
    My board is starting to sleep sometime. I honestly didn't find the reason of that behaviour...
    maybe after weak communication lost It can't get back to the broadcasting?

     

     

    Powering question investigations

    I conducted my basic experiments supplying the board using USB cable connected to the computer as well as using external (micro) USB supply.

    That method appear to me as quite stable, nevertheless I observed once or twice curious (sic!) switching off the board (communication) with only red led lighting.

     

    I decided to use and test battery supply option of the board.

    Thanks to reading about that subject on microchip and AVR forum I found, that I need to be carry about the polarization of the battery.

    That post helped me to avoid serious issue, maybe saved from destroying supply section even...

    https://www.avrfreaks.net/forum/avr-iot-wg-battery-charger-problem?skey=AVR%20IoT%20WG

    above attempt to use the simple LiPo battery from the ordinary toy

     

    WRONG POLARITY!!!

     

    let's fix it as simple as possible:

    it works now!

    Charging:

    almost charged

    fully charged:

     

    using the battery I suffered more often, mentioned above issue with "sleeping" the unit after relative short working period.

    The only solution was brutally restart (disconnect/connect the battery)

     

    Simple exercise tests from MICROCHIP site /Github and others

    Using my experience from PIC- related projects I wanted to quickly extend it using our board.

    Except I/O available on CURIOSITY/ MIKROELEKTRONIKA form factor connectors

    I wanted to use onboard switches and LEDS.

    I need to express my confuse...

    as most of that (indeed) simple projects failed...

    I humble admit it must have been my fault and I should improve codes

    nevertheless that stage isn't successful yet...

     

    High-level secured connections

     

    Also in that point some modesty was necessary...

    I’m not a hacker but I imagined to find some examples and try to experiment with the board in the security field

    Unfortunately that remains as the open question I didn't find the way to break ATECC608A

    Anyway attempt to play with it is still challenging for me...

     

    Check of general system immunity

    ...and

    Mechanical issues -

    The quality of the product from the designing/ electric and mechanical point of view

    based on my experience - is great

    I didn't experiment with MIKROELEKTRONIKA modules together with AVR-IoT but I checked possibilities of connecting these modules

    using interface with suitable form factor

    - fully compatible with CURIOSITY modules.

     

    I didn't find any cons regarding board quality.

    Reliable, aesthetic but elegant, quite handy

    with many advantages mentioned in chapters above.

     

    Summary

    After relative (too) long time of dealing with AVR-IoT WG board,

    spending several hours configuring and experimenting with Google Cloud Shell scripts

    and ATMEL START /ready to use/ examples

    as well as "self prepared" MPLAB/ MCC project

    I feel obliged to put some words as the summary.

    At the final stage of that roadtest I have quite different feelings as in the middle of my work...

    Let's explain my hesitations...

    Neglecting the enthusiasm at  the beginning when except difficulties with start up communication, it worked according to the manual and takes "30 seconds to run"

    I experienced lot of troubles trying to implement Leverege instruction of prepare of individual project/ firmware...

    I tried to described it before. It's pity that stupid misunderstanding related to Google Cloud billing issue costed as many time and emotions.

    Happily, everything works correctly now!

    I feel quite comfortable navigating through the software (MPLAB X +MCC or ATMEL)

    Also GCS configuration isn't the mystery anymore!

    Nevertheless I still remember my hesitation when installing the soft, doubts when the editing issued cause errors in GC Shell and communication was lost.

     

    Possibilities of the board especially regarding IoT security are outstanding indeed! I haven't even used few percent of its functionality.

    I focused on start fluent communication but the tool is extremely universal.

    The AVR-IoT WG is powerful equipment providing support for your project.

    Having skills and experience you can take on many challenges from the realm of IoT.

    The open question is the price.

    I, personally use cheap ESP modules. It mostly provide the same basic IoT features...

    But as I said... basic...

     

    And the last CONs...

    The Google Cloud is free ... as the trial for first 365 days...

     

    thanks for reading

    Marek


Comments

Also Enrolling

Enrollment Closes: Aug 18 
Enroll
Enrollment Closes: Jul 13 
Enroll
Enrollment Closes: Aug 7 
Enroll
Enrollment Closes: Jul 14 
Enroll
Enrollment Closes: Jul 28 
Enroll
Enrollment Closes: Jul 20 
Enroll
Enrollment Closes: Jul 17 
Enroll