Skip navigation
> RoadTest Reviews

Analog Discovery 2 + LabView Home Bundle - Review

Scoring

Product Performed to Expectations: 10
Specifications were sufficient to design with: 10
Demo Software was of good quality: 10
Product was easy to use: 10
Support materials were available: 10
The price to performance ratio was good: 10
TotalScore: 60 / 60
  • RoadTest: Analog Discovery 2 + LabView Home Bundle
  • Buy Now
  • Evaluation Type: Development Boards & Tools
  • Was everything in the box required?: Yes
  • Comparable Products/Other parts you considered: As this product is highly flexible and full of features I chose not to compare to any other tool, because I couldn't find any that has all features or most of them.
  • What were the biggest problems encountered?:

  • Detailed Review:

    I hope you all enjoy this RoadTest.

    UNBOXING

    For those who enjoy the cutting blade sound I leave hear the unboxing video.

     

     

    Quick questions

    • Is AD2 suitable for professional use?

    Short: Yes, I believe and do.   

    Long: In the last project in the company I was writing code to interface with sensors ( I2C, UART, SPI) and I used AD2 for this. Since the limitations of AD2 are within your need there is space for you to use it.

    • I am a newbie, Does it suits me?

    Short: Yes, it’s perfect for you.

             Long: AD2 by concept was designed to be an educational tool targeting hobbyist, students, and enthusiasts. The tool is quite straightforward to use, requiring only you to download the Waveforms IDE and take the Tutorial Videos that cover ALL you need.

     

    Getting started with LabView

     

    As a fast way to learn about AD2 and LabView integration, I certainly would suggest trying first the watch tutorials of each program separately in case you are completely fresh to one or both of them. This would give a good understanding of the capability of each tool and moreover I didn’t find a material like getting started with both at the same time, but some blog posts. Actually, I tried to run the examples of integration that come installed with LabView, but even though I could run them and see the results, at first, I had no idea what was going on since I never touched it LabView before. Then, I came back to the examples after this tutorial.

    Installation

    LabView2014 can be downloaded through LabView Maker Hub website as a 45-Day evaluation, but after installation just enter the serial number for the home bundle. After that, I also installed the AD2 driver for Labview so that LabView communicates with AD2. After this, I had my LabView recognizing my AD2.

    Running Example

      One important feature to note in LabView is that it works within two complementaries interfaces: Front Panel and Block Diagram. In the first, the user can see the graphical results of it’s work and in the second, the program ( which is fundamentally in block ). In the following video, I run an example that comes already installed in the installation directory.

     

     

     

    In the video I showed only the front panel, therefore here goes the Block Diagram related to the example.

    Block Diagram for Power Supply instrument




    The instruments AD2 in LabView

           As in the previous video, I only ran the example and now I show what is behind the user interface used, what does the LabView program look like.

     

    Resources about integration

    There are some interesting resources to check which

    SECOND PART

    In the second part of my roadtest, I go over the Waveforms software and develop a simple project in order to explore some AD2 capabilities.

    PROJECT - SUNLIGHT RECORD

    Purpose

      The goal of this short project is to record the light intensity in my room through the window. For that, will be used a Flora board, which has a TSL2561 light sensor, and an AD2 as a controller.

     

    Summary

      In order to read the luminosity of the environment, a Flora is attached to the AD2 which reads out the I2C signals from the sensor and then through an algorithm parses the data received into the lux unit. After that, the data parsed is logged into a CSV file and then plotted into a graphic.

     

    The light sensor

      The TSL2561 is a light-to-digital converter with I2C output. It reads the light intensity from the environment through two diodes, one sensible to visible light and infrared, and other sensible only to infrared allowing to remove the effect of the infrared in the measurement according to an experimental algorithm. The diodes signals are converted into the digital domain and made available to be read from the I2C bus. Figure 1 shows a block diagram of the sensor.

     

    Figure 1: TSL2561 overview

    Setting up the environment

      Figure 2 shows the Flora board used in this project. Header pins were soldered in order to make the pins more accessible.



    Figure 2: Flora board with header pins soldered



      Then, the AD2 was connected according to Table 1. And the result is shown in Figure  3:

     

    Table 1 - Connection map between AD2 and Flora.

     

    AD2Flora Board
    DIO 0SCL
    DIO 1SDA
    V+3V
    GNDGND


    Figure 3: Connection between Flora board and AD2

     

    Reading from I2C

      As a first step, I used the tool Protocol I2C in the Waveforms Software to test communication between Flora board and AD2.

    Power from AD2

      As for this project, I’ll be using AD2 to deliver power to the Flora board, the positive power supply (in supplies instrument) must be turned on at 3 Volts as shown in Figure 4.

     

    Figure 4: Supplies instrument in Waveforms

     

    Internal sensor power-on

    After powering up, Flora should be ready to exchange data. Then, it’s time to open the protocol instrument in the tab I2C ( in master mode ) and configure the communication channel. Figure 5 shows in red the configuration used. The Address value h39 corresponds to the 7bit address of the TSL2561 sensor according to its datasheet as shown in Figure 6 when the address pin is left floating which happens in Flora by default.

    Figure 5: Protocol instrument - Master I2C

     

    Figure 6: TSL2561 datasheet slave address info

     

    Once the communication is properly set, a command 03h to the CONTROL register of the sensor must be sent to the sensor in order to power it up internally. It happens that TSL2561 has only one register (Figure 7)  for both address(lower nibble) and control( upper nibble), then Control Register is accessible as address 80h  for the configuration I’m using. The complete addresses available can be seen in Figure 8.

    Figure 7: COMMAND register description

     

    Figure 8: TSL2561 register address

     

      Therefore, in Protocol instrument, fulfill the fields SubAddress with 0x80 and the Write field with 0x03. After clicking write, the interface should look like Figure 9. It’s important to note that the ACK bit is omitted.

     

    Figure 9:  Power-on sent to CONTROL register



      Now, that the sensor was acknowledged the next step is to read the registers that contain the digital values converted correspondents to the ambient light measured, namely Ch and Dh as Channel0, and Eh and Fh as Channel1. This can be accomplished by reading 4bytes in sequence starting from register Ch.

     

    Therefore, fill the SubAddress with 0x8Ch and the field Bytes with 4 and then click Read. The resultant data stream should be like Figure 10. Note that, the data will differ as a consequence of different ambient illumination.

     

    Figure 10: Reading 4 bytes from sensor



    Logging the data

    Up to now, the following tasks were accomplished:

    1. Power the sensor from AD2;
    2. AD2 through I2C Bus can properly send and receive data from the sensor.


         Then, the next step is to convert the data read from the sensor into luminosity intensity (lux) and record this data into a file. In order to achieve that, create a script is necessary. 
         Still, in the Protocol Instrument under the tab Sensor (Figure 11), scripts can be written in javascript and then run through the button ‘Execute’. There are also short instructions on how to use it. Even easier is to open an example under the tab Example and see how to interact with AD2. And based on the second option a script was written to fulfill the last project requirements.
    Figure 11 - Script editor

    Testing the Script

    In order to test the script ( attached ) written, a test was set at 50 iterations and Rate at 1Hz ( see Figure 12). The test consists in approximate a light source to the tsl2561 sensor and leaves the script running in the meantime, the values measured are recorded in a CSV file and then imported into Excel and plotted into a graph for ease visual analyses.

    Figure 12 - Configuration for script test


    The video below shows how the test was executed. Table 2 (in attachment)shows the data generated by the script and Figure 13 shows the graphic plotted from it. The Orange line DATA0 represents the value of the registers Ch and Dh (Channel0), the Grey line DATA1 represents the value of the registers Eh and Fh (Channel1). Both DATA0 and DATA1 represent a 16-bit wide register. Finally, the blue line represents the calculated value of luminosity in the lux unit.





          

    Figure 13: Graphic plotted from the data generated

     

         Also, in order to bring confidence to the experiment, a measurement with an MT-912 Lux Meter was performed and compared to the values obtained from the script. The results are shown in Figure 14 and Figure15, where Flora measured 77lux and the equipment measured 76,8 lux.

    Figure 14: Test measurement for comparing with MT-912 Lux Meter.

    Figure 15: Measurement set with MT-912 and Flora.

    Logging Sunlight data

      Finally, to obtain data about the light coming from the sun to my room, a setup was made as in Figure 16. The sensor was pointed to outside from close to the window. Then, data was recorded (Table 3 attached ) during about 26 hours and the graphic was plotted in Figure 17.

    Figure 16:  Setup for Sunlight measurement

    Figure 17: Data plot representing luminosity intensity in the room


         As expected, during the day the light is more intense and in the morning even more, because my windows take the sun rising. Also, around 6:40 am to 9:30 am the sunlight intensity in my room was high enough to saturate the sensor which is represented by the flat part in the orange curve in this interval. After that, the light level is lower which represents that my room is not having direct light from the sun maybe due to clouds, obstacles or even its position. At night from 9:30 pm, as it is supposed to happen, the light level tends to zero.

    Project Closing

    All goals for this project were successfully accomplished. The results obtained in the form of plots from the measurements look already intuitive for a first sight evaluation and this analysis was possible due to the possibility of exporting data easily with javascript. Also, the project proved that tsl2561 sensor is only suitable for indoor application due to its saturation point.

    Considerations on the use of Waveforms

      During the project execution, some features were missing or could be improved and some observations were found, then in this section they are described.

    Running Script

    • As a long running of the script was needed ( around 26 hours ), some issues were found. The first issue is that the script doesn't run in the background (Figure 18), because of that if one needs the screen for another task, has to use with the scripting window popped up.


      Figure 18: Executing the Script window popped up

     

    • The second observation is related to the consumption of the CPU. During the script execution, the process was taking 35% of the CPU ( Core i5, 7th gen ), see figure 19.

    Figure 19: CPU consumption while running Script

     

     

    • Another observation to point out is that while the script is running only the button Cancel is possible and if one is recording data and click, then all data already recorded is lost. I would suggest an option to jump to the function finish(), see Figure 20.

    Figure 20: Main functions in sensor script

    • At last, every time a script is saved, it is saved as a new file and there no autosave or prompt to save alterations and as a consequence, if the code is not continuously saved, then it is lost.

     

     

     

        


Comments

Also Enrolling

Enrollment Closes: Nov 15 
Enroll
Enrollment Closes: Nov 5 
Enroll
Enrollment Closes: Oct 29 
Enroll
Enrollment Closes: Nov 18 
Enroll
Enrollment Closes: Nov 15 
Enroll
Enrollment Closes: Oct 30 
Enroll