Skip navigation
> RoadTest Reviews

Bluetooth 5 Radio SoC EVM - Review

Scoring

Product Performed to Expectations: 10
Specifications were sufficient to design with: 10
Demo Software was of good quality: 10
Product was easy to use: 10
Support materials were available: 10
The price to performance ratio was good: 10
TotalScore: 60 / 60
  • RoadTest: Bluetooth 5 Radio SoC EVM
  • Buy Now
  • Evaluation Type: Development Boards & Tools
  • Was everything in the box required?: Yes
  • Comparable Products/Other parts you considered: Raspberry Pi or an Arduino with HC-05/06 modules.
  • What were the biggest problems encountered?: In the beginning I had some difficulty understanding the hardware layout of the board; guessing whether Eclipse code was loaded onto the ATSAM3U2C MCU or the RSL10 processor on the development board.

  • Detailed Review:

    Whether you create simple or complex applications, this small development board has you covered.

     

    Programming and uploading your code to the device is simple and there is enough sample code that is provided to suit your needs.

     

    This device is pretty versatile in that you can connect to it with an iPhone, Android, PC or Mac. Additionally, the board can communicate with a compatible a Arduino like the Uno through any available GPIO pins.

     

    While I didn’t quite have a Bluetooth 5 device to pair with the RSL10-002GEVB, I was able to use BTLE 4 devices with no connectivity problems at all. Serial communication from a computer worked flawlessly with the device up to 2,000,000 Baud rate I tested it for.

     

    I was also able to collect user data with button presses connected to 3.3 and GPIO and have an Arduino Uno and a Arduino Due relay the date, time with a connected RTC when a button was pressed.

     

    This device is powerful enough to control a relay board and several H-bridges together and would even work great as a DCC train controller or motor driver.

     

    Medically, I can see a use for this device as a way to develop computerized prosthetics with sensors and possibly even a text to speech engine where bytes are sent over Bluetooth in a serial connection to play as PCM samples or be directly converted to analog through a resistor DAC controlled by itself or an Arduino or Raspberry Pi.

     

    Really, your imagination for creating something new and innovative is possible. This is a very good way to create an accurate prototype from design and works a lot better than using separate components individually.

     

    I can see people embedding the device into their products as it provides an all in one solution instead of having to start all over from scratch on every project.


Comments

Also Enrolling

Enrollment Closes: Aug 16 
Enroll
Enrollment Closes: Sep 16 
Enroll
Enrollment Closes: Sep 15 
Enroll
Enrollment Closes: Sep 8 
Enroll
Enrollment Closes: Aug 21 
Enroll
Enrollment Closes: Aug 28 
Enroll
Enrollment Closes: Aug 25 
Enroll
Enrollment Closes: Aug 18 
Enroll
Enrollment Closes: Aug 18 
Enroll
Enrollment Closes: Aug 17 
Enroll