Skip navigation
> RoadTest Reviews

RoadTest the Raspberry Pi 4 Model B (2GB) - Review

Scoring

Product Performed to Expectations: 10
Specifications were sufficient to design with: 9
Demo Software was of good quality: 9
Product was easy to use: 10
Support materials were available: 9
The price to performance ratio was good: 10
TotalScore: 57 / 60
  • RoadTest: RoadTest the Raspberry Pi 4 Model B (2GB)
  • Buy Now
  • Evaluation Type: Development Boards & Tools
  • Was everything in the box required?: Yes
  • Comparable Products/Other parts you considered: Raspberry Pi 2 B and 3 B+ Model
  • What were the biggest problems encountered?: Micro HDMI to HDMI Port was not available that's why it took some time for review.

  • Detailed Review:

    Unboxing

    Raspberry Pi Box

     

    Raspberry Pi board

     

     

    Introduction

    The raspberry pi 4 has the previous model include more memory options, a faster quad-core CPU, support for dual displays at up to 4K resolution, Gigabit Ethernet, USB3.0, wireless LAN, Bluetooth 5.0, and USB-C power.

     

    Tutorial Link - https://projects.raspberrypi.org/en/projects/raspberry-pi-getting-started

     

    Specifications

    • 1.5GHz 64-bit quad-core ARM Cortex-A72 CPU ( ARM v8, BCM2837)
    • 1GB, 2GB or 4GB RAM (LPDDR4)
    • On-board wireless LAN – dual-band 802.11 b/g/n/ac
    • On-board Bluetooth 5.0, low-energy (BLE)
    • 2x USB 3.0 ports, 2x USB 2.0 ports
    • Gigabit ethernet
    • Power-over-Ethernet  (requires additional HAT)
    • 40-pin GPIO header
    • 2 micro-HDMI ports (up to 4Kp60 supported)
    • H.265 (4Kp60 decode)
    • H.264 (1080p60 decode, 1080p30 encode)
    • OpenGL ES, 3.0 graphics
    • DSI display port, CSI camera port
    • Combined 3.5mm analogue audio and composite video jack
    • Micro-SD card slot
    • USB-C power

     

    Features

    The Raspberry Pi 4 B has also brought the Operating System named - Raspbian Buster. It is a Debian 10 Buster recently released. This operating System feature has improved desktop user interface, the Chromium 74 browser, and a V3D video driver. This has boosted the performance in the open-source hardware. The major benefits of the driver include running 3D applications on the desktop.

     

    Raspberry pi provides the desktop performance environment while using with the best specialization in the use of simple and daily use application programs. If you want to access office tools Libre Office is the best to use as it comes with pre-installed in the Buster Operating System, other software is VLC Player, Python Games, Programming IDE for Python, Java, and Mathematics tools, etc.

     

    Test Review:

     

    1. Hardware Overview -

    The Raspberry pi 4 is the beast compared to the previous model of the Raspberry pi versions. There is a huge change in the durability and performance in the processing the memory and computational calculation in the model. This hardware takes lots of power as it has to support better performances that's why the model provides in comparison with the raspberry pi 3 B+ Model I will demonstrate the certain test results.

     

    Raspberry Pi 4 B

     

    Raspberry 3 B+

     

    Power Consumption:

    Power TestRaspberry Pi 3 B+Raspberry Pi 4 B
    Input Voltage5V 2A5V 3A
    PortMini D type PortC Type Port
    Tested Voltage (Normal)5.1V 0.2A5.2V 0.45A
    Tested Voltage (Load)5.2V 1.2A5.2V 2.21A

     

    Data Transfer:

    Data TestRaspberry Pi 3 B+ (USB 2.0)Raspberry Pi 4 B (USB 3.0)
    Data File (1 GB)3 min 15 Sec1 min 05 Sec
    4K Video File (3.2 GB)15 min 50 Sec3 min 10 Sec
    Audio File (87 MB)10 Sec03 Sec
    Zip File (3.8 GB)18 min 02 Sec6 min 28 Sec

     

    Video Resolution:

    Video TestRaspberry Pi 3 B +Raspberry pi 4 B
    Composite Video SupportYesYes
    HDMI SupportYesYes
    1080p 60fps SupportYesYes
    2K 30fps SupportNoYes
    4K 60fps SupportNoYes

     

    Connectivity Support:

    SupportRaspberry Pi 3 B+Raspberry Pi 4 B
    BLE4.05.0
    WiFi Module802.11 b/g/n/acdual-band 802.11 b/g/n/ac
    GPIO40 Pin40 Pin

     

     

    Performance:

    The Raspberry pi 4 keeps the CPU usage and memory from getting overloaded at the normal state where compared to the raspberry pi 3 B+ model which usually try to be at the under load but one program causes to overload the CPU and result to restart the operation ongoing i.e while trying to install OpenCV library in raspberry pi.

     

     

     

    IoT Application Use:

    While testing with the IoT Cloud Configuration with the Cayenne API the Raspberry pi 4 took 2 min approximately to install and display the dashboard reading on-screen where on the raspberry pi 3 B+ it took 5 min for overall showing the same dashboard. The only difference that was found was the temperature on the raspberry pi 4 was high compared to raspberry pi 3 B+ due to the performance use case. The heatsink is necessary to use for safety precaution and for getting better performance from the hardware processor.

     

     

    Image Processing with OpenCV 4.0

    The installation procedure for OpenCV libraries took at least 3-4 hours compared to the raspberry pi 3 B+ which took a similar procedure for 8-10 Hours and for Raspberry pi 2 B took a day. The Raspberry pi 4 has better hardware configuration that why it works with faster operations and recall hardware functions. The video testing works fines as I found no lags while streaming webcam video where there were some flickers frames for the raspberry pi 3 B+ hardware.

     

    OpenCV 4.0 link - https://www.pyimagesearch.com/2019/09/16/install-opencv-4-on-raspberry-pi-4-and-raspbian-buster/


Comments

Also Enrolling

Enrollment Closes: Sep 15 
Enroll
Enrollment Closes: Sep 8 
Enroll
Enrollment Closes: Aug 21 
Enroll
Enrollment Closes: Aug 28 
Enroll
Enrollment Closes: Aug 25 
Enroll
Enrollment Closes: Aug 18 
Enroll
Enrollment Closes: Aug 18 
Enroll
Enrollment Closes: Aug 17 
Enroll
Enrollment Closes: Aug 7 
Enroll