Skip navigation
> RoadTest Reviews

RX23W BLE 5.0 Module Target Development Board - Review

Scoring

Product Performed to Expectations: 10
Specifications were sufficient to design with: 9
Demo Software was of good quality: 10
Product was easy to use: 10
Support materials were available: 9
The price to performance ratio was good: 10
TotalScore: 58 / 60
  • RoadTest: RX23W BLE 5.0 Module Target Development Board
  • Buy Now
  • Evaluation Type: Development Boards & Tools
  • Was everything in the box required?: Yes
  • Comparable Products/Other parts you considered: NRF52 Development Kit
  • What were the biggest problems encountered?: Finding The Related Detailed Documents for Design

  • Detailed Review:

    BLE(Bluetooth Low Energy) technology has revolutionized wireless communications By its Popularity and simple characteristics. It allows devices to communicate without Consuming More Power and by maintaining high levels of security. Because of its low power and low cost, BLE has played crucial importance in the evolution of IoT applications from Wearable Devices, high-speed automotive devices to complex medical devices.

     

    Out Of the Box RX23W BLE 5.0 Module Target Development Board

     

     

     

     

    RX23W BLE 5.0 Module Target Development Board

     

    Block Diagram of RX23W BLE 5.0 Module Target Development Board

     

    The external appearance of the top side of the RX23W BLE 5.0 Module Target Development Board

     

    Features Of RX23W BLE 5.0 Module Target Development Board

     

    • R5F523W8CDLN Evaluation MCU
    • On-chip memory: 512-KB ROM, 64-KB RAM, 8-KB E2 data flash memory
    • On Board 1 User, Interfacing Switch
    • On Board 2 User, Interfacing LED
    • Current Consumption Measurement Headers
    • External Power Supply connection Headers
    • Connector for an on-board emulator: USB Micro-B
    • Connector for a USB serial-conversion interface: USB Micro-B
    • PMOD Connectors
    • Arduino Uno Interfacing Headers
    • Maximum transmission output power: 4 dBm (in 4-dBm output mode
    • USB connector: 5-V input
    • Power-supply IC: 5-V input, 3.3-V output

     

    Description Of Features Of RX23W BLE 5.0 Module Target Development Board

     

    1. Evaluation MCU R5F523W8CDLN Features(RX23W Group)

     

    32-bit RXv2 CPU core

    • Max. operating frequency: 54 MHz Capable of 88.56 DMIPS in operation at 54 MHz
    • Enhanced DSP: 32-bit multiply-accumulate and 16-bit multiply-subtract instructions supported
    • Built-in FPU: 32-bit single-precision floating-point (compliant to IEEE754)
    • Divider (fastest instruction execution takes two CPU clock cycles)
    • Fast interrupt
    • CISC Harvard architecture with 5-stage pipeline
    • Variable-length instructions, ultra-compact code
    • On-chip debugging circuit
    • Memory protection unit (MPU) supported

    Low power design and architecture

    • Operation from a single 1.8-V to 3.6-V supply
    • RTC capable of operating on the battery backup power supply
    • Three low power consumption modes
    • Low power timer (LPT) that operates during the software standby state

    On-chip flash memory for code

    • 384- to 512-Kbyte capacities
    • On-board or off-board user programming
    • Programmable at 1.8 V
    • For instructions and operand

    On-chip data flash memory

    • 8 Kbytes (1,000,000 program/erase cycles (Typ.))
    • BGO (Background Operation)

    On-chip SRAM, no wait states

    • 64-Kbyte size capacities

    Reset and supply management

    • Eight types of reset, including the power-on reset (POR)
    • Low voltage detection (LVD) with voltage settings

    Clock functions

    • Main clock oscillator frequency: 1 to 20 MHz
    • External clock input frequency: Up to 20 MHz
    • Sub-clock oscillator frequency: 32.768 kHz
    • Frequency of Bluetooth-dedicated clock oscillator: 32 MHz
    • PLL circuit input: 4 MHz to 12.5 MHz
    • On-chip low- and high-speed oscillators, dedicated on-chip low-speed oscillator for the IWDT
    • USB-dedicated PLL circuit: 4, 6, 8, or 12 MHz 54 MHz can be set for the system clock and 48 MHz for the USB clock
    • Generation of a dedicated 32.768-kHz clock for the RTC
    • Clock frequency accuracy measurement circuit (CAC)

    Realtime clock

    • Adjustment functions (30 seconds, leap year, and error)
    • Calendar count mode or binary count mode selectable
    • Time capture function
    • Time capture on event-signal input through external pins

    Independent watchdog timer

    • 15-kHz on-chip oscillator produces a dedicated clock signal to drive IWDT operation.

    Capacitive touch sensing unit

    • Self-capacitance method: A single pin configures a single key, supporting up to 12 keys
    • Mutual capacitance method: Matrix configuration with 12 pins, supporting up to 36 keys

    Up to 12 communication functions

    • Bluetooth Low Energy (1 channel) An RF transceiver and link-layer compliant with the Bluetooth 5.0 Low Energy specification
    • LE 1M PHY, LE 2M PHY, LE Coded PHY (125 kbps and 500 kbps), and LE Advertising extension support
    • On-chip Bluetooth-dedicated AES-CCM (128-bit blocks) encryption circuit
    • The 83-pin LGA product has been certified as compliant with radio-related laws (in Japan, North America, and Europe).
    • The 83-pin LGA product includes a small PCB trace antenna.
    • USB 2.0 host/function/On-The-Go (OTG) (one channel), full-speed = 12 Mbps, low-speed = 1.5 Mbps, isochronous transfer, and BC (Battery Charger) supported
    • CAN (one channel) compliant to ISO11898-1: Transfer at up to 1 Mbps
    • SCI with many useful functions (up to 4 channels) Asynchronous mode, clock synchronous mode, smart card interface Reduction of errors in communications using the bit modulation function
    • IrDA interface (one channel, in cooperation with the SCI5)
    • I2C bus interface: Transfer at up to 400 kbps, capable of SMBus operation (one channel)
    • RSPI (one channel): Transfer at up to 16 Mbps
    • Serial sound interface (one channel)
    • SD host interface (optional: one channel) SD memory/ SDIO 1-bit or 4-bit SD bus supported

    Up to 19 extended-function timers

    • 16-bit MTU: input capture, output compare, complementary PWM output, phase counting mode (five channels)
    • 16-bit TPU: input capture, output compare, phase counting mode (six channels)
    • 8-bit TMR (four channels)
    • 16-bit compare-match timers (four channels)

    12-bit A/D converter

    • Capable of conversion within 0.83 μs
    • 14 channels
    • Sampling time can be set for each channel
    • Self-diagnostic function and analog input disconnection detection assistance function

    12-bit D/A converter

    • Two channels

    Analog comparator

    • Two channels × one unit

    General I/O ports

    • 5-V tolerant, open drain, input pull-up, switching of driving capacity

     

    2. Emulator

    An emulator is mounted on the board. With the settings as shipped, the switches are shown in the below figure is turned off and the emulator is in the reset state. To use the emulator, make the corresponding switch setting in The Table.

    The shape of the emulator connector (ECN1) is USB micro-B for the IDE and for the Renesas Flash Programmer (RFP). Connect the emulator connector to the computer by a USB cable. If the power supply on the host side is on, the power is supplied to this product at the same time as the connection of the cable.

     

    3. USB-to-Serial Conversion

    USB connector CN1 is connected to the USB-to-serial conversion module from FTDI and can be used as a virtual COM port. Table Below shows the connection relationship of USB-to-serial signals

     

    Names of the USB-to-Serial Signals

    The first time the CPU board is connected to the USB port of a PC, the monitor of the PC shows the message stating that installation of the driver is in progress as shown below Figure. After that, a message indicating completion of the driver installation is displayed. The content of the message will differ from the OS version on the host PC

     

    Displays Indicating Installation of the USB-to-Serial Driver

    If you do not have a driver, download the installer for the driver from the Web site of FTDI .https://ftdichip.com/drivers/

     

    4. ACT LED

     

    The ACT LED displays the state of operation of the emulator control software. The illumination conditions are listed below. The LED is green.

    • Illuminated: Indicates that the emulator is connected to the target.
    • Blinking: Indicates that the host machine (PC) has recognized the emulator.
    • Not illuminated: Indicates that the emulator cannot be used for some reason (including its power being off)

     

    5. Power LED

    While the power LED is illuminated, power is being supplied to the board. The LED is green.

     

    6. User LEDs

    The optional user LEDs can be used for any purpose. LED0 and LED1 are mounted on the board and are respectively connected to the following ports. The LEDs are green

    LED0: Pin 47, connected to port PC0

    LED1: Pin 53, connected to port PB0

     

    7. External Power-Supply Header

     

    When more current is required than the USB is capable of supplying, use the external power-supply header (J1) to supply power. The usable voltage is 3.3 V. When this header is to be used, remove the pattern for cutting (SS19) on the soldered side, electrically separating the emulator from the target.

    The figure below shows the position of the pattern for cutting.

     

    The below Figure shows the position of the external power-supply header (the actual header component is not mounted on the board as shipped)

     

    8. Pmod Connector

    The specification of the Pmod connector (CN2) is on the assumption that Pmod modules are to be connectable. CN2 is for connection to Pmod Interface Type 6A (Type 6 + Type 1) modules* in the product as shipped. Remodeling of the board by removing patterns for cutting enables the connection of CN2 to Type 2A or Type 3A modules. Use Pmod modules for operation at the same potential as that for the evaluation MCU. However, we do not guarantee connection to all types of Pmod modules. Confirm the specifications of this product against any Pmod module you intend to use.

     

    Note: The specifications of Type 6A differ from those described in the Pmod interface specification of Digilent.

     

    Pin Assignments of the Pmod Connector

    9. Arduino UNO Headers

    For the J2, J3, J4, and J5 headers, through-holes are assigned with a pitch of 2.54 mm, and these headers are connected to the evaluation MCU according to the Arduino UNO R3 specification.

     

    Pin Assignments of J2 (6-Pin Analog Connector)

    Pin Assignments of J3 (8-Pin Power Connector)

     

    Pin Assignments of J4 (8-Pin Digital Connector)

    Pin Assignments of J5 (10-Pin Digital Connector)

     

    10. Current Measurement Header

    The current measurement header (JP1) is used to measure the current drawn by the evaluation MCU (an actual header component is not mounted on the board as shipped). The current drawn can be measured by connecting an ammeter to the evaluation MCU. When this header is to be used, remove the relevant pattern for cutting (SS20) on the soldered side. The figure below shows the positions of the header and pattern for cutting.

    11. MCU Headers

    MCU headers are provided for by two sets of through holes (CN3 and CN4) for 36-pin headers (actual header components are not mounted on the board as shipped). The pin headers have a pitch of 2.54 mm and are connected to the evaluation MCU. Pin numbers of the MCU headers correspond to those of the evaluation MCU, and most pins are connected (with pins 3, 6, 9 to 20, 33, 35, 36, and 73 to 83 as the exceptions).

     

    12. Reset Switch

    Pressing the RESET switch applies a hardware reset to the evaluation MCU

     

    13. User Switch

    An optional user switch (SW1) is mounted. It is connected to pin 42 of the evaluation MCU, which operates as pin function P15. The IRQ5 interrupt is multiplexed on the same pin.

     

    Advantages of RX23W BLE 5.0 Module Target Development Board

     

    1. Large On-chip memory
    2. Low Power Consumption
    3. Low Cost

    Every Wearable design's main concern is the Size Of the Main microcontroller and the Memory size. RX23W group BLE is perfect For Wearable applications.

     

    Renesas Try BT App interfacing with The RX23W BLE 5.0 Module Target Development Board

     

    We can check the RX23W BLE Target Board Communication with the Android Application. The Demo Firmware is Factory Preloaded, we just need to connect the Target Board with The Mobile application. The App Try BT Can be download from the app store. By connecting the Target board with the app let's try the LED Light Up Demo. In below video you can see the demo.

     

    RX23W BLE 5.0 Module Target Development Board


Comments

Also Enrolling

Enrollment Closes: Oct 1 
Enroll
Enrollment Closes: Oct 18 
Enroll
Enrollment Closes: Oct 1 
Enroll
Enrollment Closes: Oct 9 
Enroll
Enrollment Closes: Oct 4 
Enroll