Skip navigation
> RoadTests

TI and Würth Elektronik LED RoadTest+

Enrollment Closed

Start Date: 9/14/15 12:00 PM

End Date: 10/19/15 11:59 AM


Kits Offered: 10

Applicants: 66

Summary

TI and Würth Elektronik LED RoadTest+

Description

RoadTestPlus.png

 

Follow The Projects

 

WE-Logo.jpg

 

{tabbedtable} Tab LabelTexas Instruments/Würth Elektronik RoadTest+
About This RoadTest+

The modern world faces new challenges every day; learn about LED basics, TPS92512 LED driver and passive components to make your contribution to solve them!

 

Thanks to technological advancements, Light Emitting Diode (LED) becomes brighter every year and is not limited to just being used in indicators. Many applications such as automotive headlight, street light, traffic light and even commercial and residential lighting fixtures are using high brightness LEDs.

 

This RoadTest+ will challenge its recipiants to come up with an innovative solution to a modern world problem using the kit provided. Upon receiving the kit the challengers will be required to post an un-boxing blog, along with bi-weekly project updates in the Lighting space. The winning projects will be receiving an Apple Watch! See terms and conditions for details.

 

 

 

{gallery}

TPS92512_EVM.JPG

TPS92512EVM-001

light2.jpg

MSP-EXP430FR4133

light1.jpg

CC2540TDK-LIGHT

Picture_WE_Sunglasses.jpg

Each challenger will receive a pair of Würth Elektronik Sunglasses

 

applewatch.jpg

Grand Prize is an Apple Watch

iwatch sport.jpg

Runner- Up Prize is an Apple Watch Sport

The Challengers

Congratulations to the below members that have been selected to compete in this RoadTest+. I will be reaching out to you next week with your shipping details and to provide more information about this challenge. If you have any questions please let me know!

 

Challengers:

ipv1

amgalbu

sunnyiut

tonyboubady

dougw

no1089

gpolder

binarygenius

Rubi

tomaja

The Kit

The Kit will include:

 

TPS92512 Buck Regulator with Analog and PWM Dimming (TPS92512EVM-001)

The TPS92512EVM is designed to accept an input voltage range of 12V to 60V and drive high current LED stacks at up to 1.5A while providing a small form factor. The LED stack can be between 9V and 24V depending on the input voltage range. The circuit can be dimmed using an analog current adjust function, a PWM dimming function, or both simultaneously.

Features:

  • High Current Buck LED Driver
  • 12V to 60V Nominal Input
  • Analog Dimming
  • PWM Dimming
  • Small Form Factor

Bluetooth Low Energy Light Development Kit (CC2540TDK-LIGHT)

The CC2540T Bluetooth low energy (BLE)(Bluetooth Smart) light development kit is intended for customers who would like to evaluate BLE lighting control for LED light products, and develop simple applications and demonstrators based on this standard.

 

What's Included?

  • (3) BLE LED boards
  • (3) micro-USB cables

 

MSP430FR4133 LaunchPad Development Kit (MSP-EXP430FR4133)

The MSP-EXP430FR4133 LaunchPad development kit is an easy-to-use Evaluation Module (EVM) for the MSP430FR4133 microcontroller. It contains everything needed to start developing on theMSP430 Ultra-low-power (ULP) FRAM-based microcontroller (MCU) platform, including on-board emulation for programming, debugging and energy measurements. The board features on-board buttons and LEDs for quick integration of a simple user interface as well as a Liquid Crystal Display (LCD) display which showcases the integrated driver with flexible software-configurable pins. The MSP430FR4133 device features embedded FRAM (Ferroelectric Random Access Memory), a non-volatile memory known for its ultra-low power, high endurance and high speed write access.

 

Rapid prototyping is simplified by the 20-pin BoosterPack™ plug-in module headers, which support a wide range of available BoosterPacks. You can quickly add features like wireless connectivity, graphical displays, environmental sensing, and much more. Design your own BoosterPack or choose among many already available from TI and third party developers. The out-of-box provided with the MSP-EXP430FR4133 LaunchPad features the on-board segmented display and offers two operating modes. Stopwatch Mode can run a timer for up to 100 hours, or alternatively operate split time, where the display can be frozen and the stopwatch continues running in the background. The second mode provides a simple thermometer application using the on-chip temperature sensor. The temperature is displayed on the LCD and can be shown in degrees Fahrenheit or Celsius.

 

Features:

  • MSP430 ULP FRAM-based MSP430FR4133 16-bit MCU 16KB FRAM
    • 16-Bit RISC Architecture up to 8-MHz FRAM access/ 16MHz system clock speed
    • 3 x Timer Blocks
    • 10Ch 10-Bit ADC
    • 8 x 32 segment LCD driver with integrated charge pump and configurable pins
  • EnergyTrace available for ultra-low-power debugging
  • 20 pin LaunchPad standard leveraging the BoosterPack ecosystem
  • Onboard eZ-FET emulation
  • 2 buttons and 2 LEDs for User Interaction
  • Segmented LCD

 

What's Included?

  • 1x MSP-EXP430FR4133 LaunchPad Development Kit
  • 1x Micro USB cable
  • 1x Quick Start Guide

 

Free Würth Elektronik

 

Accepted entrants can request power and filter inductors, wireless charging coils, capacitors, LEDs and connectors. Check out http://katalog.we-online.de/en/  for details about the portfolio and contact us at ledroadtest@we-online.com in order to request the parts you need.

 

A $200 Voucher to be used at www.newark.com  or www.farnell.com*

restrictions apply- see terms and conditions for more detail.

Terms and Conditions

Texas Instruments and Würth Elektronik RoadTest +

Terms and Conditions

These are the terms and conditions which govern the Texas Instruments and Würth Elektronik RoadTest+ competition. This RoadTest+ requires participants to use specified components supplied free of charge by the Organiser to design and build an innovative and previously unpublished project on the theme of building a project solves a problem faced by the modern world. Participants will be required to meet the Conditions for Participation and the winner chosen by the Judges will win the Principal Prizes (detailed below). No other prizes are offered.

  1. 1 The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

Competition: Texas Instruments and Würth Elektronik RoadTest+ (or the Challenge)

Key dates:

Applications Close: midnight (GMT) on 19 October 2015

Announce Challengers: 23 October 2015

Competition Period: Challengers’ Announcement to Project Submission Close (14 weeks)

Project Submission Close: midnight (GMT) on 18 January 2016

Judging and Voting Close: midnight (GMT) on 30 January 2016

Announcement of Winner (estimated): 2 February 2016

Prizes:

Grand Prize:

Apple Watch 42mm Aluminum with Sport Band – Value $599.00

 

Second Place Prize:

Apple Watch Sport 42mm Aluminum Case – Value $399.00

 

Competition Site: www.element14.com/community/community/roadtest/1481

Site or element14 Community: www.element14.com/community

 

Judges: Members of the element14 community team chosen at the Organiser’s discretion and members of the Sponsor’s organization and element14.

Judging Criteria: All of the following which will have equal weighting:

· Originality;

· Innovation;

· Technical merit;

· Meeting the goals and intentions of the Challenge as set forth in these Terms;

· Completeness and clarity of Blogs and supporting media describing the evolution and completion of the Project

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Challenge (each one an Applicant) must:

  • Complete and submit the registration form (Registration Form) on the Competition Site

Minimum number of Challengers: 10

Conditions for Participation: in addition to meeting the requirements of these terms, all persons chosen to take part in and participating in the Challenge (each one a Challenger) must:

  • Use certain specified mandatory components from all of the following components (Kit) provided free of charge by the Organiser in the completion of their design and build project that create a solution for a problem facing the modern world. (Project)
    • The Kit comprises:

Texas Instruments:

  • EVM TPS92512
  • MSP-BNDL-FR4133IR
  • CC2540TDK-LIGHT
  • $200 Voucher to Newark.com or Farnell.com

 

Würth Elektronik:

  • Accepted entrants can request power and filter inductors, wireless charging coils, capacitors, LEDs and connectors. Check out www.we-online.com/products  for details about the portfolio and contact us at ledroadtest@we-online.com in order to request the parts you need.

 

  • Participants will be given a pair of Würth Elektronik sunglasses.

 

Approximate value of the kit is $600

  • Post an un-boxing blog of the kit within 10 days of receiving the kit. Post blogs on the progress of their Project (Blogs) not less frequently than once per 2 weeks during the Competition Period in the www.element14.com/lighting area with the tag ledroadtestplus . One or two weekly omissions are permissible as long as the total number of Blogs is at least 10.
  • Ensure the Blogs meet the requirements of these Terms and all terms of access and use applicable to the Site.

 

Sponsor: Texas Instruments and Würth Elektronik

 

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

 

Eligibility

Save as set out in these Terms, the Challenge is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.1 All Applicants must be aged at least 18 at the time of their application.

1.2 Applicants must not enter the Challenge if doing so or taking part may:

1.2.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.2.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.2.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.3 Multiple applications are permitted as long as each is complete, abides by these Terms and represents a discreet Project.

1.4 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.5 The Challenge is NOT open to:

1.5.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.5.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

1.5.3 The Judges, Sponsors or any of their Direct Families.

1.6 Certain Restrictions and conditions apply to the below countries due to the inclusion of the voucher as part of the kit. A Participant not meeting the below conditions had the right to waive their voucher to be included in the contest:

(a) Germany & Austria- Consumers must be students

(b) Belgium – Minimum order value of $50 for consumers

(c) Italy- Consumers must be students

(d) Export Regions (International markets) – Consumers must be students

(e) Czech Republic, Estonia & Bulgaria- Consumers must be students

(f) Nordics (Denmark, Finland, Norway &Sweden) – Businesses only (VAT number required)

(g) Portugal – Business only (VAT number required)

  1. 2 Applications:
  2. 3 Selecting Challengers: 
  3. 4 Blogs:
  4. 5 The Kit:
  5. 6 Projects:
  6. 7 Judging:
  7. 8 Prizes:
  8. 9 Liability:
  9. 10 General:

2.1 Each Applicant must fully complete and submit a Registration Form by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the Challenge;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Blogs for the purposes of the Challenge and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Challenge. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Challenge or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Challenge;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Challenge (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the Challenge and/or the Judges.

2.3 All applications submitted to this Challenge must meet the following criteria:

2.3.1 The application must propose a Project which is independently created and novel and/or a novel improvement to an existing design or product;

2.3.2 The proposed Project or any product made based on the proposed Project must not have been offered for sale at any time prior to the Announcement of Winner. If a patent application has been filed in respect of any aspect of a proposed Project, then the contents of that application must not be published or produced at any time during the Challenge;

2.3.3 Applicants must be the author, creator and owner of the proposed Project. Applicants must not submit someone else’s idea;

2.3.4 The proposed Project must be reasonably achievable by the within the time constraints of the Challenge;

2.3.5 Applications must not include or propose any of the following, the inclusion of which shall render any proposed Project ineligible and any application based on any such proposed Projects shall be null and void:

(a) Projects or designs which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Projects or designs that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser and/or the Judges;

(c) Projects or applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No proposed Project or Project may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Challengers will be selected by the Organiser, Judges, and/or the Sponsor if applicable, on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Challengers selected will be at least the minimum number set out in condition 1 above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 Applications describing the Projects selected for participation will be published on the Competition Site.

3.4 The Organiser will use all reasonable efforts to announce the Participants within 10 business days the Applications Close.

4.1 A Blog can be in any language.

4.2 Incomplete, corrupted or incomprehensible Blogs must not be posted. Blogs must not contain content:

4.2.1 Relating to socially taboo topics, such as illicit drug use or sexual gratification;

4.2.2 Which is or may be illegal, immoral, discriminatory or offensive as determined by the Organiser, the Sponsor (if applicable) and/or the Judges;

4.2.3 Which infringes or breaches any of the policies or terms of access or use of the Site?

4.3 Challengers are strongly encouraged to post videos, images and other media as part of their Blogs, including for example:

4.3.1 Images that are legible on screen (640x480 pixel at 72 dpi) (e.g., detailed component level schematic diagrams, photos, flow diagrams, etc.);

4.3.2 Software routines (if applicable);

4.3.3 3d print files or CNC router files (if applicable);

4.3.4 A list of all components used (including manufacturer’s part numbers).

4.4 Each Blog (and associated content) must be submitted electronically to the Competition Site.

4.5 Each Blog must be published under the Applicant’s element14.com username.

5.1 The Kit is provided "as is" and the Organiser (and the Sponsor, if any) make no warranties or representations of any kind with respect thereto.  The use of the Kit is entirely at the risk of the Participant.

5.2 The Kit may not be returned and no credit, refunds or cash alternatives are available in respect of the Kit.

5.3 The Kit is provided for the purposes of the Challenge only and, without prejudice to the generality of 6.1, the use of the Kit for any other purpose is entirely at the Participant’s risk.

5.4 In no event will the Organiser or any Sponsor have any Liability to any Participant or any third party for any incidental, special, direct, indirect, or consequential damages resulting from the Applicant’s use of the Kit. Subject to condition 10.2, Challengers are wholly responsible for their use of the Kit and for taking reasonable precautions for ensuring their own safety, in both the assembly and testing of their Projects.

6.1 Projects must be submitted electronically to the Competition Site by Project Submission Close.

6.2 Projects must accord with the description and parameters for that Project set out in the application for that Project.

6.3 Projects must comply with all requirements of condition 3.3 and, without limitation, must not:

6.3.1 Infringe or give rise to any claim that they infringe the IP of any third party;

6.3.2 Include or give rise to any of the following, the inclusion of or reference to which shall render any Project ineligible to take part in this Competition:

(a) socially taboo topics, such as illicit drug use or sexual gratification;

(b) any material or ideas which could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser and/or the Judges;

(c) any material or ideas which would infringe or breach any of the policies or terms of access or use of the Site.

7.1 The winner(s) will be selected by the Judges in their absolute discretion based on the Judging Criteria. Winners must meet all eligibility requirements of these Terms. There shall be such number of winners as the Judges shall determine.

7.2 The Judges’ decision is final and without right of appeal. No correspondence will be entered into. The Judges reserve the right not to select a winner if, in their sole discretion, they do not consider any of the Projects to merit the Prize.

7.3 The Judges and the Organiser will use all reasonable efforts to complete judging by Judging and Voting Close and to notify the winner(s) via a blog posted on the Competition Site by the Announcement of Winner Date.

7.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the Challenge, the Kit or other competitions with which the Organiser or the Sponsor may be connected from time to time. Refusal to take part in any other form of publicity will mean that any Prize and title and status of Winner will be forfeited and the Judges may select another winner.

7.5 Details of the winners will also be published in the media.

7.6 The Competition may include a Community Choice award winner.  Any Community Choice award winner will be selected by vote of the members of the Site. Any such winner agrees to his or her name, image, Blogs or Project being publicised and used for promotional purposes in accordance with condition 8.4, 8.5 and all other Terms and agrees and acknowledges that there is no prize associated with winning the Community Choice Award.

8.1 Prize(s) must be accepted within 12 months of the date that the Organiser announces the winner(s).

8.2 If a winner declines or fails to accept a prize then the prize and title will be forfeited and awarded to the next appropriate Participant as determined by the Judges.

8.3 The Organiser reserves the right no to award prizes in accordance with condition 8.2.

8.4 Any Prize(s) are provided "as is" and the Organiser (and the Sponsor, if any) make no warranties or representations of any kind with respect thereto, whether as to quality, condition, use, suitability or otherwise.  The Organiser will use reasonable efforts to pass to the winner the benefit of such warranties (if any) as may be available from the supplier or manufacturer of any Prize. All further warranties or representations in relation to any prize are hereby expressly excluded to the fullest extent permitted at law. Prizes may not be returned and no credit, refunds or cash alternatives are available in respect of any Prize.

8.5 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

9.1 The Organiser hereby excludes all and any Liability arising out of the competition or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

9.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

9.3 Subject to 10.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

10.1 The Challenge is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the Challenge to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

10.2 The Challenge may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the Challenge at any time due to circumstances outside its reasonable control.

10.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the Challenge or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

10.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Competition Site and it is a condition of entry to the Challenge that Applicants and Challengers agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

10.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

10.6 These Terms and the operation of the Challenge shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.


Comments

ALSO ENROLLING

Enrollment Closes: Feb 17 
Enroll
Enrollment Closes: Feb 17 
Enroll
Enrollment Closes: Feb 25 
Enroll
Enrollment Closes: Mar 15 
Enroll
Enrollment Closes: Feb 21 
Enroll
Enrollment Closes: Mar 8 
Enroll
Enrollment Closes: Mar 1 
Enroll
Enrollment Closes: Feb 26 
Enroll

Roadtesters

No new members have been added recently.