Skip navigation
> RoadTests

IDT ZMOD4410 Indoor Air Quality Raspberry Pi HAT

Now Enrolling

Start Date: 9/24/20 12:00 PM

End Date: 10/30/20 01:00 AM


Kits Offered: 4

Applicants: 31

Enrollment closes in:

Summary

RoadTest the Renesas/IDT ZMOD4410 Indoor Air Quality Sensor Module using the Raspberry Pi.

Description

renesas logo

 

{tabbedtable} Tab LabelTab Content
About

In this roadtest, you will have the opportunity of test the ZMOD4410 Gas Sensor Module, which is designed to detect total volatile organic compounds (TVOC) and monitoring indoor air quality (IAQ). The ZMOD4410 Sensor Module is conveniently mounted on a Raspberry Pi Hat by AVNET. Roadtesters will also receive a Raspberry Pi Raspberry Pi 3 Model B and 16GB SD Card.

 

About the Renesas ZMOD4410 Indoor Air Quality Sensor Module

Providing best-in-class stability and sensitivity, the Renesas ZMOD4410 gas sensor module is designed to detect trace gases in various locations within indoor environments. It features embedded artificial intelligence (e-AI), enabling smart odor sensing for ventilation systems, bathroom monitoring and controls, and air quality monitors. It can be configured for use in individual rooms in homes and buildings, such as bathroom and kitchens, to solve unique air quality problems. The sensor is supplied with pre-compiled libraries.

 

It is a 12-pin LGA assembly (3.0 x 3.0 x 0.7 mm) that consists of a gas sense element and a CMOS signal conditioning IC. The module’s sense element consists of a heater element on a Si-based MEMS structure and a metal oxide (MOx) chemiresistor. The signal conditioner controls the sensor temperature and measures the MOx conductivity, which is a function of the gas concentration.

 

The measurement results can be read via an I2C interface with the user’s microprocessor, which processes the data to determine the TVOC concentration, IAQ rating and estimated carbon dioxide (eCO2) level. This flexibility makes the sensors in the ZMOD4410 sensor capable of providing a variety of measurement options by varying the method of operation or changing the firmware used to interpret the resistance measurements. Downloadable firmware libraries and source code provided by IDT enables detection of TVOC and odors and supports smart devices measuring IAQ that require low-power operation.

 

SensorBlock Diagram
ZMOD4410 Gas Sensor Moduleblock diagram

 

Features

  • Sensor output based on AI machine learning algorithmic features:

– Measurement of total organic compounds (TVOC) concentrations and indoor air quality (IAQ)

– Module algorithm estimates carbon dioxide level (eCO2)

– Algorithm to set a control signal to trigger an external action based on IAQ and odor change

– Algorithm to discriminate sulfur-based odors

  • Firmware for mobile, industrial, and consumer applications
  • Algorithm to set a control signal to trigger an external action based on IAQ and odor change
  • Renesas offers downloadable source files and compiled code, enabling a product road map of indoor air measurement innovation

Indoor Air Quality specifications

About The Avnet ZMOD4410 IAQ Pi HAT

To roadtest the ZMOD4410 Indoor Air Quality Sensor Module, element14 chose to use the Avnet Renesas ZMOD4410 Indoor Air Quality HAT built for Raspberry Pi. The HAT features an on-board calibrated ZMOD4410 sensor that measures the concentrations of Total Volatile Organic Compounds (TVOC) and can estimate carbon dioxide (eCO2) levels. In addition to the ZMOD4410 sensor, the HAT incorporates a Renesas HS3001 Precision Relative Humidity and Temperature Sensor, along with software-controlled status LEDs.

AVNET ZMOD4410 IAQ Pi HATBlock Diagram
ZMOD4410 Pi HatZMOD4410 Pi Hat block diagram

BUY NOW

Features

  • Convenient Raspberry Pi HAT form factor for evaluation, development and quick prototyping of products that monitor indoor air quality
  • Detects a wide range of TVOC, from parts-per-billion to parts-per-million and provides eCO2 levels
  • Sensors are chemically tested and factory calibrated
  • On-board user-adjustable power supply option and current measurement connection points
  • Supplied with pre-compiled Raspberry Pi OS test / validation application
  • Renesas offers licensed downloadable compiled code, enabling a product road map of indoor air measurement innovation

 

In addition to the  AVNET ZMOD4410 Pi HAT, we will be including a Raspberry Pi 3 Model B and a 16GB SD card.Raspberry Pi 3 Model B16gb sd card

About the Renesas Software

So far we've talked about the hardware in this roadtest. Let's now talk about the software. Since this is a commercial product, not an “open source." Hence, source code for the software is not provided. The Renesas is encrypted and requires a software license to download and obtain the binary libraries that make the sensor function.

 

1. To validate the HAT’s operation and begin measuring TVOC and eCO2 “out of the box” with a Raspberry Pi solution, Avnet provides a pre-compiled test application built with those algorithm libraries that runs under the Raspberry Pi operating system. You can download it here under "Software Downloads."

 

2. You can download Renesas’ Software License Agreement and procedure to download the ZMOD algorithm libraries and related confidential data by clicking here Scroll down to downloads and you will see files with a yellow lock icon:

renesas software downloads

Click the icon and you will be prompted to create a Renesas account. After your account is verified, you can click the file and you will be taken to the Secure Access Request.

(Be patient. it takes some time to approve your account and get access.)

 

RoadTesting The ZMOD4410 Indoor Air Quality Sensor Module

There are two ways to approach this roadtest:

  • Basic Users (hobbyists, makers): You can run the demo provided by Avnet, which is easy to do and anyone familiar with the Pi should be able to do. This blog can give you some ideas.
  • Advanced Users (embedded developers, pro-makers, engineers. entrepreneurs): If you want to create a project (or anything beyond the demo), you will need to get a software license from Renesas, download the binaries, and work through the documentation. This requires a higher level of skill and more experience. Note: You will not be able to modify the algorithm due to Renesas’ license policy, nor can you re-distribute the licensed binary file.

 

Additional and Resource Information

Important Dates

Enrollment Begin: Sept 24 2020

Enrollment Ends: October 30 2020

RoadTesters Selected: Nov 4 2020 (estimated)

Product Shipped: TBD

RoadTesting Begins: TBD

Reminder/Update Email: TBD

Submit Reviews By: TBD

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, rscasny, as soon as possible before the deadline.

RoadTesters

Submit an application today to become an official roadtester. At the end of the enrollment period, the official roadtesters will be announced.

Other

The Avnet IDT ZMOD4410 Indoor Air Quality Raspberry Pi Hat is an evaluation, development and quick-prototyping tool intended for developing a wide variety of mains-powered and battery-powered products with Indoor Air Quality monitoring capability.

 

 

The Hat features an on-board calibrated ZMOD4410 sensor which measures the concentrations of Total Volatile Organic Compounds (TVOC) and can estimate carbon dioxide (eCO2) levels. These are important indicators for monitoring Indoor Air Quality. The Avnet IDT ZMOD4410 Indoor Air Quality Raspberry Pi Hat is an evaluation, development and quick-prototyping tool intended for developing a wide variety of mains-powered and battery-powered products with Indoor Air Quality monitoring capability.

 

 

The Hat features an on-board calibrated ZMOD4410 sensor which measures the concentrations of Total Volatile Organic Compounds (TVOC) and can estimate carbon dioxide (eCO2) levels. These are important indicators for monitoring Indoor Air Quality.

Avnet IDT ZMOD4410 Indoor Air Quality Raspberry Pi Hat

BUY NOW

 

The ZMOD4410 sensor device is a small module containing a low-power programmable signal conditioning IC and a specially-developed MEMS gas sensing element. Under software direction, the ZMOD4410 precisely controls the internal temperature of its sensing element, allowing for the detection of a wide range of indoor air contaminants by accurately measuring the sensing element’s conductivity and resistance. This flexibility makes the ZMOD4410 capable of providing a variety of measurement options by varying the method of operation or changing the firmware used to operate it. Downloadable libraries provided by IDT under license make upgrades straightforward to implement. All sensors are electrically and chemically (gas) tested with calibration data stored in the ZMOD4410’s built-in nonvolatile memory.

 

 

Note that the associated libraries may be obtained from IDT; they are not included with the Avnet ZMOD4410 Indoor Air Quality Sensor Raspberry Pi Hat. To validate the Hat’s operation and begin measuring TVOC and eCO2, Avnet provides a pre-compiled application built with those libraries which runs under Raspbian, the official supported operating system for the Raspberry Pi. In addition to the ZMOD4410, the Hat includes an IDT HS3001 Precision Relative Humidity and Temperature Sensor, along with software-controlled status LEDs.

 

 

ZMOD4410 Gas Sensor Module

The ZMOD4410 Gas Sensor Module is designed for detecting total volatile organic compounds (TVOC) and monitoring indoor air quality (IAQ). It is a 12-pin LGA assembly (3.0 x 3.0 x 0.7 mm) that consists of a gas sense element and a CMOS signal conditioning IC. The module’s sense element consists of a heater element on a Si-based MEMS structure and a metal oxide (MOx) chemiresistor. The signal conditioner controls the sensor temperature and measures the MOx conductivity, which is a function of the gas concentration.

 

The measurement results can be read via an I2C interface with the user’s microprocessor, which processes the data to determine the TVOC concentration, IAQ rating and estimated carbon dioxide (eCO2) level. This flexibility makes the sensors in the ZMOD4410 platform capable of providing a variety of measurement options by varying the method of operation or changing the firmware used to interpret the resistance measurements. Downloadable firmware libraries and source code provided by IDT enables detection of TVOC and odors  and supports smart devices measuring IAQ that require low-power operation. The ZMOD4410 is ideal for applications such as thermostats, air purifiers, building controls, smart fans, HVAC equipment, and smart devices.

 

 

Benefits

  • Convenient Raspberry Pi Hat form factor for evaluation, development and quick-prototyping of products that monitor Indoor Air Quality
  • Detects a wide range of TVOC, from parts-per-billion to parts-per-million and provides eCO2 levels
  • Sensors are chemically tested and factory calibrated
  • On-board user-adjustable power supply option and current measurement connection points
  • Configurable alarm/interrupt output
  • Supplied with pre-compiled Raspbian application
  • IDT offers licensed downloadable compiled code, enabling a product road map of indoor air measurement innovation

Applications

  • Smart home appliances
  • Smart thermostats, smart speakers, smart fans, smoke alarms, vacuum cleaners, garage openers, security systems, HVAC, air purifiers, and building automation

Additional Information

Terms and Conditions

Avnet IDT ZMOD4410 Indoor Air Quality Raspberry Pi – RoadTest

Terms and Conditions

These are the terms and conditions which govern the Avnet IDT ZMOD4410 Indoor Air Quality Raspberry Pi RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

 

Key dates:

Applications Close: midnight (GMT) on October 30 2020

Announcement of Winner (estimated): Nov 4 2020

Prize: Avnet IDT ZMOD4410 Indoor Air Quality Raspberry Pi

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.


Comments

ALSO ENROLLING

Enrollment Closes: Nov 12 
Enroll
Enrollment Closes: Oct 29 
Enroll
Enrollment Closes: Nov 11 
Enroll
Enrollment Closes: Oct 29 
Enroll
Enrollment Closes: Oct 26 
Enroll

Roadtesters

No new members have been added recently.