4 Replies Latest reply on Jan 4, 2020 11:59 AM by marcelheijkoop

    External 5v supply  instructions missing in user manual?

    superpat

      Hi,

       

      I am making the assumption that one can power the audio card AND the Pi from the Aux 5V jack, thus avoiding the need for TWO power supplies.

       

      Just tried to use the Wolfson audio card with external 5V supply (5v Aux), so I can try the integrated speaker amplifiers.

       

      It will not work  without adding a link or 0 ohm resistor  R44, located by the side of the 5v jack socket. without this link, the aux 5v does NOT feed the internal 3.3 and 1.8 v regs.

       

      (see schematic diagrams.....  R44 is marked as DNP  do not populate, )

       

      The  user  manual states that one has to add terminations for the speaker cables and also

       

       It is necessary to supply auxiliary power to the Audio Card in order to drive
      external loudspeakers. An external power supply with output voltage of 5V,
      current delivery capability of 2,000mA, a centre positive power plug of internal
      diameter 2.1mm, and external diameter 5.5mm.

       

      But there is nothing about  inserting 0 ohm or link in R44

       

      SHOULD THERE BE?

       

      Also, adding a link to R44 position is not for the inexperienced solderer! It's a 0603  size component.

       

      regards

       

      Patrick

       

      Message was edited by: Patrick Keane