1 22 23 24 25 26 389 Replies Latest reply on Aug 4, 2020 3:16 AM by nonsensus Go to original post
      • 360. Re: New reworked driver for Wolfson/Cirrus Logic audio card
        hiassoft

        Double-check if your configuration is correct. If you still can't get it working please post the dmesg, vcdbg log etc info as described in the Troubleshooting section here RPi Linux driver for Wolfson / Cirrus Logic Audio Card

         

        so long,

         

        Hias

        • 361. Re: New reworked driver for Wolfson/Cirrus Logic audio card
          ebw44

          I'm trying to setup a raspberry (Model B Revision 2.0) with the wolfson audio card (rev A02). I'm not sure if the drivers in the lastest Raspbian are compatible with that hardware. Following the directions from RPi Linux driver for Wolfson / Cirrus Logic Audio Card  I cannot get aplay to play a wav file (which does work through the pi jack or hdmi). The error I get is:

          aplay: pcm_write:2011: write error: Input/output error

          And here is the output of the troubleshooting commands:

          pi@raspberrypi:~ $ paste /boot/config.txt

          # For more options and information see

          # http://rpf.io/configtxt

          # Some settings may impact device functionality. See link above for details

           

          # uncomment if you get no picture on HDMI for a default "safe" mode

          #hdmi_safe=1

           

          # uncomment this if your display has a black border of unused pixels visible

          # and your display can output without overscan

          #disable_overscan=1

           

          # uncomment the following to adjust overscan. Use positive numbers if console

          # goes off screen, and negative if there is too much border

          #overscan_left=16

          #overscan_right=16

          #overscan_top=16

          #overscan_bottom=16

           

          # uncomment to force a console size. By default it will be display's size minus

          # overscan.

          #framebuffer_width=1280

          #framebuffer_height=720

           

          # uncomment if hdmi display is not detected and composite is being output

          #hdmi_force_hotplug=1

           

          # uncomment to force a specific HDMI mode (this will force VGA)

          #hdmi_group=1

          #hdmi_mode=1

           

          # uncomment to force a HDMI mode rather than DVI. This can make audio work in

          # DMT (computer monitor) modes

          #hdmi_drive=2

           

          # uncomment to increase signal to HDMI, if you have interference, blanking, or

          # no display

          #config_hdmi_boost=4

           

          # uncomment for composite PAL

          #sdtv_mode=2

           

          #uncomment to overclock the arm. 700 MHz is the default.

          #arm_freq=800

           

          # Uncomment some or all of these to enable the optional hardware interfaces

          #dtparam=i2c_arm=on

          #dtparam=i2s=on

          #dtparam=spi=on

           

          # Uncomment this to enable the lirc-rpi module

          #dtoverlay=lirc-rpi

           

          # Additional overlays and parameters are documented /boot/overlays/README

           

          # Enable audio (loads snd_bcm2835)

          #dtparam=audio=on

          dtoverlay=rpi-cirrus-wm5102

          dtdebug=1

           

          B

           

          pi@raspberrypi:~ $ vcgencmd version | paste

          Jun  7 2018 15:31:38

          Copyright (c) 2012 Broadcom

          version 4800f08a139d6ca1c5ecbee345ea6682e2160881 (clean) (release)

          pi@raspberrypi:~ $ sudo vcdbg log msg 2>&1 | paste

          001022.708: brfs: File read: /mfs/sd/config.txt

          001023.360: brfs: File read: 1619 bytes

          001044.627: HDMI:EDID version 1.3, 1 extensions, screen size 70x39 cm

          001044.734: HDMI:EDID features - videodef 0x80 !standby !suspend !active off; colour encoding:RGB444|YCbCr422; sRGB is not default colourspace; preferred format is native; does not support GTF

          001044.892: HDMI:EDID found preferred DMT detail timing format: 1366x768p @ 60 Hz (81)

          001044.982: HDMI:EDID found CEA detail timing format: 1280x720p @ 60 Hz (4)

          001045.068: HDMI:EDID found DMT format: code 4, 640x480p @ 60 Hz in established timing I/II

          001045.145: HDMI:EDID found DMT format: code 5, 640x480p @ 72 Hz in established timing I/II

          001045.231: HDMI:EDID found DMT format: code 6, 640x480p @ 75 Hz in established timing I/II

          001045.311: HDMI:EDID found DMT format: code 9, 800x600p @ 60 Hz in established timing I/II

          001045.397: HDMI:EDID found DMT format: code 10, 800x600p @ 72 Hz in established timing I/II

          001045.473: HDMI:EDID found DMT format: code 11, 800x600p @ 75 Hz in established timing I/II

          001045.551: HDMI:EDID found DMT format: code 16, 1024x768p @ 60 Hz in established timing I/II

          001045.629: HDMI:EDID found DMT format: code 17, 1024x768p @ 70 Hz in established timing I/II

          001045.716: HDMI:EDID found DMT format: code 18, 1024x768p @ 75 Hz in established timing I/II

          001045.851: HDMI:EDID standard timings block x 8: 0x81C0 0101 0101 0101 0101 0101 0101 0101

          001045.954: HDMI:EDID found DMT format: code 85, 1280x720p @ 60 Hz (16:9) in standard timing 0

          001059.010: HDMI:EDID parsing v3 CEA extension 0

          001059.090: HDMI:EDID monitor support - underscan IT formats:yes, basic audio:yes, yuv444:yes, yuv422:yes, #native DTD:1

          001059.186: HDMI:EDID found CEA detail timing format: 1920x1080i @ 50 Hz (20)

          001059.274: HDMI:EDID found CEA detail timing format: 1920x1080i @ 60 Hz (5)

          001059.359: HDMI:EDID found CEA detail timing format: 1280x720p @ 50 Hz (19)

          001059.443: HDMI:EDID found CEA detail timing format: 720x576p @ 50 Hz (17)

          001059.525: HDMI:EDID found CEA detail timing format: 720x480p @ 60 Hz (2)

          001059.606: HDMI:EDID found CEA format: code 4, 1280x720p @ 60Hz (native)

          001059.685: HDMI:EDID found CEA format: code 19, 1280x720p @ 50Hz

          001059.755: HDMI:EDID found CEA format: code 5, 1920x1080i @ 60Hz

          001059.829: HDMI:EDID found CEA format: code 20, 1920x1080i @ 50Hz

          001059.899: HDMI:EDID found CEA format: code 3, 720x480p @ 60Hz

          001059.976: HDMI:EDID found CEA format: code 18, 720x576p @ 50Hz

          001060.053: HDMI:EDID found CEA format: code 16, 1920x1080p @ 60Hz

          001060.125: HDMI:EDID found CEA format: code 31, 1920x1080p @ 50Hz

          001060.202: HDMI:EDID found CEA format: code 32, 1920x1080p @ 24Hz

          001060.276: HDMI:EDID found CEA format: code 33, 1920x1080p @ 25Hz

          001060.354: HDMI:EDID found CEA format: code 34, 1920x1080p @ 30Hz

          001060.425: HDMI:EDID found CEA format: code 7, 1440x480i @ 60Hz

          001060.502: HDMI:EDID found CEA format: code 22, 1440x576i @ 50Hz

          001060.594: HDMI:EDID found audio format 2 channels PCM, sample rate: 32|44|48 kHz, sample size: 16|20|24 bits

          001060.657: HDMI:EDID found Video Capability DB length 2

          001060.721: HDMI:EDID video capability: CE:3 IT:3 PT:0 QS:0

          001060.776: HDMI:EDID found HDMI VSDB length 7

          001060.842: HDMI:EDID HDMI VSDB has physical address 2.0.0.0

          001060.906: HDMI:EDID HDMI VSDB supports AI:yes, dual link DVI:no

          001060.980: HDMI:EDID HDMI VSDB deep colour support - 48-bit:no 36-bit:yes 30-bit:yes DC_yuv444:yes

          001061.042: HDMI:EDID HDMI VSDB max TMDS clock 225 MHz

          001061.100: HDMI:EDID HDMI VSDB has no latency information

          001061.184: HDMI:EDID filtering formats with pixel clock > 162 MHz or h. blanking > 1023

          001061.450: HDMI:EDID preferred mode remained as DMT (81) 1366x768p @ 60 Hz with pixel clock 85 MHz

          001075.833: brfs: File read: /mfs/sd/config.txt

          001076.352: HDMI:Setting property pixel encoding to Default

          001076.417: HDMI:Setting property pixel clock type to PAL

          001076.475: HDMI:Setting property content type flag to No data

          001076.539: HDMI:Setting property fuzzy format match to enabled

          001076.671: gpioman: gpioman_get_pin_num: pin LEDS_PWR_OK not defined

          001085.661: gpioman: gpioman_get_pin_num: pin WL_LPO_CLK not defined

          001085.734: gpioman: gpioman_get_pin_num: pin BT_ON not defined

          001085.798: gpioman: gpioman_get_pin_num: pin WL_ON not defined

          001257.909: gpioman: gpioman_get_pin_num: pin LEDS_PWR_OK not defined

          001258.008: hdmi: HDMI:>>>>>>>>>>>>>Rx sensed, reading EDID<<<<<<<<<<<<<

          001270.129: hdmi: HDMI:EDID version 1.3, 1 extensions, screen size 70x39 cm

          001270.238: hdmi: HDMI:EDID features - videodef 0x80 !standby !suspend !active off; colour encoding:RGB444|YCbCr422; sRGB is not default colourspace; preferred format is native; does not support GTF

          001270.404: hdmi: HDMI:EDID found preferred DMT detail timing format: 1366x768p @ 60 Hz (81)

          001270.498: hdmi: HDMI:EDID found CEA detail timing format: 1280x720p @ 60 Hz (4)

          001270.589: hdmi: HDMI:EDID found DMT format: code 4, 640x480p @ 60 Hz in established timing I/II

          001270.672: hdmi: HDMI:EDID found DMT format: code 5, 640x480p @ 72 Hz in established timing I/II

          001270.762: hdmi: HDMI:EDID found DMT format: code 6, 640x480p @ 75 Hz in established timing I/II

          001270.842: hdmi: HDMI:EDID found DMT format: code 9, 800x600p @ 60 Hz in established timing I/II

          001270.932: hdmi: HDMI:EDID found DMT format: code 10, 800x600p @ 72 Hz in established timing I/II

          001271.016: hdmi: HDMI:EDID found DMT format: code 11, 800x600p @ 75 Hz in established timing I/II

          001271.098: hdmi: HDMI:EDID found DMT format: code 16, 1024x768p @ 60 Hz in established timing I/II

          001271.183: hdmi: HDMI:EDID found DMT format: code 17, 1024x768p @ 70 Hz in established timing I/II

          001271.273: hdmi: HDMI:EDID found DMT format: code 18, 1024x768p @ 75 Hz in established timing I/II

          001271.408: hdmi: HDMI:EDID standard timings block x 8: 0x81C0 0101 0101 0101 0101 0101 0101 0101

          001271.515: hdmi: HDMI:EDID found DMT format: code 85, 1280x720p @ 60 Hz (16:9) in standard timing 0

          001284.576: hdmi: HDMI:EDID parsing v3 CEA extension 0

          001284.661: hdmi: HDMI:EDID monitor support - underscan IT formats:yes, basic audio:yes, yuv444:yes, yuv422:yes, #native DTD:1

          001284.762: hdmi: HDMI:EDID found CEA detail timing format: 1920x1080i @ 50 Hz (20)

          001284.854: hdmi: HDMI:EDID found CEA detail timing format: 1920x1080i @ 60 Hz (5)

          001284.940: hdmi: HDMI:EDID found CEA detail timing format: 1280x720p @ 50 Hz (19)

          001285.029: hdmi: HDMI:EDID found CEA detail timing format: 720x576p @ 50 Hz (17)

          001285.111: hdmi: HDMI:EDID found CEA detail timing format: 720x480p @ 60 Hz (2)

          001285.196: hdmi: HDMI:EDID found CEA format: code 4, 1280x720p @ 60Hz (native)

          001285.279: hdmi: HDMI:EDID found CEA format: code 19, 1280x720p @ 50Hz

          001285.353: hdmi: HDMI:EDID found CEA format: code 5, 1920x1080i @ 60Hz

          001285.427: hdmi: HDMI:EDID found CEA format: code 20, 1920x1080i @ 50Hz

          001285.501: hdmi: HDMI:EDID found CEA format: code 3, 720x480p @ 60Hz

          001285.581: hdmi: HDMI:EDID found CEA format: code 18, 720x576p @ 50Hz

          001285.662: hdmi: HDMI:EDID found CEA format: code 16, 1920x1080p @ 60Hz

          001285.740: hdmi: HDMI:EDID found CEA format: code 31, 1920x1080p @ 50Hz

          001285.822: hdmi: HDMI:EDID found CEA format: code 32, 1920x1080p @ 24Hz

          001285.896: hdmi: HDMI:EDID found CEA format: code 33, 1920x1080p @ 25Hz

          001285.977: hdmi: HDMI:EDID found CEA format: code 34, 1920x1080p @ 30Hz

          001286.054: hdmi: HDMI:EDID found CEA format: code 7, 1440x480i @ 60Hz

          001286.135: hdmi: HDMI:EDID found CEA format: code 22, 1440x576i @ 50Hz

          001286.233: hdmi: HDMI:EDID found audio format 2 channels PCM, sample rate: 32|44|48 kHz, sample size: 16|20|24 bits

          001286.300: hdmi: HDMI:EDID found Video Capability DB length 2

          001286.371: hdmi: HDMI:EDID video capability: CE:3 IT:3 PT:0 QS:0

          001286.429: hdmi: HDMI:EDID found HDMI VSDB length 7

          001286.500: hdmi: HDMI:EDID HDMI VSDB has physical address 2.0.0.0

          001286.568: hdmi: HDMI:EDID HDMI VSDB supports AI:yes, dual link DVI:no

          001286.647: hdmi: HDMI:EDID HDMI VSDB deep colour support - 48-bit:no 36-bit:yes 30-bit:yes DC_yuv444:yes

          001286.713: hdmi: HDMI:EDID HDMI VSDB max TMDS clock 225 MHz

          001286.775: hdmi: HDMI:EDID HDMI VSDB has no latency information

          001286.865: hdmi: HDMI:EDID filtering formats with pixel clock > 162 MHz or h. blanking > 1023

          001287.137: hdmi: HDMI:EDID preferred mode remained as DMT (81) 1366x768p @ 60 Hz with pixel clock 85 MHz

          001287.210: hdmi: HDMI: hotplug attached with HDMI support

          001287.290: hdmi: HDMI:hdmi_get_state is deprecated, use hdmi_get_display_state instead

          001289.748: hdmi: HDMI: power_on to DMT mode 1366x768@60

          001292.973: hdmi: HDMI: Action callback added to queue to happen at frame 2

          001293.042: hdmi: HDMI: Action stop_3d_mode added to queue to happen at frame 2

          001293.106: hdmi: HDMI: Action unmute added to queue to happen at frame 3

          001293.177: hdmi: HDMI: Action cec_init added to queue to happen at frame 3

          001359.980: *** Restart logging

          001360.047: brfs: File read: 1619 bytes

          001361.584: brfs: File read: /mfs/sd/cmdline.txt

          001361.666: Read command line from file 'cmdline.txt':

          001361.729: 'dwc_otg.lpm_enable=0 console=serial0,115200 console=tty1 root=PARTUUID=71d3722f-02 rootfstype=ext4 elevator=deadline fsck.repair=yes rootwait'

          001362.054: brfs: File read: 142 bytes

          001727.566: brfs: File read: /mfs/sd/kernel.img

          001727.644: Loading 'kernel.img' to 0x8000 size 0x476898

          001727.739: No kernel trailer - assuming DT-capable

          001727.829: brfs: File read: 4679832 bytes

          001732.240: brfs: File read: /mfs/sd/bcm2708-rpi-b.dtb

          001732.304: Loading 'bcm2708-rpi-b.dtb' to 0x47e898 size 0x554f

          001815.577: brfs: File read: 21839 bytes

          001819.243: brfs: File read: /mfs/sd/config.txt

          001819.675: brfs: File read: 1619 bytes

          001833.791: brfs: File read: /mfs/sd/overlays/rpi-cirrus-wm5102.dtbo

          001867.115: Loaded overlay 'rpi-cirrus-wm5102'

          002847.695: gpioman: gpioman_get_pin_num: pin EMMC_ENABLE not defined

          002879.601: Device tree loaded to 0x1bfea100 (size 0x5e1c)

          002880.977: gpioman: gpioman_get_pin_num: pin SDCARD_CONTROL_POWER not defined

          004772.342: vchiq_core: vchiq_init_state: slot_zero = 0x5b580000, is_master = 1

          004778.144: hdmi: HDMI:hdmi_get_state is deprecated, use hdmi_get_display_state instead

          004784.118: TV service:host side not connected, dropping notification 0x00000002, 0x00000002, 0x00000051

          pi@raspberrypi:~ $ dmesg | paste

          [    0.000000] Booting Linux on physical CPU 0x0

          [    0.000000] Linux version 4.14.50+ (dc4@dc4-XPS13-9333) (gcc version 4.9.3 (crosstool-NG crosstool-ng-1.22.0-88-g8460611)) #1122 Tue Jun 19 12:21:21 BST 2018

          [    0.000000] CPU: ARMv6-compatible processor [410fb767] revision 7 (ARMv7), cr=00c5387d

          [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT nonaliasing instruction cache

          [    0.000000] OF: fdt: Machine model: Raspberry Pi Model B Rev 2

          [    0.000000] Memory policy: Data cache writeback

          [    0.000000] cma: Reserved 8 MiB at 0x1b400000

          [    0.000000] On node 0 totalpages: 114688

          [    0.000000] free_area_init_node: node 0, pgdat c09c04f8, node_mem_map db010000

          [    0.000000]   Normal zone: 1008 pages used for memmap

          [    0.000000]   Normal zone: 0 pages reserved

          [    0.000000]   Normal zone: 114688 pages, LIFO batch:31

          [    0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768

          [    0.000000] pcpu-alloc: [0] 0

          [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 113680

          [    0.000000] Kernel command line: bcm2708_fb.fbwidth=1366 bcm2708_fb.fbheight=768 bcm2708_fb.fbswap=1 vc_mem.mem_base=0x1ec00000 vc_mem.mem_size=0x20000000  dwc_otg.lpm_enable=0 console=ttyAMA0,115200 console=tty1 root=PARTUUID=71d3722f-02 rootfstype=ext4 elevator=deadline fsck.repair=yes rootwait

          [    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)

          [    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

          [    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

          [    0.000000] Memory: 435256K/458752K available (6421K kernel code, 587K rwdata, 1988K rodata, 440K init, 677K bss, 15304K reserved, 8192K cma-reserved)

          [    0.000000] Virtual kernel memory layout:

                             vector  : 0xffff0000 - 0xffff1000   (   4 kB)

                             fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)

                             vmalloc : 0xdc800000 - 0xff800000   ( 560 MB)

                             lowmem  : 0xc0000000 - 0xdc000000   ( 448 MB)

                             modules : 0xbf000000 - 0xc0000000   (  16 MB)

                               .text : 0xc0008000 - 0xc064d94c   (6423 kB)

                               .init : 0xc08ca000 - 0xc0938000   ( 440 kB)

                               .data : 0xc0938000 - 0xc09cae90   ( 588 kB)

                                .bss : 0xc09d07d0 - 0xc0a79d24   ( 678 kB)

          [    0.000000] SLUB: HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

          [    0.000000] ftrace: allocating 24091 entries in 71 pages

          [    0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16

          [    0.000029] sched_clock: 32 bits at 1000kHz, resolution 1000ns, wraps every 2147483647500ns

          [    0.000071] clocksource: timer: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 1911260446275 ns

          [    0.000165] bcm2835: system timer (irq = 27)

          [    0.000740] Console: colour dummy device 80x30

          [    0.001316] console [tty1] enabled

          [    0.001367] Calibrating delay loop... 697.95 BogoMIPS (lpj=3489792)

          [    0.060334] pid_max: default: 32768 minimum: 301

          [    0.060850] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)

          [    0.060907] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)

          [    0.062216] Disabling memory control group subsystem

          [    0.062431] CPU: Testing write buffer coherency: ok

          [    0.063561] Setting up static identity map for 0x8200 - 0x8238

          [    0.064853] devtmpfs: initialized

          [    0.073957] random: get_random_u32 called from bucket_table_alloc+0x88/0x1c4 with crng_init=0

          [    0.074822] VFP support v0.3: implementor 41 architecture 1 part 20 variant b rev 5

          [    0.075273] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns

          [    0.075345] futex hash table entries: 256 (order: -1, 3072 bytes)

          [    0.076687] pinctrl core: initialized pinctrl subsystem

          [    0.078069] NET: Registered protocol family 16

          [    0.081028] DMA: preallocated 1024 KiB pool for atomic coherent allocations

          [    0.087421] hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.

          [    0.087493] hw-breakpoint: maximum watchpoint size is 4 bytes.

          [    0.087645] Serial: AMBA PL011 UART driver

          [    0.090704] bcm2835-mbox 2000b880.mailbox: mailbox enabled

          [    0.131363] bcm2835-dma 20007000.dma: DMA legacy API manager at dc80d000, dmachans=0x1

          [    0.133614] SCSI subsystem initialized

          [    0.133904] usbcore: registered new interface driver usbfs

          [    0.134038] usbcore: registered new interface driver hub

          [    0.134268] usbcore: registered new device driver usb

          [    0.140804] raspberrypi-firmware soc:firmware: Attached to firmware from 2018-06-07 15:31

          [    0.142808] clocksource: Switched to clocksource timer

          [    0.229597] VFS: Disk quotas dquot_6.6.0

          [    0.229779] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

          [    0.230106] FS-Cache: Loaded

          [    0.230470] CacheFiles: Loaded

          [    0.247469] NET: Registered protocol family 2

          [    0.248701] TCP established hash table entries: 4096 (order: 2, 16384 bytes)

          [    0.248836] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)

          [    0.248956] TCP: Hash tables configured (established 4096 bind 4096)

          [    0.249136] UDP hash table entries: 256 (order: 0, 4096 bytes)

          [    0.249195] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

          [    0.249579] NET: Registered protocol family 1

          [    0.250320] RPC: Registered named UNIX socket transport module.

          [    0.250375] RPC: Registered udp transport module.

          [    0.250402] RPC: Registered tcp transport module.

          [    0.250427] RPC: Registered tcp NFSv4.1 backchannel transport module.

          [    0.252312] hw perfevents: no irqs for PMU, sampling events not supported

          [    0.252434] hw perfevents: enabled with armv6_1176 PMU driver, 3 counters available

          [    0.256234] workingset: timestamp_bits=14 max_order=17 bucket_order=3

          [    0.268471] FS-Cache: Netfs 'nfs' registered for caching

          [    0.269857] NFS: Registering the id_resolver key type

          [    0.269949] Key type id_resolver registered

          [    0.269980] Key type id_legacy registered

          [    0.270028] nfs4filelayout_init: NFSv4 File Layout Driver Registering...

          [    0.274802] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 251)

          [    0.275280] io scheduler noop registered

          [    0.275330] io scheduler deadline registered (default)

          [    0.275908] io scheduler cfq registered

          [    0.275957] io scheduler mq-deadline registered

          [    0.275986] io scheduler kyber registered

          [    0.278284] BCM2708FB: allocated DMA memory 5b500000

          [    0.278397] BCM2708FB: allocated DMA channel 0 @ dc80d000

          [    0.304487] Console: switching to colour frame buffer device 170x48

          [    0.326870] bcm2835-rng 20104000.rng: hwrng registered

          [    0.327339] vc-mem: phys_addr:0x00000000 mem_base=0x1ec00000 mem_size:0x20000000(512 MiB)

          [    0.328665] vc-sm: Videocore shared memory driver

          [    0.329527] gpiomem-bcm2835 20200000.gpiomem: Initialised: Registers at 0x20200000

          [    0.349467] brd: module loaded

          [    0.362259] loop: module loaded

          [    0.362451] Loading iSCSI transport class v2.0-870.

          [    0.363734] usbcore: registered new interface driver smsc95xx

          [    0.364002] dwc_otg: version 3.00a 10-AUG-2012 (platform bus)

          [    0.592635] Core Release: 2.80a

          [    0.592879] Setting default values for core params

          [    0.593105] Finished setting default values for core params

          [    0.793600] Using Buffer DMA mode

          [    0.799777] Periodic Transfer Interrupt Enhancement - disabled

          [    0.805964] Multiprocessor Interrupt Enhancement - disabled

          [    0.812081] OTG VER PARAM: 0, OTG VER FLAG: 0

          [    0.818248] Dedicated Tx FIFOs mode

          [    0.825328] WARN::dwc_otg_hcd_init:1046: FIQ DMA bounce buffers: virt = 0xdb514000 dma = 0x5b514000 len=9024

          [    0.831672] FIQ FSM acceleration enabled for :

                         Non-periodic Split Transactions

                         Periodic Split Transactions

                         High-Speed Isochronous Endpoints

                         Interrupt/Control Split Transaction hack enabled

          [    0.862483] dwc_otg: Microframe scheduler enabled

          [    0.862755] WARN::hcd_init_fiq:459: FIQ on core 0 at 0xc049a168

          [    0.869046] WARN::hcd_init_fiq:460: FIQ ASM at 0xc049a444 length 36

          [    0.875282] WARN::hcd_init_fiq:486: MPHI regs_base at 0xdc8a5000

          [    0.881547] dwc_otg 20980000.usb: DWC OTG Controller

          [    0.887793] dwc_otg 20980000.usb: new USB bus registered, assigned bus number 1

          [    0.894067] dwc_otg 20980000.usb: irq 56, io mem 0x00000000

          [    0.900155] Init: Port Power? op_state=1

          [    0.906244] Init: Power Port (0)

          [    0.912693] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

          [    0.918949] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

          [    0.925128] usb usb1: Product: DWC OTG Controller

          [    0.931083] usb usb1: Manufacturer: Linux 4.14.50+ dwc_otg_hcd

          [    0.937169] usb usb1: SerialNumber: 20980000.usb

          [    0.944495] hub 1-0:1.0: USB hub found

          [    0.950680] hub 1-0:1.0: 1 port detected

          [    0.957931] dwc_otg: FIQ enabled

          [    0.957943] dwc_otg: NAK holdoff enabled

          [    0.957952] dwc_otg: FIQ split-transaction FSM enabled

          [    0.957971] Module dwc_common_port init

          [    0.958505] usbcore: registered new interface driver usb-storage

          [    0.965379] mousedev: PS/2 mouse device common for all mice

          [    0.971679] IR NEC protocol handler initialized

          [    0.977958] IR RC5(x/sz) protocol handler initialized

          [    0.984140] IR RC6 protocol handler initialized

          [    0.990253] IR JVC protocol handler initialized

          [    0.996237] IR Sony protocol handler initialized

          [    1.002048] IR SANYO protocol handler initialized

          [    1.007873] IR Sharp protocol handler initialized

          [    1.013560] IR MCE Keyboard/mouse protocol handler initialized

          [    1.019293] IR XMP protocol handler initialized

          [    1.026519] bcm2835-wdt 20100000.watchdog: Broadcom BCM2835 watchdog timer

          [    1.033044] bcm2835-cpufreq: min=700000 max=700000

          [    1.039610] sdhci: Secure Digital Host Controller Interface driver

          [    1.045592] sdhci: Copyright(c) Pierre Ossman

          [    1.052109] sdhost-bcm2835 20202000.mmc: could not get clk, deferring probe

          [    1.058433] sdhci-pltfm: SDHCI platform and OF driver helper

          [    1.065291] ledtrig-cpu: registered to indicate activity on CPUs

          [    1.071480] hidraw: raw HID events driver (C) Jiri Kosina

          [    1.077786] usbcore: registered new interface driver usbhid

          [    1.083761] usbhid: USB HID core driver

          [    1.090654] vchiq: vchiq_init_state: slot_zero = db580000, is_master = 0

          [    1.098742] [vc_sm_connected_init]: start

          [    1.110376] [vc_sm_connected_init]: end - returning 0

          [    1.117515] Initializing XFRM netlink socket

          [    1.123654] NET: Registered protocol family 17

          [    1.129609] Key type dns_resolver registered

          [    1.137159] registered taskstats version 1

          [    1.151074] uart-pl011 20201000.serial: cts_event_workaround enabled

          [    1.157346] 20201000.serial: ttyAMA0 at MMIO 0x20201000 (irq = 81, base_baud = 0) is a PL011 rev2

          [    2.064540] console [ttyAMA0] enabled

          [    2.077917] Indeed it is in host mode hprt0 = 00021501

          [    2.149881] sdhost: log_buf @ db513000 (5b513000)

          [    2.162795] random: fast init done

          [    2.252895] mmc0: sdhost-bcm2835 loaded - DMA enabled (>1)

          [    2.266266] of_cfs_init

          [    2.295208] usb 1-1: new high-speed USB device number 2 using dwc_otg

          [    2.308118] of_cfs_init: OK

          [    2.318278] Waiting for root device PARTUUID=71d3722f-02...

          [    2.330505] Indeed it is in host mode hprt0 = 00001101

          [    2.450737] mmc0: host does not support reading read-only switch, assuming write-enable

          [    2.468238] mmc0: new high speed SDHC card at address 1234

          [    2.481439] mmcblk0: mmc0:1234 SA08G 7.42 GiB

          [    2.495282]  mmcblk0: p1 p2

          [    2.539828] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)

          [    2.555082] VFS: Mounted root (ext4 filesystem) readonly on device 179:2.

          [    2.579745] devtmpfs: mounted

          [    2.589942] usb 1-1: New USB device found, idVendor=0424, idProduct=9514

          [    2.603466] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0

          [    2.620066] Freeing unused kernel memory: 440K

          [    2.631340] This architecture does not have kernel memory protection.

          [    2.646008] hub 1-1:1.0: USB hub found

          [    2.659696] hub 1-1:1.0: 5 ports detected

          [    2.992950] usb 1-1.1: new high-speed USB device number 3 using dwc_otg

          [    3.133674] usb 1-1.1: New USB device found, idVendor=0424, idProduct=ec00

          [    3.147529] usb 1-1.1: New USB device strings: Mfr=0, Product=0, SerialNumber=0

          [    3.165756] smsc95xx v1.0.6

          [    3.270280] smsc95xx 1-1.1:1.0 eth0: register 'smsc95xx' at usb-20980000.usb-1.1, smsc95xx USB 2.0 Ethernet, b8:27:eb:1c:1d:27

          [    3.309951] systemd[1]: System time before build time, advancing clock.

          [    3.392952] usb 1-1.2: new low-speed USB device number 4 using dwc_otg

          [    3.501425] NET: Registered protocol family 10

          [    3.516013] Segment Routing with IPv6

          [    3.553513] ip_tables: (C) 2000-2006 Netfilter Core Team

          [    3.567591] usb 1-1.2: New USB device found, idVendor=046d, idProduct=c00e

          [    3.581694] usb 1-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=0

          [    3.596078] usb 1-1.2: Product: USB-PS/2 Optical Mouse

          [    3.608299] usb 1-1.2: Manufacturer: Logitech

          [    3.644439] input: Logitech USB-PS/2 Optical Mouse as /devices/platform/soc/20980000.usb/usb1/1-1/1-1.2/1-1.2:1.0/0003:046D:C00E.0001/input/input0

          [    3.667346] hid-generic 0003:046D:C00E.0001: input,hidraw0: USB HID v1.10 Mouse [Logitech USB-PS/2 Optical Mouse] on usb-20980000.usb-1.2/input0

          [    3.690125] random: systemd: uninitialized urandom read (16 bytes read)

          [    3.714963] systemd[1]: systemd 232 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD +IDN)

          [    3.750919] systemd[1]: Detected architecture arm.

          [    3.792973] systemd[1]: Set hostname to <raspberrypi>.

          [    3.812949] usb 1-1.3: new high-speed USB device number 5 using dwc_otg

          [    3.888760] random: systemd: uninitialized urandom read (16 bytes read)

          [    3.954333] usb 1-1.3: New USB device found, idVendor=2001, idProduct=3319

          [    3.969530] usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=3

          [    3.984974] usb 1-1.3: Product: Wireless N Nano USB Adapter

          [    3.998637] usb 1-1.3: Manufacturer: Realtek

          [    4.010914] usb 1-1.3: SerialNumber: 00e04c000001

          [    4.158613] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read)

          [    4.364130] uart-pl011 20201000.serial: no DMA platform data

          [    5.054807] systemd[1]: Set up automount Arbitrary Executable File Formats File System Automount Point.

          [    5.083663] systemd[1]: Listening on udev Control Socket.

          [    5.107960] systemd[1]: Listening on Journal Socket.

          [    5.132659] systemd[1]: Created slice System Slice.

          [    5.157633] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.

          [    5.189563] systemd[1]: Starting Set the console keyboard layout...

          [    5.226726] systemd[1]: Started Forward Password Requests to Wall Directory Watch.

          [    8.027758] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)

          [    8.939159] systemd-journald[87]: Received request to flush runtime journal from PID 1

          [   11.676618] snd-rpi-cirrus soc:sound: ASoC: CODEC DAI wm5102-aif1 not registered - will retry

          [   15.565259] 8192eu: loading out-of-tree module taints kernel.

          [   17.088715] RTL871X: module init start

          [   17.088737] RTL871X: rtl8192eu v4.4.1_17696.20160509_BTCOEX20160412-0042

          [   17.088743] RTL871X: build time: Aug 26 2018 15:52:50

          [   17.088748] RTL871X: rtl8192eu BT-Coex version = BTCOEX20160412-0042

          [   17.384075] smsc95xx 1-1.1:1.0 eth0: hardware isn't capable of remote wakeup

          [   18.892616] smsc95xx 1-1.1:1.0 eth0: link up, 100Mbps, full-duplex, lpa 0xC1E1

          [   18.945994] Adding 102396k swap on /var/swap.  Priority:-2 extents:1 across:102396k SSFS

          [   19.550928] RTL871X: hal_com_config_channel_plan chplan:0x21

          [   19.562053] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562075] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562082] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562089] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562095] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562101] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562107] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562114] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562120] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562126] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562132] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562138] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562144] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562150] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562156] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562162] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562168] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562175] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562181] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562187] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562194] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562266] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562275] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562282] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562288] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562294] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562300] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562307] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562312] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562322] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562329] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562335] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562343] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562350] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562356] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562362] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562368] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562374] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562380] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562386] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562392] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562399] RTL871X: Wrong rate section: (CCK,2T)

          [   19.562490] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562501] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562508] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562515] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562521] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562527] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562534] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562540] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562546] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562552] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562558] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562564] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562572] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562579] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562585] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562591] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562597] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562603] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562610] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562616] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562622] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562628] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562634] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562641] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562647] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562653] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562659] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562665] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562671] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562677] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562683] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562690] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562697] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562703] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562709] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562715] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562721] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562727] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562733] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562740] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562746] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.562752] RTL871X: Wrong rate section: (OFDM,2T)

          [   19.563016] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 20M][rate section HT][rf path 2T][chnl 01]

          [   19.563033] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 20M][rate section HT][rf path 2T][chnl 01]

          [   19.563043] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 20M][rate section HT][rf path 2T][chnl 01]

          [   19.563053] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 20M][rate section HT][rf path 2T][chnl 02]

          [   19.563063] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 20M][rate section HT][rf path 2T][chnl 02]

          [   19.563074] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 20M][rate section HT][rf path 2T][chnl 02]

          [   19.563085] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 20M][rate section HT][rf path 2T][chnl 03]

          [   19.563094] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 20M][rate section HT][rf path 2T][chnl 03]

          [   19.563105] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 20M][rate section HT][rf path 2T][chnl 03]

          [   19.563114] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 20M][rate section HT][rf path 2T][chnl 04]

          [   19.563124] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 20M][rate section HT][rf path 2T][chnl 04]

          [   19.563133] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 20M][rate section HT][rf path 2T][chnl 04]

          [   19.563142] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 20M][rate section HT][rf path 2T][chnl 05]

          [   19.563152] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 20M][rate section HT][rf path 2T][chnl 05]

          [   19.563161] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 20M][rate section HT][rf path 2T][chnl 05]

          [   19.563170] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 20M][rate section HT][rf path 2T][chnl 06]

          [   19.563180] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 20M][rate section HT][rf path 2T][chnl 06]

          [   19.563189] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 20M][rate section HT][rf path 2T][chnl 06]

          [   19.563199] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 20M][rate section HT][rf path 2T][chnl 07]

          [   19.563210] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 20M][rate section HT][rf path 2T][chnl 07]

          [   19.563219] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 20M][rate section HT][rf path 2T][chnl 07]

          [   19.563229] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 20M][rate section HT][rf path 2T][chnl 08]

          [   19.563238] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 20M][rate section HT][rf path 2T][chnl 08]

          [   19.563247] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 20M][rate section HT][rf path 2T][chnl 08]

          [   19.563256] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 20M][rate section HT][rf path 2T][chnl 09]

          [   19.563266] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 20M][rate section HT][rf path 2T][chnl 09]

          [   19.563275] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 20M][rate section HT][rf path 2T][chnl 09]

          [   19.563284] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 20M][rate section HT][rf path 2T][chnl 10]

          [   19.563294] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 20M][rate section HT][rf path 2T][chnl 10]

          [   19.563303] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 20M][rate section HT][rf path 2T][chnl 10]

          [   19.563312] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 20M][rate section HT][rf path 2T][chnl 11]

          [   19.563323] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 20M][rate section HT][rf path 2T][chnl 11]

          [   19.563332] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 20M][rate section HT][rf path 2T][chnl 11]

          [   19.563344] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 20M][rate section HT][rf path 2T][chnl 12]

          [   19.563353] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 20M][rate section HT][rf path 2T][chnl 12]

          [   19.563365] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 20M][rate section HT][rf path 2T][chnl 13]

          [   19.563374] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 20M][rate section HT][rf path 2T][chnl 13]

          [   19.563518] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 40M][rate section HT][rf path 2T][chnl 03]

          [   19.563528] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 40M][rate section HT][rf path 2T][chnl 03]

          [   19.563538] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 40M][rate section HT][rf path 2T][chnl 03]

          [   19.563547] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 40M][rate section HT][rf path 2T][chnl 04]

          [   19.563557] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 40M][rate section HT][rf path 2T][chnl 04]

          [   19.563566] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 40M][rate section HT][rf path 2T][chnl 04]

          [   19.563576] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 40M][rate section HT][rf path 2T][chnl 05]

          [   19.563587] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 40M][rate section HT][rf path 2T][chnl 05]

          [   19.563597] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 40M][rate section HT][rf path 2T][chnl 05]

          [   19.563606] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 40M][rate section HT][rf path 2T][chnl 06]

          [   19.563617] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 40M][rate section HT][rf path 2T][chnl 06]

          [   19.563626] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 40M][rate section HT][rf path 2T][chnl 06]

          [   19.563637] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 40M][rate section HT][rf path 2T][chnl 07]

          [   19.563647] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 40M][rate section HT][rf path 2T][chnl 07]

          [   19.563656] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 40M][rate section HT][rf path 2T][chnl 07]

          [   19.563665] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 40M][rate section HT][rf path 2T][chnl 08]

          [   19.563675] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 40M][rate section HT][rf path 2T][chnl 08]

          [   19.563684] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 40M][rate section HT][rf path 2T][chnl 08]

          [   19.563694] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 40M][rate section HT][rf path 2T][chnl 09]

          [   19.563703] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 40M][rate section HT][rf path 2T][chnl 09]

          [   19.563713] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 40M][rate section HT][rf path 2T][chnl 09]

          [   19.563723] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 40M][rate section HT][rf path 2T][chnl 10]

          [   19.563734] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 40M][rate section HT][rf path 2T][chnl 10]

          [   19.563743] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 40M][rate section HT][rf path 2T][chnl 10]

          [   19.563752] RTL871X: duplicate tx power limit combination [band 2.4G][regulation FCC][bw 40M][rate section HT][rf path 2T][chnl 11]

          [   19.563762] RTL871X: duplicate tx power limit combination [band 2.4G][regulation ETSI][bw 40M][rate section HT][rf path 2T][chnl 11]

          [   19.563771] RTL871X: duplicate tx power limit combination [band 2.4G][regulation MKK][bw 40M][rate section HT][rf path 2T][chnl 11]

          [   19.658674] random: crng init done

          [   19.658699] random: 7 urandom warning(s) missed due to ratelimiting

          [   19.663787] RTL871X: rtw_ndev_init(wlan0) if1 mac_addr=54:2a:a2:83:be:6d

          [   19.713533] snd-rpi-cirrus soc:sound: ASoC: CODEC DAI wm5102-aif1 not registered - will retry

          [   19.713911] usbcore: registered new interface driver rtl8192eu

          [   19.713923] RTL871X: module init ret=0

          [   20.030267] arizona spi0.1: Failed to get mclk1: -2

          [   20.030300] arizona spi0.1: Failed to get mclk2: -2

          [   20.030831] LDO1: supplied by RPi-Cirrus 1v8

          [   20.031724] snd-rpi-cirrus soc:sound: ASoC: CODEC DAI wm5102-aif1 not registered - will retry

          [   20.104756] arizona spi0.1: WM5102 revision C

          [   20.201903] Adding alias for supply MICVDD,(null) -> MICVDD,spi0.1

          [   20.209459] Adding alias for supply MICVDD,(null) -> MICVDD,spi0.1

          [   20.209481] Adding alias for supply DBVDD2,(null) -> DBVDD2,spi0.1

          [   20.209490] Adding alias for supply DBVDD3,(null) -> DBVDD3,spi0.1

          [   20.209497] Adding alias for supply CPVDD,(null) -> CPVDD,spi0.1

          [   20.209505] Adding alias for supply SPKVDDL,(null) -> SPKVDDL,spi0.1

          [   20.209512] Adding alias for supply SPKVDDR,(null) -> SPKVDDR,spi0.1

          [   20.210224] snd-rpi-cirrus soc:sound: ASoC: CODEC DAI wm5102-aif1 not registered - will retry

          [   20.378032] wm8804 1-003b: revision E

          [   20.379011] snd-rpi-cirrus soc:sound: ASoC: CODEC DAI wm5102-aif1 not registered - will retry

          [   20.448487] snd-rpi-cirrus soc:sound: ASoC: CODEC DAI wm5102-aif1 not registered - will retry

          [   20.542596] MICVDD: supplied by RPi-Cirrus 1v8

          [   20.559674] snd-rpi-cirrus soc:sound: ASoC: CODEC DAI wm5102-aif1 not registered - will retry

          [   21.154124] snd-rpi-cirrus soc:sound: wm5102-aif1 <-> 20203000.i2s mapping ok

          [   24.060186] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready

          [   26.082930] RTL871X: nolinked power save enter

          [   65.749734] bcm2835-i2s 20203000.i2s: I2S SYNC error!

          [   92.645061] bcm2835-dma 20007000.dma: DMA transfer could not be terminated

          [  282.645964] bcm2835-i2s 20203000.i2s: I2S SYNC error!

          [  282.647131] bcm2835-i2s 20203000.i2s: I2S SYNC error!

          [  282.712384] arizona spi0.1: ASRC underclocked

          [  303.213388] bcm2835-dma 20007000.dma: DMA transfer could not be terminated

          pi@raspberrypi:~ $ lsmod | paste

          Module                  Size  Used by

          snd_soc_wm5102        373712  1

          snd_soc_wm_adsp        35582  1 snd_soc_wm5102

          snd_soc_arizona        37115  1 snd_soc_wm5102

          arizona_micsupp         3513  1

          gpio_arizona            2839  0

          snd_soc_wm8804_i2c      1986  1

          snd_soc_wm8804          9488  1 snd_soc_wm8804_i2c

          arizona_spi             1971  0

          arizona_ldo1            3848  1

          8192eu               1146036  0

          evdev                  11644  1

          cfg80211              542242  1 8192eu

          rfkill                 21476  3 cfg80211

          snd_soc_rpi_cirrus     13936  0

          snd_soc_bcm2835_i2s     7385  2

          regmap_mmio             3874  1 snd_soc_bcm2835_i2s

          snd_soc_core          178157  7 snd_soc_wm8804,snd_soc_rpi_cirrus,snd_soc_wm5102,arizona_micsupp,snd_soc_bcm2835_i2s,snd_soc_arizona,snd_soc_wm_adsp

          snd_compress            9956  2 snd_soc_core,snd_soc_wm_adsp

          snd_pcm_dmaengine       5370  1 snd_soc_core

          i2c_bcm2835             6465  0

          snd_pcm                89590  6 snd_soc_wm8804,snd_soc_rpi_cirrus,snd_pcm_dmaengine,snd_soc_bcm2835_i2s,snd_soc_arizona,snd_soc_core

          snd_timer              22396  1 snd_pcm

          spi_bcm2835             7456  0

          snd                    60154  5 snd_compress,snd_soc_rpi_cirrus,snd_timer,snd_soc_core,snd_pcm

          uio_pdrv_genirq         3718  0

          uio                     9901  1 uio_pdrv_genirq

          fixed                   3033  11

          ip_tables              12427  0

          x_tables               22098  1 ip_tables

          ipv6                  401778  18

          pi@raspberrypi:~ $ aplay -l | paste

          **** List of PLAYBACK Hardware Devices ****

          card 0: RPiCirrus [RPi-Cirrus], device 0: WM5102 AiFi wm5102-aif1-0 []

            Subdevices: 1/1

            Subdevice #0: subdevice #0

           

          Thanks to anyone that can give me any advice

          • 362. Re: New reworked driver for Wolfson/Cirrus Logic audio card
            hiassoft

            ebw44  schrieb:

             

            I'm trying to setup a raspberry (Model B Revision 2.0) with the wolfson audio card (rev A02). I'm not sure if the drivers in the lastest Raspbian are compatible with that hardware. Following the directions from RPi Linux driver for Wolfson / Cirrus Logic Audio Card  I cannot get aplay to play a wav file (which does work through the pi jack or hdmi). The error I get is:

            aplay: pcm_write:2011: write error: Input/output error

            ....

            [   92.645061] bcm2835-dma 20007000.dma: DMA transfer could not be terminated

            The Wolfson card should work just fine on the old RPi (with 26 pin GPIO and pads/pogo-pins for the I2S signals), I'm regularily testing recent kernels for such a setup.

             

            Your configuration also looks fine, but the "DMA ransfer could not be terminated" indicates that there might be a contact problem with the pogo pins - which was a rather common problem.

             

            Try cleaning the P5 pads on the RPi where the pogo pins contact to and also the pogo pins (alcohol and a q-tip usually do the trick). Also make sure the pogo-pins are aligned nicely and make good contact with the pads.

             

            so long,

             

            Hias

            1 of 1 people found this helpful
            • 364. Re: New reworked driver for Wolfson/Cirrus Logic audio card
              miguschweiz

              Hello

               

              Is it possible to play via alsa to AIF1RX3 - AIF1RX8 ? I'm only able to send to AIF1RX1&2. I could need it to route the sound with crossover ladspa plugin to headphones, and Room correction ladspa plugin to speaker (AIF2TX1&2). Looks like the driver is missing some Subdevices (has only 1),as the card would support it. Is there a change to get that in future.

               

              Greets

               

              Michael

              • 365. Re: New reworked driver for Wolfson/Cirrus Logic audio card
                hiassoft

                miguschweiz  schrieb:

                 

                Is it possible to play via alsa to AIF1RX3 - AIF1RX8 ? I'm only able to send to AIF1RX1&2. I could need it to route the sound with crossover ladspa plugin to headphones, and Room correction ladspa plugin to speaker (AIF2TX1&2). Looks like the driver is missing some Subdevices (has only 1),as the card would support it. Is there a change to get that in future.

                Technically it's possible to use AIF1RX1-AIFRX8 (by using TDM mode with 8 slots), I used that as a test while developing the DSP / TDM mode implementation I made in the bcm2835-i2s driver.

                 

                But there are some rather severe limitations which reduce it's practical usefulness:

                 

                The bcm2835 I2S hardware can only transmit 2 channels. So you have to choose which 2 out of the 8 slots / RX interfaces to use.

                 

                Switching the slot configuration can only be done when the I2S hardware is idle. So, for example, if you have a recording running you can't choose another configuration for playback - you have to stop recording first.

                 

                Given these limitations it's not worth the hassle to extend the card driver. If you just want easy access to eg "lineout only" / "headphone only" you can do that via an alsa card conf (in /usr/share/alsa/cards) that exposes separate PCMs and (temporarily) sets the WM5102 alsa mixer controls on-the-fly.

                 

                See eg here for an example: https://github.com/HiassofT/rpi-cirrus-config/blob/master/alsa/RPiCirrus.conf

                 

                This is the alsa card conf we use in LibreELEC to expose an IEC958 (S/PDIF) PCM. By default the card is configured to output sound to line out, headphone out and S/PDIF out, if you use the IEC958 PCM line out, headphone out and speaker out are muted and the S/PDIF out is setup to unity gain (0dB) so compressed AC3/DTS streams can be transmitted via S/PDIF but won't reach the analog outputs - undecoded AC3/DTS streams would sound like ugly noise and could even damage speakers or your ears.

                 

                Changing the WM5102 (output) mixer controls on the fly works fine, so you can even do that when you have a recording running.

                 

                so long,

                 

                Hias

                1 of 1 people found this helpful
                • 366. Re: New reworked driver for Wolfson/Cirrus Logic audio card
                  miguschweiz

                  Thanks for the reply

                   

                  Good to know, will use a workaround then instead.

                   

                  Michael

                  • 367. Re: New reworked driver for Wolfson/Cirrus Logic audio card
                    psyj

                    Matthias,

                     

                    A long time away from the BB and software development for me, moving house and building a new one! Why is this important (to me)?

                     

                    Well I have moved over to a rather fine Marantz amp  ......... which 30 seconds after end of play starts letting out a nasty mains hum. It seems that it is much less tolerant than my old amp of its inputs going open circuit.  I presume that this is due to the sound card being put into standby (via DAPM?). Despite several experiments I have failed to find out which module / parameter needs to be hit.  Is this something that your driver does, or does it sit in the wider system?

                     

                    As always, many thanks

                     

                    John

                     

                    More generally for those that are interested,  the PCB I fabricated up last year still works fine, despite my fears about surface oxidation of the copper.  However I will be moving over to the ribbon cable approach that I mentioned when I build my Quad clone ...... which my wife tells me should be after I have built our bedroom :-(

                    • 368. Re: New reworked driver for Wolfson/Cirrus Logic audio card
                      hiassoft

                      psyj  schrieb:

                       

                      Well I have moved over to a rather fine Marantz amp  ......... which 30 seconds after end of play starts letting out a nasty mains hum. It seems that it is much less tolerant than my old amp of its inputs going open circuit.  I presume that this is due to the sound card being put into standby (via DAPM?). Despite several experiments I have failed to find out which module / parameter needs to be hit.  Is this something that your driver does, or does it sit in the wider system?

                      This is very odd, never had such an issue. Does this also happen if you select an unused input on the amp? Maybe something's coupling into the audio cable from the soundcard to the amp?

                       

                      There's the pmdown_time module parameter of snd-soc-core which controls how long the outputs will be active after the sound device has been closed. But the default is 5000ms which doesn't quite match your 30 seconds...

                       

                      so long,

                       

                      Hias

                      • 369. Re: New reworked driver for Wolfson/Cirrus Logic audio card
                        psyj

                        MY apologies, I forgot to reply  (which might be important for some other readers).  The input hum is the same regardless of whether the audio cable is plugged into the pi or not.  So yes it seems the input (all of them) is very intolerant of being left open circuit.  I have checked the timing again, and yes it is 30 seconds, which is odd since the time to pmdown is 5 seconds.  Obviously in the grand scheme of things this problem is unimportant, since it is in no way connected to how to use the wolfson/pi, so please do not worry yourself. You most certainly have more important things to do.

                         

                        In addition, I have just brought a "Allo" relay switched analogue attenuator, which always presents a load to the amp input....hence no problem. I have high hopes for it, especially since I can run the 5102 at its full output

                         

                        Reegards

                         

                        John

                        • 370. Re: New reworked driver for Wolfson/Cirrus Logic audio card
                          candjhorn

                          Hi. I've just bought a PI 3B+ and the Wolfson card which I have modified and configured as per your article, but I have been unable to get any audio from it. I've run the Playback_to_Lineout script. I've put a logic analyer on the interface pins, and I am getting a frame sync signal but no PCM data or clock. Running dmesg after boot I can see several messages saying CODEC DAI wm5102-aifi not registered. If I try to ouput audio (from media player) dmesg then shows DMA transfer could not be terminated, which I think is consistent with the PCM clock not running. I'm running Raspian 4.14.79 v7. I'm new to the Pi and to Linux, so could you please suggest what might be wrong.

                           

                          Chris

                          • 371. Re: New reworked driver for Wolfson/Cirrus Logic audio card
                            hiassoft

                            candjhorn  schrieb:

                             

                            Hi. I've just bought a PI 3B+ and the Wolfson card which I have modified and configured as per your article, but I have been unable to get any audio from it. I've run the Playback_to_Lineout script. I've put a logic analyer on the interface pins, and I am getting a frame sync signal but no PCM data or clock. Running dmesg after boot I can see several messages saying CODEC DAI wm5102-aifi not registered. If I try to ouput audio (from media player) dmesg then shows DMA transfer could not be terminated, which I think is consistent with the PCM clock not running. I'm running Raspian 4.14.79 v7. I'm new to the Pi and to Linux, so could you please suggest what might be wrong.

                            Triple-check if you correctly removed R39 (especially if there's maybe a short between the R39 pads) and if you correctly wired up the PCM clock and data connections from/to P5.

                             

                            Here's my "cheat-sheet" for doing the mod (I recently modified a Wolfson card for a friend)

                            remove pogo-pins
                            remove R39 (back of PCB, near mounting screw)
                            
                            pogo/P5 layout, from top of PCB
                            
                                     CARD<-      ->GPIO header P1
                            
                                            2  1
                            P35 <- PCM_FS   4  3  PCM_CLK -> P12
                            P40 <- PCM_DOUT 6  5  PCM_DIN -> P38
                                            8  7
                            

                             

                            so long,

                             

                            Hias

                            • 372. Re: New reworked driver for Wolfson/Cirrus Logic audio card
                              candjhorn

                              Thank for your reply Hias. However, I'm pretty sure that I've carried out all the mods correctly. I have just checked for a short across the R39 pads with a multimeter and there is no short. I've also checked from one end of R39 to the P5 pad, and the other end of  R39 to R30 and both those connections check out OK.  I've just checked continuity from the P5 pads right through to the Pi and they are all connected correctly, so I am fairly confident the hardware is connected correctly.

                               

                              On the software side things seem to have installed OK. If I right click the speaker symbol I can see and select the cirrus card. If I look at audio devices in VLC Media player I can see a load of cirrus devices, all of which I've selected in turn, none of which give me any audio.

                               

                              Unfortunately I am new to Unix (more of a Windows person) so not that sure what I'm doing. I've run Playback_to_Lineout from the command prompt by navigating into the relevant directory and typing ./Playback_to_Lineout.sh. Is that right? (I also tried it without the ./) However, I had rather assumed that even without that I should have been seeing the ppm clock.

                               

                              When I first boot up, both red and green LEDs come on, but after a few seconds the red one then goes off. Is that correct?

                               

                              Are there any diagnostics I can run to further track down the problem?

                               

                              Chris

                              • 373. Re: New reworked driver for Wolfson/Cirrus Logic audio card
                                hiassoft

                                Bootup looks fine, it's the same here with the Cirrus card (don't have the Wolfson card hooked up ATM). After power both LEDs are lit, when the card is configured the red one goes off. As you also seem to get the RPi-Cirrus device showing up everything looks fine from the driver / kernel side.

                                 

                                Just to be sure: have you used the cirrus-ng-scripts.tgz from my website? If yes, then calling ./Playback_to_Lineout.sh from the directory where you exctracted it is fine, too. If in doubt better run Reset_paths.sh before that.

                                 

                                It's very puzzling though that you seem to get a frame sync signal but no pcm clock - both of them are generated by the Wolfson/Cirrus card.

                                 

                                Can you test with the following command:

                                speaker-test -D hw:RPiCirrus,0 -c 2 -r 44100 -t sine
                                

                                 

                                This should output a sine signal alternating on the left and right channel, using a samplerate of 44.1kHz in format S16_LE (16 bits).

                                 

                                Then check with the logic analyzer, you should have a 44.1kHz frame sync signal and a 1.4MHz PCM clock. PCM data out (driven from the RPi, but only if the clocks are correct) should show data alternating on the left and right channel.

                                 

                                so long,

                                 

                                Hias

                                • 374. Re: New reworked driver for Wolfson/Cirrus Logic audio card
                                  candjhorn

                                  Hi Hias, Yes the scripts are definitely the ones downloaded from your website. I've run the speaker-test command as you requested. As soon as it starts, I get the 44.1kHz frame signal running but still no data or clock. I get the following on the screen:

                                   

                                  speaker-test 1.1.3

                                   

                                  Playback device is hw:RPiCirrus,0

                                  Stream parameters are 44100Hz, S16_LE, 2 channels

                                  Sine wave rate is 440.0000Hz

                                  Rate set to 44100 Hz (requested 44100Hz)

                                  Buffer size range from 128 to 131072

                                  Period size range from 64 to 65536

                                  Using max buffer size 131072

                                  Periods = 4

                                  was set period_size = 32768

                                  was set buffer_size = 131072

                                  0 - Front Left

                                  1 - Front Right

                                   

                                  After 30 seconds or so I then get the following on the screen:

                                  Write error: -5, Input/output error

                                  xrun recovery failed: -5, Input/output error

                                  Transfer failed: Input/output error

                                  I then get the prompt back and the frame sync signal stops.

                                   

                                  As you say, it is strange that I am getting frame sync but no data or clock. I've verified that the frame sync is indeed being produced by the Wolfson card (by unplugging that connection from the Pi header). The frame sync only runs when something is trying to output audio, such as if I have VLC media player running, or the speaker-test.

                                   

                                  Chris