-
Re: Conecting 3 devices wirelessly
BigG Sep 6, 2017 8:58 AM (in response to nicoloquinte)2 of 2 people found this helpfulA few questions to narrow it down a bit.
Will the controllers be indoors or outdoors?
How often will the controllers need to communicate with each other. i.e. continuous streaming or intermittent?
Then how much data will be sent per transmission.
-
Re: Conecting 3 devices wirelessly
nicoloquinte Sep 6, 2017 9:47 AM (in response to BigG)Thanks for answering me,
The thing will be outdoor and the controllers don't need to communicate to each other the connection need to be continuous streaming but the two controllers need to send continuous data to the receiver, the data will be a combination of different text strings in the form of packets (could be full serial text / non-encrypted.)
moreover, the object can fly at 15 Km/h.
Thanks,
Nico
-
Re: Conecting 3 devices wirelessly
BigG Sep 6, 2017 10:27 AM (in response to nicoloquinte)If it is just text characters then my suggestion would be to look at using ANT radio transceiver module or new Bluetooth 5 transceiver module.
-
-
-
Re: Conecting 3 devices wirelessly
dougwSep 6, 2017 10:58 AM (in response to nicoloquinte)
ZigBee, Bluetooth, and Wi-Fi can also go 100m. I would likely try Bluetooth for simplicity at all nodes.
-
Re: Conecting 3 devices wirelessly
nicoloquinte Sep 6, 2017 11:05 AM (in response to dougw)Ok thanks for all I will use bluetooth (I didnt knew the range could be so enormous)
-
Hello ,I' m currently making a project and I need to connnect two controllers to a master device and I want it to have only one emmiter/reciever (max 70-80M range or a bit less)
What technology I would use ?