6 Replies Latest reply on Nov 7, 2017 5:09 PM by dougw

    Interface Arduino with Maxon Controllers

    darren_busuttil

      Hi all, thank you for your kind attention.

       

      My question is on how to interface an Arduino (Mega) with 2 types of motor controllers from Maxon.  The motor and controllers are the following:

       

      Motor:  EC-45 FLAT 50W  -   https://www.maxonmotor.com/maxon/view/product/251601

      Controller 1:  EPOS2 50/5 -  https://www.maxonmotor.com/maxon/view/product/control/Positionierung/347717

      Controller 2:  ESCON 50/5 - https://www.maxonmotor.com/maxon/view/product/control/4-Q-Servokontroller/409510

       

      Cubli:  http://www.idsc.ethz.ch/research-dandrea/research-projects/cubli.html

       

      My degree project is to implement a one-dimensional Cubli, by which I will use the motor mentioned above and controlled by one of the controllers mentioned above.  In the original Cubli project the motor was controlled with Controller 1 and interfaced with an STM microcontroller.

       

      What I want is to use an Arduino microcontroller, therefore my questions are the following:

       

      1. Controller 1 has interfaces USB, CANOpen and RS232 and I am aware of the non-compatible Logic Levels for Digital IO Pins, but can the Arduino microcontroller be interfaced with one of those interfaces?
      2. Controller 2 somehow can be used with Arduino, but I don't know essentially how to perform it right now, the only source is the video https://www.youtube.com/watch?v=ePJaqmZa0L4.  Also, this controller only has USB interface, so my question is - how can I communicate the ESCON controller with the Arduino and is it possible for this interface only using USB?  Till now I am assuming that the EC-45 FLAT motor is compatible with Controller 2, so any feedback on this aswell will also be greatly appreciate it.

       

      Any required additional info needed please do not hesitate to contact me back.

       

      Thank you again for your kind attention and I look forward for a reply.

       

      Darren Busuttil

      Darren.Busuttil.a103229@mcast.edu.mt