3 Replies Latest reply on Dec 25, 2017 3:03 AM by camille0103

    PCB Templates

    cheriton

      I have recently moved to Circuit Studio from Protel 99SE and am mostly enjoying the extra features while not having too steep a learning curve as it's quite similar to my old system.

      My only real issue is that I've lost the old Protel PCB wizard which used to generate a template for my PCBs with our logo, board name, date, revision, etc,. etc..

      I have looked extensively through CS's various menus and settings and, unless I'm wrong there is no way of making a new PCB with a template showing the same information as before.

      Am I wrong? Is there some way of generating templates for PCBs?

        • Re: PCB Templates
          alexsander_altium

          Hey John, I have an answer for you but its a bit of a work around as its not in the software as of now. To create a template to CircuitStudio this is what you'll have to do:

           

          1. create your project you want to use as a template

          2. give the project, sch, and pcb files the same name (file extension can be different)

          example:

          MyTemplate.PrjPCB

          MyTemplate.CSPCBDoc

          MyTemplate.SCHDoc

           

          3. save these files here: C:\Users\Public\Documents\Altium\CS\Templates\PCB Projects

          4. add to the "PCB Project Templates.ini" file in the same folder as step 3

           

          using step 2 as an example we would put an entry into the INI as follows

           

          [MyTemplate]

           

          Category=Custom

          Title= My custom project template

          Description=Starter PCB w/title block, Schematic with Titleblock, Project with options set.

           

          (you can also add an EMF image of the same name if you want a visual preview)

           

          5. Restart / open CircuitStudio

          6. Create a new project : file>new project  Here you should see a custom category in the templates list

           

          Good luck.

          -Alexsander