16 Replies Latest reply on Jun 1, 2020 7:05 AM by beacon_dave

    Fischertechnik and arduino

    brv64

      Hello!

       

      I'm having a bit of trouble interfacing the Arduino with the Ultrasonic Sensor from Fichertechnik
      https://content.ugfischer.com/cbfiles/fischer/Zulassungen/ft/133009-Ultrasonic-distance-sensor.pdf

      Does anyone have any idea of how I could make it work?
      This is the code I have so far and what I got from the oscilloscope

       

      void setup() {
        // put your setup code here, to run once:
        Serial.begin(9600);
        Serial1.begin(115200, SERIAL_8N1);
        //Serial1.begin(2400);
        pinMode(2,OUTPUT);
      }
      
      
      char data1 = 'a';
      char data2 = 'a';
      
      
      void loop() {
        // put your main code here, to run repeatedly:
        //analogWrite(2,153);
        //delay(1);
        Serial.println("Data: ");
        /*
        for(int i = 0; i < 1; i++){
          digitalWrite(2,HIGH);
          delayMicroseconds(100);
          digitalWrite(2,LOW);
          delayMicroseconds(50);
        }
        */
        
        digitalWrite(2,HIGH);
        delayMicroseconds(125);
        digitalWrite(2,LOW);
        delayMicroseconds(78);
        
        //digitalWrite(2,HIGH);
        //delayMicroseconds(90);
        //digitalWrite(2,LOW);
        
        //Serial1.print('a');
        data1 = Serial1.read();
        data2 = Serial1.read();
        Serial.println(data1,DEC);
        Serial.println(data2,DEC);
        delay(100);
      }
        • Re: Fischertechnik and arduino
          shabaz

          Hi Brandon,

           

          Please could you use the editor tools to share the oscilloscope image (with the Google drive link we have to share information before we can access it, which I at least am not comfortable with and others may or may not feel the same).

           

          The question I had was, how are you handling the same-wire for transmitting the low pulse, and the received data?

           

          One easy method could be to use a transistor (as open drain or open collector) to pull the line low, although software-only methods are possible too.

            • Re: Fischertechnik and arduino
              brv64

              It's ok, I understand.

              I added the images on the post.

              I got those images by connecting the probe directly into a TXT controller and the sensor.

              If you need more images or information, please let me know

              1 of 1 people found this helpful
                • Re: Fischertechnik and arduino
                  shabaz

                  Hi Brandon,

                   

                  I think you're not capturing the beginning part (perhaps your trigger condition needs changing, or different timebase setting), because you should see a 0.2msec delay from when you pull the line low. I can't see a 200msec delay on the traces.

                  However, more concerning, is that there are multiple voltage levels in the trace, when there should only be two levels, low and high. It could be a situation where the microcontroller is functioning with (say) 3.3V logic, and the sensor is working at 5V logic levels for example. Anyway, that needs resolving, before something gets damaged. You can use logic level converters to help here.

                  1 of 1 people found this helpful
                    • Re: Fischertechnik and arduino
                      beacon_dave

                      Hi Shabaz - here is what I see on the scope with a FT Robotics TXT controller and the FT ultrasonic sensor.

                       

                      It doesn't appear to quite match the documentation...

                       

                      As for the levels, the ultrasonic sensor originally was supplied with construction kits for the earlier 'TX' controllers, which were later replaced with the 'TXT' controllers. There is a blog about inside the TX controller here:

                      Hacking the Fischertechnik TX Controller - Stefan Brunner

                       

                      oscilloscope screenshot

                       

                      oscilloscope screenshot

                       

                       

                      oscilloscope screenshot

                       

                      oscilloscope screenshot

                       

                      oscilloscope screenshot

                       

                      oscilloscope screenshot

                       

                      oscilloscope screenshot

                       

                      oscilloscope screenshot

                       

                      oscilloscope screenshot

                       

                      oscilloscope screenshot

                       

                      oscilloscope screenshot

                       

                      oscilloscope screenshot

                       

                      oscilloscope screenshot

                       

                      oscilloscope screenshot

                      2 of 2 people found this helpful
                        • Re: Fischertechnik and arduino
                          shabaz

                          Hi Dave,

                           

                          Great captures! I just had a look at the URL you mentioned, the controllers look really sophisticated!

                            • Re: Fischertechnik and arduino
                              beacon_dave

                              I'm starting to wonder if my captures are inverted...

                               

                              Doesn't really help with the signal being on a black wire with a red connector, and the ground on red/green wire with a green connector... At least the power is on a red wire with a red connector.

                              1 of 1 people found this helpful
                                • Re: Fischertechnik and arduino
                                  beacon_dave

                                  I had another look at this and it is starting to make sense now. The timings appear to be a bit out compared to the documentation though.

                                   

                                  This screenshot shows two 'host queries'. The first query doesn't get a response from the sensor (not mandatory) but presumably causes an ultrasonic 'TX Burst' at the sensor. The second around 10ms later, with the 'RX Response' data supplied in two bytes, high first, then the low. 

                                   

                                  oscilloscope screenshot

                                   

                                   

                                   

                                  This screenshot shows the second 'Host Query' in more detail. The low pulse from the controller is around 44us rather than the documented 78us. The '2-Byte answer' is a bit quicker than the documented 0.2ms - 1ms. The high byte shows a value of 0x80 with only bit D7 set indicating it is the 'first byte'. The low byte shows a value of 0x09 with only bits D0 and D3 set. This distance value corresponds with the value displayed in the control software.

                                  oscilloscope screenshot

                                  1 of 1 people found this helpful
                                    • Re: Fischertechnik and arduino
                                      beacon_dave

                                      It's been a slow day so just posting a few more oscilloscope screenshots I grabbed whilst looking at this sensor set-up yesterday evening.

                                       

                                      The high byte can be seen on the left side which remains at value 0x80 for all these captures. Top bit is set which indicates that it is the 'first byte'.

                                       

                                      This one shows a value of '10' being received. Bits D1 and D3 set in the low byte. Cursors on bit D3 show a bit timing value of around 9us which appears consistent with 115kbaud.

                                      oscilloscope screenshot

                                       

                                       

                                      I should have turned the cursors off at this stage for clarity (or set up my triggering correctly rather than being lazy and relying on digital storage ) but I wasn't intending on posting them here until now.

                                       

                                      Value of '11' being received. Bits D0, D1 & D3 set in the low byte.

                                      oscilloscope screenshot

                                       

                                       

                                      Value of '12' being received. bits D2 & D3 set in the low byte.

                                      oscilloscope screenshot

                                       

                                       

                                      Value of '2' being received. Bit D1 set in the low byte.

                                      oscilloscope screenshot

                                       

                                      For some reason 2 was the smallest distance range I could make the sensor detect with my test setup. Should go down to 0 (distance <4cm)

                                       

                                       

                                      I was able to get a max value of 1023 (distance >400cm) however. With hindsight I should perhaps of captured this end to demonstrate bits D8 and D9 being set in the high byte.

                                       

                                       

                                      Timebase changed from 20us/div to 50us/div for the last three screenshots to include the 'host query' low pulse in the capture.

                                       

                                       

                                      Value of '3' being received. Bits D0 & D1 set in the low byte.

                                      oscilloscope screenshot

                                       

                                      Value of '4' being received. Bit D2 set in the low byte.

                                      oscilloscope screenshot

                                       

                                      Value of '5' being received. Bits D0 & D2 set in the low byte.

                                      oscilloscope screenshot

                                       

                                      Starting to wonder if there is a good tool for quickly annotating oscilloscope captures. Would be nice to be able to quickly draw a grid to overlay the bit positions and have it scale to fit between the desired start and end points allowing for highlighting of start and stop bits.

                                      1 of 1 people found this helpful
                                        • Re: Fischertechnik and arduino
                                          mcb1

                                          Would be nice to be able to quickly draw a grid to overlay the bit positions and have it scale to fit between the desired start and end points allowing for highlighting of start and stop bits.

                                          Almost seems to be a logic analyser ...

                                            • Re: Fischertechnik and arduino
                                              beacon_dave

                                              Yes, but I was thinking more along the lines of a general graphics app that would allow a tutor to quickly overlay and scale an annotation graphic on top of any scope capture image to help illustrate what one is looking at.

                                               

                                              I was thinking along the lines of a Visio smart shape, however Visio is perhaps not the best tool for working with bitmap graphics unless you want to include them as part of a larger document.

                                                • Re: Fischertechnik and arduino
                                                  shabaz

                                                  I've tried manually writing on traces (using digital pen):

                                                  But in the end it seemed a bit ugly (my handwriting isn't great!) so I just used lines/text as usual:

                                                  I suppose what could be done is pull the trace content as a file (most oscilloscopes will allow that) and then use filtering and line-fitting techniques to automatically clean it up. It might actually not be that hard. Could be an interesting project : )

                                                  As a next level it would be very neat if it could detect popular shapes (like sine waves, charge/discharge curves etc) and automatically fit a line (especially if it could be manually tidied up later too, if the user observed that an important part of the trace was accidentally filtered out by the line-fitting algorithm).

                                                  1 of 1 people found this helpful
                                                    • Re: Fischertechnik and arduino
                                                      beacon_dave

                                                      Hi Shabaz - those annotations look great.

                                                       

                                                      I've never quite mastered the digital pen - I tend to need an e-slate tablet which allows you to still write on paper but capture as e-ink, then overlay the two.

                                                       

                                                      I have been meaning to look at pulling the trace out as a file as I find one downside to the standard capture snapshot option is that you often don't end up with a wide enough view of the signal at a sufficient resolution. Would be nice to have an option to create a 'widescreen' screenshot using the complete sample data as opposed to just the window you currently have displayed on the scope. Some higher end scopes may already have this as an option though.

                                          • Re: Fischertechnik and arduino
                                            beacon_dave

                                            The specification for the newer TXT controller can be found at:

                                            https://www.fischertechnik.de/en/products/playing/robotics/522429-robotics-txt-controller

                                            Similar form factor but it is based around a dual processor ARM Cortex A8 (32bit/600mHz) + Cortex M3

                                            1 of 1 people found this helpful
                                  • Re: Fischertechnik and arduino
                                    beacon_dave

                                    It is a shame that the publishing date for this new book has been put back until March 2018

                                    https://www.amazon.co.uk/dp/3864904269/_encoding=UTF8?coliid=I12JZFYLSO5E4A&colid=3C0DWEIAWWTCA&psc=0

                                    as it would have likely answered your question...