1 Reply Latest reply on May 15, 2018 10:31 AM by ifish

    Pi Zero W instead of B+ for GPIO LCD Panel?

    mr_widget

      Per the recent-ish project on the podcast Ben and the gang created a GPIO-based Pi hack with the connectors removed.  Would a similar configuration be feasible using a Pi Zero W?  Most sites in the blogosphere seem to insist only composite video can be connected, but I have a 4.3" panel that I would like to use for a similar project (A dedicated jazz station radio).  It appears that most of the connector is the same between the Pi B+ and the Zero, so if I use the same TFT breakout adaptor would that be successful?

       

      J.R.