1 Reply Latest reply on Jul 26, 2018 7:25 AM by e14softwareuk

    Net Class and Layer Rule or Custom Query Rule doesn't exist

    meengineer

      I see there is an option for Net and Layer rules and a net class rules, but there isn't a net class and layer rule. 

       

      ie.  Sometimes spacing rules on inner traces can be less than spacing rules on outer traces. 

       

      It seems crazy that I would need to make a rule for each net versus a net net class.

       

      So, am I missing something?

       

      I'd be OK if a custom query could be used as well so i can write out the formula to break it down, but that doesn't seem to be an option either.