1 Reply Latest reply on Jun 26, 2017 10:26 AM by jafoste4

    MZEMBV sdsoc 2016.2 platform does not pass Xilinx platform_dm_test

    irelectronic

      The sdsoc 2016.2 platform for Microzed embedded develompment kit don't pass the platform_dm_test procedure.

      Platform_dm_test is a basic liveness test for every data mover used within an SDSOC system compiler.

      The error message is below:

      Parameter cannot be set on a locked block. The block 'processing_system7_1' is locked, because: * This IP has board specific outputs. Current project board 'unset' and the board 'em.avnet.com:microzed_7020:part0:1.1' used to customize the IP 'mzembv_processing_system7_1_0' do not match.