-
Re: Changing Templates does not work
e14softwareuk Jan 31, 2019 8:45 AM (in response to sclifford)Hi, this previous post may help.
-
Re: Changing Templates does not work
sclifford Jan 31, 2019 10:28 PM (in response to e14softwareuk)Sorry but this old post does not fix my issue! I did just as the post stated and i still have the same problem!
Scott
-
Re: Changing Templates does not work
e14softwareuk Feb 1, 2019 4:29 AM (in response to sclifford)1 of 1 people found this helpfulDoes the following work for you. In the CS template folder (C:\Users\Public\Documents\Altium\CS\Templates) copy Letter.SchDot to MyLetter.SchDot. Open CircuitStudio and then drag the new SchDot file onto the application to edit. You should be able to delete the existing logo and add your own image.
In your opening post you refer to errors but the images are missing, it may help if you could edit the post to include the images.
-
Re: Changing Templates does not work
sclifford Feb 1, 2019 8:02 AM (in response to e14softwareuk)OK ... Peter I am going to have to pay better attention to the extensions on these files, and how to properly load them into CS. First the ????.SCHDot files are not accessible from within the File pull down menu/Open Document in CS. This is what got me into trouble, the only way to get the ????.SCHDot files into CS is by dragging them into CS from a window open in File Explore from Windows. Once I dragged in my case the file I named Letter-Driver.SCHDot from File Explore into CS I was able to get the changes made I wanted.
Note once you make the changes to the template one needs to go to there original schematic and right click on the schematic and go under Options, then Document Options to change the default template to the one you just made.
I hope this helps others who wont make the same mistake I made in trying to do this in CS only.
Thanks
For your Help!!!
-
Re: Changing Templates does not work
e14softwareuk Feb 1, 2019 10:10 AM (in response to sclifford)Thanks for letting the community know you have got this working and it should be a valuable how to for other CircuitStudio users.
-
Re: Changing Templates does not work
voltsandjolts Feb 2, 2019 6:04 AM (in response to sclifford)You can open ".SchDot" files from within CS:
File > Open Document > Select extension filter " *.* " (any file) > Pick your SchDot file from the templates directory
... / Public Documents / Altium / CS / Templates
Edit it, add your logo.
Right Click on logo image > Properties > Select "Embedded"
Double click outside the page area to view document options.
Select Parameters tab - here is the source of the special strings you can add to your template.
Add special strings e.g. "=DocumentFullPathAndName", "=SheetNumber", "=SheetTotal" etc. as required to your template.
Save or Save As *.SchDot
Change your default template preference in
File System Preferences > Schematic > General > Defaults
Done.
-
-
-
-
Why can I not change the templates in CS to load my own logo. I am using the Letter format yet when I load the form form the location noted in C:\Users\Public\Documents\Altium\CS\Templates it is completely different than the one show in CS. Second when i load the form it has a black square in the center as well as when I load a logo CS lock up completely!
Here is the Version that loads when I create a schematic
Here is version when i load the Letter template.
What am i doing wrong? I am running CS on my brand new new Surface Pro 6 running windows 10
Scott