1 Reply Latest reply on Feb 8, 2019 1:28 AM by drozwood90

    where is uz7ev.dtsi?

    cb_cross

      Is Avnet working on a DTSI file for the UltraZed boards?

      For instance, after creating a PetaLinux project with the Xilinx provided BSP for the ZCU104, there is this file:  xilinx-zcu104-2018.2/components/plnx_workspace/device-tree/device-tree/zcu104-revc.dtsi

      That file gets referenced when running `petalinux-config` as:

          * DTG Settings

              ** MACHINE_NAME

                  *** zcu104-revc

       

      The UltraZed-EV has no corresponding file after creating a PetaLinux project using the Avnet provided BSP.

       

      I am thinking the lack of this DTSI file is an issue.

       

      I want to TFTP boot my uz7ev board, same as I can do with the ZCU104.

      I followed the steps for the uz7ev as I did for the ZCU104, but the BOOT.BIN file I created for the uz7ev file and flashed to it just generates a little bit of garbled text in the terminal window.