9 Replies Latest reply on Feb 11, 2019 9:52 AM by deville

    Booting from the SD-card: Uboot stuck at I2C:

    deville

      Hi Everyone,

       

      I'm doing a manual build for the Ultrazed-EV-SOM board and When I try to boot the message queue stops at I2C:

      By absence of the defconfig of the board I used the  Xilinx ZynqMP ZCU102 revA defconfig like I've encountered on the old Avnet forums.

       

       

      Xilinx Zynq MP First Stage Boot Loader

       

      Release 2018.2 Feb 6 2019 - 12:16:26

      NOTICE: ATF running on XCZU7EV/silicon v4/RTL5.1 at 0xfffea000

      NOTICE: BL31: Secure code at 0x0

      NOTICE: BL31: Non secure code at 0x8000000

       

      NOTICE: BL31: v1.4(release):93a69a5a

      NOTICE: BL31: Built : 12:25:57, Feb 5 2019

       

      PMUFW:\0x09v1.0

       

      U-Boot 2018.01-dirty (Feb 06 2019 - 12:11:01 +0100) Xilinx ZynqMP ZCU102 revA

      I2C:

       

      Has someone an idea how to get past this or what might be wrong?

       

      Deville

        • Re: Booting from the SD-card: Uboot stuck at I2C:
          drozwood90

          HI,

           

          It seems odd that it is stopping at that location.  The first thing that comes to my mind is to reseat the SOM on the carrier.  The connectors are rather stiff due to the signal integrity they were designed for.  Make sure to carefully disconnect the SOM.  Then after aligning it, press it back in following the perimeter of the board pressing every 1 inch or so.  Visually look along the edge of the connector and ensure that the top and bottom are mating properly.

           

          Of course follow all ESD safety when doing this as you will be touching the bare board during this process.

           

          --Dan