1 Reply Latest reply on Nov 19, 2019 4:55 PM by steveicarus

    I2C protocol for the TDNext 1.26Mpixel Camera Kit

    camerafun

      I am working on a project in which I need to communicate with the 1.26Mpixel camera via a different linux kernel than the boot.bin given on the SD card. In order to communicate with the camera I need to know its I2C commands/registers and the bit configuration of the PMOD and any other configuration details. I also need to know if the camera is software or hardware triggered. Is this information available anywhere? I have not been able to find it, but I might have just missed the location.