4 Replies Latest reply on Jun 6, 2019 10:30 AM by adamwebber

    Still having issues with Printer Driver for Output Generation

    adamwebber

      A Couple of years ago I got an Epson ET-3750 Printer.  After I installed the driver, none of my output generation PDF files came out correctly.  They are all shrunk to about 60%.  I cannot find a workaround for them.  It used to be really nice when I could click on a component and it would display all of the data relating to that part.  I can still click on the parts (at 100%) but it's a guessing game as to where the location will be since it displays the sheets on a smaller scale (at 60%).  I've tried updating the printer driver, uninstalling it, changing it, but to no avail.  It's like it's stuck in this mode now.  Included is an example of a development board I designed last year.

       

      Is there any way that I can fix this problem?  It's quite annoying and doesn't help when I create a project for a client.